USBLib API Guide
1.00.00.01
|
#include <usblib.h>
Data Fields | |
tStdRequest | pfnGetDescriptor |
tStdRequest | pfnRequestHandler |
tInterfaceCallback | pfnInterfaceChange |
tInfoCallback | pfnConfigChange |
tInfoCallback | pfnDataReceived |
tInfoCallback | pfnDataSent |
tUSBIntHandler | pfnResetHandler |
This callback is made when a USB reset is detected. More... | |
tUSBIntHandler | pfnSuspendHandler |
tUSBIntHandler | pfnResumeHandler |
This is called when resume signaling is detected. More... | |
tUSBIntHandler | pfnDisconnectHandler |
This callback is made when the device is disconnected from the USB bus. More... | |
tUSBEPIntHandler | pfnEndpointHandler |
tUSBDeviceHandler | pfnDeviceHandler |
USB event handler functions used during enumeration and operation of the device stack.
tStdRequest tCustomHandlers::pfnGetDescriptor |
This callback is made whenever the USB host requests a non-standard descriptor from the device.
tStdRequest tCustomHandlers::pfnRequestHandler |
This callback is made whenever the USB host makes a non-standard request.
tInterfaceCallback tCustomHandlers::pfnInterfaceChange |
This callback is made in response to a SetInterface request from the host.
tInfoCallback tCustomHandlers::pfnConfigChange |
This callback is made in response to a SetConfiguration request from the host.
tInfoCallback tCustomHandlers::pfnDataReceived |
This callback is made when data has been received following to a call to USBDCDRequestDataEP0.
tInfoCallback tCustomHandlers::pfnDataSent |
This callback is made when data has been transmitted following a call to USBDCDSendDataEP0.
tUSBIntHandler tCustomHandlers::pfnResetHandler |
This callback is made when a USB reset is detected.
Referenced by USBDeviceEnumResetHandler().
tUSBIntHandler tCustomHandlers::pfnSuspendHandler |
This callback is made when the bus has been inactive long enough to trigger a suspend condition.
Referenced by USBDeviceIntHandlerInternal().
tUSBIntHandler tCustomHandlers::pfnResumeHandler |
This is called when resume signaling is detected.
Referenced by USBDeviceIntHandlerInternal(), and USBDeviceResumeTickHandler().
tUSBIntHandler tCustomHandlers::pfnDisconnectHandler |
This callback is made when the device is disconnected from the USB bus.
Referenced by USBDeviceIntHandlerInternal().
tUSBEPIntHandler tCustomHandlers::pfnEndpointHandler |
This callback is made to inform the device of activity on all endpoints other than endpoint zero.
Referenced by USBDeviceIntHandlerInternal().
tUSBDeviceHandler tCustomHandlers::pfnDeviceHandler |
This generic handler is provided to allow requests based on a given instance to be passed into a device. This is commonly used by a top level composite device that is using multiple instances of a class.
Referenced by USBDeviceIntHandlerInternal().