Data Structures | Macros | Typedefs | Variables
CANMSP432E4.h File Reference

Detailed Description

CAN driver implementation for a MSP432E4 CAN controller.

============================================================================

The CAN header file should be included in an application as follows:

Stack requirements

The CANMSP432E4 driver is a (ring) buffered driver that stores data it may

have already received in a user-supplied background buffer.

#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/devices/msp432e4/inc/msp432.h>
#include <ti/devices/msp432e4/driverlib/gpio.h>
#include <ti/devices/msp432e4/driverlib/pin_map.h>
#include <ti/drivers/dpl/ClockP.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>
#include <ti/drivers/gpio/GPIOMSP432E4.h>
#include <ti/drivers/CAN.h>
#include <ti/drivers/utils/List.h>
#include <ti/drivers/utils/StructRingBuf.h>
Include dependency graph for CANMSP432E4.h:

Go to the source code of this file.

Data Structures

struct  CANMSP432E4_HWAttrs
 CANMSP432E4 Hardware attributes. More...
 
struct  CANMSP432E4_Object
 CANMSP432E4 Object. More...
 

Macros

#define CANMSP432E4_PA0_CAN0RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_CAN0RX)
 PA0 is used for CAN0 RX. More...
 
#define CANMSP432E4_PA1_CAN0TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_CAN0TX)
 PA1 is used for CAN0 RX. More...
 
#define CANMSP432E4_PB0_CAN1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_CAN1RX)
 PB0 is used for CAN1 RX. More...
 
#define CANMSP432E4_PB1_CAN1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_CAN1TX)
 PB1 is used for CAN1 RX. More...
 

Typedefs

typedef void(* CANMSP432E4_ErrorCallback) (CAN_Handle handle, uint32_t error)
 The definition of an optional callback function used by the CAN driver to notify the application when a receive error (FIFO overrun, parity error, etc) occurs. More...
 
typedef struct CANMSP432E4_ObjectCANMSP432E4_Handle
 

Variables

const CAN_FxnTable CANMSP432E4_fxnTable
 

Macro Definition Documentation

§ CANMSP432E4_PA0_CAN0RX

#define CANMSP432E4_PA0_CAN0RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_CAN0RX)

PA0 is used for CAN0 RX.

§ CANMSP432E4_PA1_CAN0TX

#define CANMSP432E4_PA1_CAN0TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_CAN0TX)

PA1 is used for CAN0 RX.

§ CANMSP432E4_PB0_CAN1RX

#define CANMSP432E4_PB0_CAN1RX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_CAN1RX)

PB0 is used for CAN1 RX.

§ CANMSP432E4_PB1_CAN1TX

#define CANMSP432E4_PB1_CAN1TX   GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_CAN1TX)

PB1 is used for CAN1 RX.

Typedef Documentation

§ CANMSP432E4_ErrorCallback

typedef void(* CANMSP432E4_ErrorCallback) (CAN_Handle handle, uint32_t error)

The definition of an optional callback function used by the CAN driver to notify the application when a receive error (FIFO overrun, parity error, etc) occurs.

Parameters
CAN_HandleCAN_Handle
errorThe current value of the receive status register. Please refer to the device data sheet to interpret this value.

§ CANMSP432E4_Handle

Variable Documentation

§ CANMSP432E4_fxnTable

const CAN_FxnTable CANMSP432E4_fxnTable
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale