USBLib API Guide  1.00.00.01
Data Fields
tHIDReportIdle Struct Reference

#include <usbdhid.h>

Data Fields

uint8_t ui8Duration4mS
 
uint8_t ui8ReportID
 
uint16_t ui16TimeTillNextmS
 
uint32_t ui32TimeSinceReportmS
 

Detailed Description

The structure used to track idle time for reports. An array of these structures is passed to the HID device class driver during USBDHIDInit and is used to track automatic resending of each report (if not disabled by the host).

Field Documentation

§ ui8Duration4mS

uint8_t tHIDReportIdle::ui8Duration4mS

The idle duration for the report expressed in units of 4mS. 0 indicates infinite and informs the class driver not to send the report unless a state change occurs.

Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().

§ ui8ReportID

uint8_t tHIDReportIdle::ui8ReportID

The ID of the report which this structure applies to. This is the report ID as specified using a ReportID tag in the report descriptor rather than the index of the report in the HID class descriptor array. If only a single Input report is supported and, thus, no ReportID tag is present, this field should be set to 0.

Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().

§ ui16TimeTillNextmS

uint16_t tHIDReportIdle::ui16TimeTillNextmS

The number of milliseconds before we need to send a copy of a given report back to the host. This field is updated by the HID driver and used to time sending of USBD_HID_EVENT_IDLE_TIMEOUT.

Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().

§ ui32TimeSinceReportmS

uint32_t tHIDReportIdle::ui32TimeSinceReportmS

The number of milliseconds that have passed since the last time this report was sent. The HID class driver needs to track this since Set_Idle requests are required to take effect as if issued immediately after the last transmission of the report to which they refer.

Referenced by USBDHIDGamepadCompositeInit(), USBDHIDKeyboardCompositeInit(), USBDHIDMouseCompositeInit(), and USBDHIDSensorCompositeInit().


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale