![]() |
![]() |
UARTMSP432E4 Object. More...
#include <UARTMSP432E4.h>
Data Fields | |
struct { | |
bool opened:1 | |
UART_Mode readMode:1 | |
UART_Mode writeMode:1 | |
UART_DataMode readDataMode:1 | |
UART_DataMode writeDataMode:1 | |
UART_ReturnMode readReturnMode:1 | |
UART_Echo readEcho:1 | |
bool bufTimeout:1 | |
bool callCallback:1 | |
bool drainByISR:1 | |
bool rxEnabled:1 | |
bool inReadCallback:1 | |
volatile bool readCallbackPending:1 | |
} | state |
ClockP_Handle | timeoutClk |
uint32_t | baudRate |
UART_LEN | dataLength |
UART_STOP | stopBits |
UART_PAR | parityType |
RingBuf_Object | ringBuffer |
UARTMSP432E4_FxnSet | readFxns |
unsigned char * | readBuf |
size_t | readSize |
size_t | readCount |
SemaphoreP_Handle | readSem |
unsigned int | readTimeout |
UART_Callback | readCallback |
const unsigned char * | writeBuf |
size_t | writeSize |
size_t | writeCount |
SemaphoreP_Handle | writeSem |
unsigned int | writeTimeout |
UART_Callback | writeCallback |
HwiP_Handle | hwi |
UARTMSP432E4 Object.
The application must not access any member variables of this structure!
bool UARTMSP432E4_Object::opened |
UART_Mode UARTMSP432E4_Object::readMode |
UART_Mode UARTMSP432E4_Object::writeMode |
UART_DataMode UARTMSP432E4_Object::readDataMode |
UART_DataMode UARTMSP432E4_Object::writeDataMode |
UART_ReturnMode UARTMSP432E4_Object::readReturnMode |
UART_Echo UARTMSP432E4_Object::readEcho |
bool UARTMSP432E4_Object::bufTimeout |
bool UARTMSP432E4_Object::callCallback |
bool UARTMSP432E4_Object::drainByISR |
bool UARTMSP432E4_Object::rxEnabled |
bool UARTMSP432E4_Object::inReadCallback |
volatile bool UARTMSP432E4_Object::readCallbackPending |
struct { ... } UARTMSP432E4_Object::state |
ClockP_Handle UARTMSP432E4_Object::timeoutClk |
uint32_t UARTMSP432E4_Object::baudRate |
UART_LEN UARTMSP432E4_Object::dataLength |
UART_STOP UARTMSP432E4_Object::stopBits |
UART_PAR UARTMSP432E4_Object::parityType |
RingBuf_Object UARTMSP432E4_Object::ringBuffer |
UARTMSP432E4_FxnSet UARTMSP432E4_Object::readFxns |
unsigned char* UARTMSP432E4_Object::readBuf |
size_t UARTMSP432E4_Object::readSize |
size_t UARTMSP432E4_Object::readCount |
SemaphoreP_Handle UARTMSP432E4_Object::readSem |
unsigned int UARTMSP432E4_Object::readTimeout |
UART_Callback UARTMSP432E4_Object::readCallback |
const unsigned char* UARTMSP432E4_Object::writeBuf |
size_t UARTMSP432E4_Object::writeSize |
size_t UARTMSP432E4_Object::writeCount |
SemaphoreP_Handle UARTMSP432E4_Object::writeSem |
unsigned int UARTMSP432E4_Object::writeTimeout |
UART_Callback UARTMSP432E4_Object::writeCallback |
HwiP_Handle UARTMSP432E4_Object::hwi |