ComparatorMSP432E4 Hardware attributes.
More...
#include <ComparatorMSP432E4.h>
ComparatorMSP432E4 Hardware attributes.
A sample structure is shown below:
{
.intNum = INT_COMP0,
.intPriority = (~0),
}
};
§ intNum
uint32_t ComparatorMSP432E4_HWAttrs::intNum |
< Device-specific interrupt number
§ intPriority
uint32_t ComparatorMSP432E4_HWAttrs::intPriority |
§ compNum
uint32_t ComparatorMSP432E4_HWAttrs::compNum |
§ positiveTerminal
§ triggerLevel
§ refLevel
Output pin. Some comparators only have 1 option.
§ outputPin
uint32_t ComparatorMSP432E4_HWAttrs::outputPin |
The documentation for this struct was generated from the following file: