![]() |
![]() |
CRCMSP432E4 Hardware Attributes. More...
#include <CRCMSP432E4.h>
Data Fields | |
CRC_CallbackFxn | callbackFxn |
uint32_t | timeout |
uint32_t | seed |
uint32_t | finalXorValue |
uint32_t | configRegister |
void * | resultLocation |
uint32_t | resultRawPartial |
uint32_t | resultProcessedPartial |
CRC_DataSize | dataSize |
CRC_ByteSwap | byteSwapInput |
CRC_ReturnBehavior | returnBehavior |
uint8_t | isOpen |
uint8_t | ongoingPartial |
CRCMSP432E4 Hardware Attributes.
The CRCMSP432E4 driver does not have any configurable hardware attributes. NULL should be used for the hwAttrs parameter of the CRC_Config struct.
CRCMSP432E4 Object
The application must not access any member variables of this structure!
CRC_CallbackFxn CRCMSP432E4_Object::callbackFxn |
uint32_t CRCMSP432E4_Object::timeout |
uint32_t CRCMSP432E4_Object::seed |
uint32_t CRCMSP432E4_Object::finalXorValue |
uint32_t CRCMSP432E4_Object::configRegister |
void* CRCMSP432E4_Object::resultLocation |
uint32_t CRCMSP432E4_Object::resultRawPartial |
uint32_t CRCMSP432E4_Object::resultProcessedPartial |
CRC_DataSize CRCMSP432E4_Object::dataSize |
CRC_ByteSwap CRCMSP432E4_Object::byteSwapInput |
CRC_ReturnBehavior CRCMSP432E4_Object::returnBehavior |
uint8_t CRCMSP432E4_Object::isOpen |
uint8_t CRCMSP432E4_Object::ongoingPartial |