Struct containing the parameters required for encrypting/decrypting and a message.
More...
#include <AESECB.h>
Struct containing the parameters required for encrypting/decrypting and a message.
§ key
§ input
uint8_t* AESECB_Operation::input |
- Encryption: The plaintext buffer to be encrypted in the ECB operation.
- Decryption: The ciphertext to be decrypted.
§ output
uint8_t* AESECB_Operation::output |
- Encryption: The output ciphertext buffer that the encrypted plaintext is copied to.
- Decryption: The plaintext derived from the decrypted ciphertext is copied here.
§ inputLength
size_t AESECB_Operation::inputLength |
Length of the input and output in bytes. Must be a multiple of the AES block size (16 bytes)
The documentation for this struct was generated from the following file: