Macros | |
#define | ComparatorMSP432E4_EVENT_RISING (Comparator_EVENT_RESERVED + 1) |
#define | ComparatorMSP432E4_EVENT_FALLING (Comparator_EVENT_RESERVED + 2) |
#define | ComparatorMSP432E4_EVENT_EDGE (Comparator_EVENT_RESERVED + 3) |
#define | ComparatorMSP432E4_EVENT_HIGH (Comparator_EVENT_RESERVED + 4) |
#define | ComparatorMSP432E4_EVENT_LOW (Comparator_EVENT_RESERVED + 5) |
Comparator callback function. In the case of both edges, the edge will not be determined for accuracy.
#define ComparatorMSP432E4_EVENT_RISING (Comparator_EVENT_RESERVED + 1) |
#define ComparatorMSP432E4_EVENT_FALLING (Comparator_EVENT_RESERVED + 2) |
#define ComparatorMSP432E4_EVENT_EDGE (Comparator_EVENT_RESERVED + 3) |
#define ComparatorMSP432E4_EVENT_HIGH (Comparator_EVENT_RESERVED + 4) |
#define ComparatorMSP432E4_EVENT_LOW (Comparator_EVENT_RESERVED + 5) |