Network Services API  2.70.01.02
Data Fields
URLHandler_Setup Struct Reference

Structure containing URL Handler components. More...

#include <ti/net/http/urlhandler.h>

Collaboration diagram for URLHandler_Setup:
Collaboration graph

Data Fields

void * params
 Parameters needed for URL Handler instantiation. More...
 
URLHandler_CreateFxn create
 URL Handler Create function. More...
 
URLHandler_DeleteFxn del
 URL Handler Delete function. More...
 
URLHandler_ProcessFxn process
 URL Handler Process function. More...
 
URLHandler_ScanFieldFxn scanField
 Scan field function. More...
 
void * reserved1
 This field is reserved - set to NULL. More...
 

Detailed Description

Structure containing URL Handler components.

This structure contains parameters needed for setup of a user- defined URLHandler object and pointers to associated user-defined URLHandler_* functions. The created HTTP Server maintains a table of this data structure for each unique URL Handler.

Field Documentation

§ params

void* URLHandler_Setup::params

Parameters needed for URL Handler instantiation.

§ create

URLHandler_CreateFxn URLHandler_Setup::create

URL Handler Create function.

§ del

URLHandler_DeleteFxn URLHandler_Setup::del

URL Handler Delete function.

§ process

URLHandler_ProcessFxn URLHandler_Setup::process

URL Handler Process function.

§ scanField

URLHandler_ScanFieldFxn URLHandler_Setup::scanField

Scan field function.

§ reserved1

void* URLHandler_Setup::reserved1

This field is reserved - set to NULL.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale