Network Developers Kit API  3.71.00.05
Data Structures | Typedefs | Functions
Telnet Service

The Telnet Server service provides a mechanism for exposing a stream IO connection to any remote telnet client console. More...

Data Structures

struct  _ntparam_telnet
 
struct  _ci_service_telnet
 

Typedefs

typedef struct _ntparam_telnet NTPARAM_TELNET
 
typedef struct _ci_service_telnet CI_SERVICE_TELNET
 

Functions

void * TelnetOpen (NTARGS *pNTA, NTPARAM_TELNET *pNTP)
 Create an instance of the Telnet Server. More...
 
void TelnetClose (void *hTelnet)
 Destroy an instance of the Telnet Server. More...
 

Detailed Description

The Telnet Server service provides a mechanism for exposing a stream IO connection to any remote telnet client console.

Typedef Documentation

§ NTPARAM_TELNET

§ CI_SERVICE_TELNET

Function Documentation

§ TelnetOpen()

void* TelnetOpen ( NTARGS *  pNTA,
NTPARAM_TELNET pNTP 
)

Create an instance of the Telnet Server.

Parameters
[in]pNTAPointer to common arg structure used for all services
[in]pNTPPointer to Telnet parameter structure
Remarks
When a Telnet session is established, a telnet child task is spawned that will call the supplied callback function. This callback function should return a local file descriptor of one end of a full duplex pipe. If the callback function returns -1, the connection is aborted.
When either the terminal or telnet connection end of the pipe is broken, the other connection is closed and the session is ended.
Returns
Success: handle to new Telnet Server instance
Failure: NULL
See also
TelnetClose()

§ TelnetClose()

void TelnetClose ( void *  hTelnet)

Destroy an instance of the Telnet Server.

Parameters
[in]hTelnetHandle to Telnet Server instance obtained from TelnetOpen()
Remarks
When called the server is shut down and no further Telnet sessions can be established. Also, all spawned connections are immediately terminated.
See also
TelnetOpen()
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale