Network Developers Kit API  3.71.00.05
Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
HTTP Server Service

The HTTP Server service provides a mechanism for serving HTTP content to remote HTTP client applications. More...

Data Structures

struct  _ntparam_http
 
struct  _ci_service_http
 

Macros

#define HTTPPORT   80
 
#define MAX_RESPONSE_SIZE   200
 
#define http400(Sock)   httpSendErrorResponse((Sock), HTTP_BAD_REQUEST)
 
#define http404(Sock)   httpSendErrorResponse((Sock), HTTP_NOT_FOUND)
 
#define http405(Sock)   httpSendErrorResponse((Sock), HTTP_NOT_ALLOWED)
 
#define http501(Sock)   httpSendErrorResponse((Sock), HTTP_NOT_IMPLEMENTED)
 

Typedefs

typedef struct _ntparam_http NTPARAM_HTTP
 
typedef struct _ci_service_http CI_SERVICE_HTTP
 

Enumerations

enum  HTTP_STATUS_CODE {
  HTTP_OK =200,
  HTTP_NO_CONTENT =204,
  HTTP_BAD_REQUEST =400,
  HTTP_AUTH_REQUIRED =401,
  HTTP_NOT_FOUND =404,
  HTTP_NOT_ALLOWED =405,
  HTTP_NOT_IMPLEMENTED =501,
  HTTP_STATUS_CODE_END
}
 

Functions

void * httpOpen (NTARGS *pNTA, NTPARAM_HTTP *pNTP)
 Create an instance of the HTTP Server. More...
 
void httpClose (void *hHTTP)
 Destroy an instance of the HTTP Server. More...
 
int httpVersion (void)
 
void httpSendClientStr (SOCKET Sock, char *Response)
 
void httpSendStatusLine (SOCKET Sock, int StatusCode, char *ContentType)
 
void httpSendFullResponse (SOCKET Sock, int StatusCode, char *RequestedFile)
 
void httpSendEntityLength (SOCKET Sock, int32_t EntityLength)
 
void httpSendErrorResponse (SOCKET Sock, int StatusCode)
 

Variables

char * CONTENT_TYPE_APPLET
 
char * CONTENT_TYPE_AU
 
char * CONTENT_TYPE_CSS
 
char * CONTENT_TYPE_DOC
 
char * CONTENT_TYPE_GIF
 
char * CONTENT_TYPE_HTML
 
char * CONTENT_TYPE_JPG
 
char * CONTENT_TYPE_MPEG
 
char * CONTENT_TYPE_PDF
 
char * CONTENT_TYPE_WAV
 
char * CONTENT_TYPE_ZIP
 
char * CONTENT_TYPE
 
char * CONTENT_LENGTH
 
char * CRLF
 
char * DEFAULT_NAME
 
char * HTTP_VER
 
char * SPACE
 
int(* httpErrorResponseHook )(SOCKET Sock, int StatusCode)
 

Detailed Description

The HTTP Server service provides a mechanism for serving HTTP content to remote HTTP client applications.

Deprecated:
The HTTP Server support in the NDK is deprecated and will be removed in the near future. Users are highly recommended to migrate to the HTTPServer module provided by the Network Services (NS) Component.

Macro Definition Documentation

§ HTTPPORT

#define HTTPPORT   80

§ MAX_RESPONSE_SIZE

#define MAX_RESPONSE_SIZE   200

§ http400

#define http400 (   Sock)    httpSendErrorResponse((Sock), HTTP_BAD_REQUEST)

§ http404

#define http404 (   Sock)    httpSendErrorResponse((Sock), HTTP_NOT_FOUND)

§ http405

#define http405 (   Sock)    httpSendErrorResponse((Sock), HTTP_NOT_ALLOWED)

§ http501

#define http501 (   Sock)    httpSendErrorResponse((Sock), HTTP_NOT_IMPLEMENTED)

Typedef Documentation

§ NTPARAM_HTTP

typedef struct _ntparam_http NTPARAM_HTTP

§ CI_SERVICE_HTTP

Deprecated:
The HTTP Server support in the NDK is deprecated and will be removed in the near future. Users are highly recommended to migrate to the HTTPServer module provided by the Network Services (NS) Component.

Enumeration Type Documentation

§ HTTP_STATUS_CODE

Enumerator
HTTP_OK 
HTTP_NO_CONTENT 
HTTP_BAD_REQUEST 
HTTP_AUTH_REQUIRED 
HTTP_NOT_FOUND 
HTTP_NOT_ALLOWED 
HTTP_NOT_IMPLEMENTED 
HTTP_STATUS_CODE_END 

Function Documentation

§ httpOpen()

void* httpOpen ( NTARGS *  pNTA,
NTPARAM_HTTP pNTP 
)

Create an instance of the HTTP Server.

Deprecated:
The HTTP Server support in the NDK is deprecated and will be removed in the near future. Users are highly recommended to migrate to the HTTPServer module provided by the Network Services (NS) Component.
Parameters
[in]pNTAPointer to common arg structure used for all services
[in]pNTPPointer to HTTP parameter structure
Remarks
Starts the HTTP server process. This process will create a connection to the HTTP Port and listen. When a connection is made, another task will be created to service the request.
Returns
Success: handle to new HTTP Server instance
Failure: NULL
See also
httpClose()

§ httpClose()

void httpClose ( void *  hHTTP)

Destroy an instance of the HTTP Server.

Deprecated:
The HTTP Server support in the NDK is deprecated and will be removed in the near future. Users are highly recommended to migrate to the HTTPServer module provided by the Network Services (NS) Component.
Parameters
[in]hHTTPHandle to HTTP Server instance obtained from httpOpen()
Remarks
Destroys the instance of the HTTP Server indicated by the supplied handle. Once called, the Server is shut down.
See also
httpOpen()

§ httpVersion()

int httpVersion ( void  )

§ httpSendClientStr()

void httpSendClientStr ( SOCKET  Sock,
char *  Response 
)

§ httpSendStatusLine()

void httpSendStatusLine ( SOCKET  Sock,
int  StatusCode,
char *  ContentType 
)

§ httpSendFullResponse()

void httpSendFullResponse ( SOCKET  Sock,
int  StatusCode,
char *  RequestedFile 
)

§ httpSendEntityLength()

void httpSendEntityLength ( SOCKET  Sock,
int32_t  EntityLength 
)

§ httpSendErrorResponse()

void httpSendErrorResponse ( SOCKET  Sock,
int  StatusCode 
)

Variable Documentation

§ CONTENT_TYPE_APPLET

char* CONTENT_TYPE_APPLET

INTERNAL

§ CONTENT_TYPE_AU

char* CONTENT_TYPE_AU

§ CONTENT_TYPE_CSS

char* CONTENT_TYPE_CSS

§ CONTENT_TYPE_DOC

char* CONTENT_TYPE_DOC

§ CONTENT_TYPE_GIF

char* CONTENT_TYPE_GIF

§ CONTENT_TYPE_HTML

char* CONTENT_TYPE_HTML

§ CONTENT_TYPE_JPG

char* CONTENT_TYPE_JPG

§ CONTENT_TYPE_MPEG

char* CONTENT_TYPE_MPEG

§ CONTENT_TYPE_PDF

char* CONTENT_TYPE_PDF

§ CONTENT_TYPE_WAV

char* CONTENT_TYPE_WAV

§ CONTENT_TYPE_ZIP

char* CONTENT_TYPE_ZIP

§ CONTENT_TYPE

char* CONTENT_TYPE

§ CONTENT_LENGTH

char* CONTENT_LENGTH

§ CRLF

char* CRLF

§ DEFAULT_NAME

char* DEFAULT_NAME

§ HTTP_VER

char* HTTP_VER

§ SPACE

char* SPACE

§ httpErrorResponseHook

int(* httpErrorResponseHook) (SOCKET Sock, int StatusCode)
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale