![]() |
![]() |
USBLib API Guide
1.00.00.01
|
#include <usbdbulk.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps. More... | |
const uint8_t | ui8PwrAttributes |
const tUSBCallback | pfnRxCallback |
void * | pvRxCBData |
const tUSBCallback | pfnTxCallback |
void * | pvTxCBData |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
tBulkInstance | sPrivateData |
The structure used by the application to define operating parameters for the bulk device.
const uint16_t tUSBDBulkDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
Referenced by USBDBulkInit().
const uint16_t tUSBDBulkDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
Referenced by USBDBulkInit().
const uint16_t tUSBDBulkDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps.
Referenced by USBDBulkInit().
const uint8_t tUSBDBulkDevice::ui8PwrAttributes |
Indicates whether the device is self- or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
Referenced by USBDBulkInit().
const tUSBCallback tUSBDBulkDevice::pfnRxCallback |
A pointer to the callback function which will be called to notify the application of events related to the device's data receive channel.
Referenced by USBDBulkCompositeInit().
void* tUSBDBulkDevice::pvRxCBData |
A client-supplied pointer which will be sent as the first parameter in all calls made to the receive channel callback, pfnRxCallback.
const tUSBCallback tUSBDBulkDevice::pfnTxCallback |
A pointer to the callback function which will be called to notify the application of events related to the device's data transmit channel.
Referenced by USBDBulkCompositeInit().
void* tUSBDBulkDevice::pvTxCBData |
A client-supplied pointer which will be sent as the first parameter in all calls made to the transmit channel callback, pfnTxCallback.
const uint8_t* const* tUSBDBulkDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain pointers to the following string descriptors in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1), Interface description string (language 1) and Configuration description string (language 1).
If supporting more than 1 language, the strings for indices 1 through 5 must be repeated for each of the other languages defined in the language descriptor.
Referenced by USBDBulkCompositeInit().
const uint32_t tUSBDBulkDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be 1 + (5 * number of supported languages).
tBulkInstance tUSBDBulkDevice::sPrivateData |
The private instance data for this device. This memory must not be modified by any code outside the bulk class driver.
Referenced by USBDBulkCompositeInit(), and USBDBulkInit().