![]() |
![]() |
USBLib API Guide
1.00.00.01
|
#include <usblib.h>
Data Fields | |
bool | bTransmitBuffer |
tUSBCallback | pfnCallback |
void * | pvCBData |
tUSBPacketTransfer | pfnTransfer |
tUSBPacketAvailable | pfnAvailable |
void * | pvHandle |
uint8_t * | pui8Buffer |
uint32_t | ui32BufferSize |
The size, in bytes, of the buffer pointed to by pi8Buffer. More... | |
tUSBBufferVars | sPrivateData |
The structure used by the application to initialize a buffer object that will provide buffered access to either a transmit or receive channel.
bool tUSBBuffer::bTransmitBuffer |
This field sets the mode of the buffer. If true, the buffer operates as a transmit buffer and supports calls to USBBufferWrite by the client. If false, the buffer operates as a receive buffer and supports calls to USBBufferRead.
Referenced by USBBufferEventCallback(), and USBBufferWrite().
tUSBCallback tUSBBuffer::pfnCallback |
A pointer to the callback function which will be called to notify the application of all asynchronous events related to the operation of the buffer.
Referenced by USBBufferInit().
void* tUSBBuffer::pvCBData |
A pointer that the buffer will pass back to the client in the first parameter of all callbacks related to this instance.
Referenced by USBBufferCallbackDataSet().
tUSBPacketTransfer tUSBBuffer::pfnTransfer |
The function which should be called to transmit a packet of data in transmit mode or receive a packet in receive mode.
Referenced by USBBufferInit().
tUSBPacketAvailable tUSBBuffer::pfnAvailable |
The function which should be called to determine if the endpoint is ready to accept a new packet for transmission in transmit mode or to determine the size of the buffer required to read a packet in receive mode.
Referenced by USBBufferInit().
void* tUSBBuffer::pvHandle |
The handle to pass to the low level function pointers provided in the pfnTransfer and pfnAvailable members. For USB device use, this is the psDevice parameter required by the relevant device class driver APIs. For USB host use, this is the pipe identifier returned by USBHCDPipeAlloc.
uint8_t* tUSBBuffer::pui8Buffer |
A pointer to memory to be used as the ring buffer for this instance.
Referenced by USBBufferInit().
uint32_t tUSBBuffer::ui32BufferSize |
The size, in bytes, of the buffer pointed to by pi8Buffer.
Referenced by USBBufferInit().
tUSBBufferVars tUSBBuffer::sPrivateData |
The private data for the USB buffer that is allocated by the application.
Referenced by USBBufferInfoGet(), and USBBufferInit().