Macros
values that will be passed to the

Macros

#define ComparatorMSP432E4_EVENT_RISING   (Comparator_EVENT_RESERVED + 1)
 
#define ComparatorMSP432E4_EVENT_FALLING   (Comparator_EVENT_RESERVED + 2)
 
#define ComparatorMSP432E4_EVENT_EDGE   (Comparator_EVENT_RESERVED + 3)
 
#define ComparatorMSP432E4_EVENT_HIGH   (Comparator_EVENT_RESERVED + 4)
 
#define ComparatorMSP432E4_EVENT_LOW   (Comparator_EVENT_RESERVED + 5)
 

Detailed Description

Comparator callback function. In the case of both edges, the edge will not be determined for accuracy.

Macro Definition Documentation

§ ComparatorMSP432E4_EVENT_RISING

#define ComparatorMSP432E4_EVENT_RISING   (Comparator_EVENT_RESERVED + 1)

§ ComparatorMSP432E4_EVENT_FALLING

#define ComparatorMSP432E4_EVENT_FALLING   (Comparator_EVENT_RESERVED + 2)

§ ComparatorMSP432E4_EVENT_EDGE

#define ComparatorMSP432E4_EVENT_EDGE   (Comparator_EVENT_RESERVED + 3)

§ ComparatorMSP432E4_EVENT_HIGH

#define ComparatorMSP432E4_EVENT_HIGH   (Comparator_EVENT_RESERVED + 4)

§ ComparatorMSP432E4_EVENT_LOW

#define ComparatorMSP432E4_EVENT_LOW   (Comparator_EVENT_RESERVED + 5)
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale