173 #ifndef ti_drivers_spi_SPIMSP432E4DMA__include 174 #define ti_drivers_spi_SPIMSP432E4DMA__include 179 #include <ti/devices/msp432e4/inc/msp432.h> 181 #include <ti/devices/msp432e4/driverlib/pin_map.h> 184 #include <ti/drivers/dpl/HwiP.h> 185 #include <ti/drivers/dpl/SemaphoreP.h> 201 #define SPIMSP432E4_PA2_SSI0CLK GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 2, GPIO_PA2_SSI0CLK) 206 #define SPIMSP432E4_PA3_SSI0FSS GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 3, GPIO_PA3_SSI0FSS) 211 #define SPIMSP432E4_PA4_SSI0XDAT0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 4, GPIO_PA4_SSI0XDAT0) 216 #define SPIMSP432E4_PA5_SSI0XDAT1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 5, GPIO_PA5_SSI0XDAT1) 221 #define SPIMSP432E4_PB5_SSI1CLK GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 5, GPIO_PB5_SSI1CLK) 226 #define SPIMSP432E4_PB4_SSI1FSS GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 4, GPIO_PB4_SSI1FSS) 231 #define SPIMSP432E4_PE4_SSI1XDAT0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 4, GPIO_PE4_SSI1XDAT0) 236 #define SPIMSP432E4_PE5_SSI1XDAT1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 5, GPIO_PE5_SSI1XDAT1) 241 #define SPIMSP432E4_PD3_SSI2CLK GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 3, GPIO_PD3_SSI2CLK) 246 #define SPIMSP432E4_PG7_SSI2CLK GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 7, GPIO_PG7_SSI2CLK) 251 #define SPIMSP432E4_PD2_SSI2FSS GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 2, GPIO_PD2_SSI2FSS) 256 #define SPIMSP432E4_PG6_SSI2FSS GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 6, GPIO_PG6_SSI2FSS) 261 #define SPIMSP432E4_PD1_SSI2XDAT0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 1, GPIO_PD1_SSI2XDAT0) 266 #define SPIMSP432E4_PG5_SSI2XDAT0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 5, GPIO_PG5_SSI2XDAT0) 271 #define SPIMSP432E4_PD0_SSI2XDAT1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 0, GPIO_PD0_SSI2XDAT1) 276 #define SPIMSP432E4_PG4_SSI2XDAT1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 4, GPIO_PG4_SSI2XDAT1) 281 #define SPIMSP432E4_PQ0_SSI3CLK GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 0, GPIO_PQ0_SSI3CLK) 286 #define SPIMSP432E4_PF3_SSI3CLK GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 3, GPIO_PF3_SSI3CLK) 291 #define SPIMSP432E4_PQ1_SSI3FSS GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 1, GPIO_PQ1_SSI3FSS) 296 #define SPIMSP432E4_PF2_SSI3FSS GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 2, GPIO_PF2_SSI3FSS) 301 #define SPIMSP432E4_PQ2_SSI3XDAT0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 2, GPIO_PQ2_SSI3XDAT0) 306 #define SPIMSP432E4_PF1_SSI3XDAT0 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 1, GPIO_PF1_SSI3XDAT0) 311 #define SPIMSP432E4_PQ3_SSI3XDAT1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTQ, 3, GPIO_PQ3_SSI3XDAT1) 316 #define SPIMSP432E4_PF0_SSI3XDAT1 GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTF, 0, GPIO_PF0_SSI3XDAT1) 347 #define SPIMSP432E4_PIN_NO_CONFIG (0xFFFFFFFF) uint32_t activeChannel
Definition: SPIMSP432E4DMA.h:475
Definition: SPIMSP432E4DMA.h:458
uint32_t intNum
Definition: SPIMSP432E4DMA.h:424
uint32_t txDmaChannel
Definition: SPIMSP432E4DMA.h:437
uint32_t transferTimeout
Definition: SPIMSP432E4DMA.h:474
UDMAMSP432E4 Global configuration.
Definition: UDMAMSP432E4.h:143
Serial Peripheral Interface (SPI) Driver Interface.
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:584
uint32_t xdat1PinMask
Definition: SPIMSP432E4DMA.h:449
uDMA driver implementation for MSP432E4.
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:620
size_t framesTransferred
Definition: SPIMSP432E4DMA.h:468
uint16_t minDmaTransferSize
Definition: SPIMSP432E4DMA.h:440
SPIMSP432E4DMA Hardware attributes.
Definition: SPIMSP432E4DMA.h:420
uint32_t baseAddr
Definition: SPIMSP432E4DMA.h:422
UDMAMSP432E4_Handle dmaHandle
Definition: SPIMSP432E4DMA.h:462
uint32_t dataSize
Definition: SPIMSP432E4DMA.h:473
uint16_t defaultTxBufValue
Definition: SPIMSP432E4DMA.h:432
SPI_Mode spiMode
Definition: SPIMSP432E4DMA.h:480
size_t framesQueued
Definition: SPIMSP432E4DMA.h:467
size_t altTransferSize
Definition: SPIMSP432E4DMA.h:470
uint32_t intPriority
Definition: SPIMSP432E4DMA.h:426
uint32_t xdat0PinMask
Definition: SPIMSP432E4DMA.h:447
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:711
uint32_t bitRate
Definition: SPIMSP432E4DMA.h:472
uint16_t rxScratchBuf
Definition: SPIMSP432E4DMA.h:478
uint32_t busyBit
Definition: SPIMSP432E4DMA.h:476
SPI_Transaction * headPtr
Definition: SPIMSP432E4DMA.h:464
SemaphoreP_Handle transferComplete
Definition: SPIMSP432E4DMA.h:460
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:563
SPI_Mode
Definitions for various SPI modes of operation.
Definition: SPI.h:590
uint32_t rxDmaChannel
Definition: SPIMSP432E4DMA.h:435
HwiP_Handle hwiHandle
Definition: SPIMSP432E4DMA.h:459
uint16_t * scratchBufPtr
Definition: SPIMSP432E4DMA.h:429
uint32_t fssPinMask
Definition: SPIMSP432E4DMA.h:445
uint32_t clkPinMask
Definition: SPIMSP432E4DMA.h:443
SPI_CallbackFxn transferCallbackFxn
Definition: SPIMSP432E4DMA.h:461
SPI_Transaction * tailPtr
Definition: SPIMSP432E4DMA.h:465
const SPI_FxnTable SPIMSP432E4DMA_fxnTable
SPI_TransferMode transferMode
Definition: SPIMSP432E4DMA.h:481
bool isOpen
Definition: SPIMSP432E4DMA.h:484
size_t priTransferSize
Definition: SPIMSP432E4DMA.h:469
uint8_t format
Definition: SPIMSP432E4DMA.h:483