![]() |
![]() |
PRELIMINARY Comparator Driver Interface
WARNING These APIs are PRELIMINARY, and subject to change in the next few months.
The Comparator driver serves as the main interface for a typical RTOS application. Its purpose is to redirect the Comparator APIs to device specific implementations which are specified using a pointer to a Comparator_FxnTable. The device specific implementations are responsible for creating all the RTOS specific primitives to allow for thread-safe operation.
The Comparator driver is an analog driver that accepts a configuration of two analog input signals, compares those values, and then outputs high on the output signal if the positive input is more positive than that of the negative input terminal. This output signal can be configured in either inverted or non-inverted based off the user configuration.
Device specific capabilities such as output analog filters and programmable hysteresis are configured via the implementation specific hwAttrs configuration structure. This top level driver provides all APIs needed to provide a uniform and generic Comparator driver experience regardless of the underlying peripheral implementation.
This documentation provides a basic usage summary and a set of examples in the form of commented code fragments. Detailed descriptions of the APIs are provided in subsequent sections.
The Comparator driver is used to monitor two input analog signals and generate an output if the potential of the positive input terminal is greater than that of the negative input channel. This is commonly used for power supply supervision as well as precision slope analog-to-digital conversions. The code below sets up two arbitrary input signals to the Comparator driver and handles triggers of the voltage crossing in the appropriate callback function.
The Comparator driver supports two distinct methods of accessing/utilizing the underlying comparator peripheral's output signal: accessing the output level dynamically and providing a user callback function.
Accessing the output level directly can be done by calling the Comparator_getLevel() API after the driver has been successfully opened and started. This function will return a Comparator_OUTPUT_HIGH if the positive input terminal is more positive than the negative terminal and Comparator_OUTPUT_LOW if the reverse is true. If the output level of the comparator peripheral cannot be determined or the device is in an error state a value of Comparator_OUTPUT_NOT_AVAILABLE is returned.
The user callback functionality provides a way for the Comparator driver and its underlying implementation to communicate functional events as well as errors to the calling user application. If a non-null function pointer is provided to the callbackFxn configuration parameter a call to the callback will be invoked whenever a relevant event occurs in the driver. Primarily this callback will be invoked when the output of the comparator is triggered (or inversely triggered), however error events can also be passed through this callback.
Note that these programming models are compatible with each other and can be mixed accordingly. For example a user callback can be provided and the Comparator_getLevel() API can be called in any scenario.
Note that while the code above operates with a callback function provided, if a NULL value is given as the callbackFxn parameter the Comparator_getLevel() function can be invoked to dynamically get the output level of an initialized/started Comparator driver instance.
Refer to the Driver's Configuration section for driver configuration information.
#include <stdint.h>
Go to the source code of this file.
Data Structures | |
| struct | Comparator_Params |
| Comparator Parameters. More... | |
| struct | Comparator_FxnTable |
| The definition of a comparator function table that contains the required set of functions to control a specific comparator driver implementation. More... | |
| struct | Comparator_Config_ |
| Comparator driver's custom configuration structure. More... | |
Macros | |
| #define | Comparator_STATUS_RESERVED (-32) |
| #define | Comparator_STATUS_SUCCESS (0) |
| Successful status code. More... | |
| #define | Comparator_STATUS_ERROR (-1) |
| Generic error status code. More... | |
| #define | Comparator_EVENT_RESERVED (32) |
| #define | Comparator_EVENT_OUTPUT_TRIGGERED (1) |
| The comparator output triggered in the positive direction. More... | |
| #define | Comparator_EVENT_OUTPUT_INVERTED_TRIGGERED (2) |
| The comparator output triggered in the inverted direction. More... | |
| #define | Comparator_EVENT_ERROR (-1) |
| An error occurred with the underlying comparator driver. More... | |
Typedefs | |
| typedef struct Comparator_Config_ * | Comparator_Handle |
| A handle that is returned from a Comparator_open() call. More... | |
| typedef void(* | Comparator_CallBackFxn) (Comparator_Handle handle, int32_t event) |
| Comparator callback function. More... | |
| typedef void(* | Comparator_CloseFxn) (Comparator_Handle handle) |
| A function pointer to a driver specific implementation of Comparator_close(). More... | |
| typedef uint32_t(* | Comparator_GetLevelFxn) (Comparator_Handle handle) |
| A function pointer to a driver specific implementation of Comparator_getLevel(). More... | |
| typedef void(* | Comparator_InitFxn) (Comparator_Handle handle) |
| A function pointer to a driver specific implementation of Comparator_init(). More... | |
| typedef Comparator_Handle(* | Comparator_OpenFxn) (Comparator_Handle handle, Comparator_Params *params) |
| A function pointer to a driver specific implementation of Comparator_open(). More... | |
| typedef int32_t(* | Comparator_StartFxn) (Comparator_Handle handle) |
| A function pointer to a driver specific implementation of Comparator_start(). More... | |
| typedef void(* | Comparator_StopFxn) (Comparator_Handle handle) |
| A function pointer to a driver specific implementation of Comparator_stop(). More... | |
| typedef int32_t(* | Comparator_GetParamsFxn) (Comparator_Handle handle, Comparator_Params *params) |
| A function pointer to a driver specific implementation of Comparator_getParams(). More... | |
| typedef int32_t(* | Comparator_SetParamsFxn) (Comparator_Handle handle, Comparator_Params *params) |
| A function pointer to a driver specific implementation of Comparator_setParams(). More... | |
| typedef struct Comparator_Config_ | Comparator_Config |
| Comparator driver's custom configuration structure. More... | |
Enumerations | |
| enum | Comparator_OutputPolarity { Comparator_OUTPUT_NORMAL, Comparator_OUTPUT_INVERTED } |
| Comparator Output Polarity. More... | |
| enum | Comparator_OutputLevel { Comparator_OUTPUT_HIGH, Comparator_OUTPUT_LOW, Comparator_OUTPUT_NOT_AVAILABLE } |
| Comparator Output Level. More... | |
| enum | Comparator_InterruptLevel { Comparator_INTERRUPT_NONE, Comparator_INTERRUPT_RISING, Comparator_INTERRUPT_FALLING, Comparator_INTERRUPT_BOTH, Comparator_INTERRUPT_HIGH, Comparator_INTERRUPT_LOW } |
| Comparator Interrupt Level. More... | |
Functions | |
| void | Comparator_close (Comparator_Handle handle) |
| Function to close a Comparator driver instance. More... | |
| int_fast16_t | Comparator_control (Comparator_Handle handle, uint_fast16_t cmd, void *arg) |
| Function performs implementation specific features on a given Comparator_Handle. More... | |
| Comparator_OutputLevel | Comparator_getLevel (Comparator_Handle handle) |
| Function returns the level of the comparator output. The output level correlates to the polarity specified by the parameter passed into the Comparator_Params.outputPolarity parameter while opening the device with Comparator_open(). More... | |
| void | Comparator_init (void) |
| Function to initialize the Comparator driver. More... | |
| Comparator_Handle | Comparator_open (uint32_t index, Comparator_Params *params) |
| Function to initialize the Comparator peripheral. More... | |
| void | Comparator_Params_init (Comparator_Params *params) |
| Function to initialize the Comparator_Params structure to its default values. More... | |
| int32_t | Comparator_start (Comparator_Handle handle) |
| Function to start the comparator instance. More... | |
| void | Comparator_stop (Comparator_Handle handle) |
| Function to stop a comparator instance. If the comparator instance is already stopped this function has no effect. More... | |
| int32_t | Comparator_getParams (Comparator_Handle handle, Comparator_Params *params) |
| Function to get the parameters of a comparator instance. More... | |
| int32_t | Comparator_setParams (Comparator_Handle handle, Comparator_Params *params) |
| Function to get the parameters of a comparator instance. More... | |
| typedef struct Comparator_Config_* Comparator_Handle |
A handle that is returned from a Comparator_open() call.
| typedef void(* Comparator_CallBackFxn) (Comparator_Handle handle, int32_t event) |
Comparator callback function.
Callback from the Comparator driver. This will be called when the driver is setup with a callback function pointer provided to the Comparator_Params.callbackFxn parameter and is used to communicate events and errors to the calling application.
| [out] | handle | Comparator_Handle |
| [out] | event | Events that can occur as part of the Comparator driver operation. |
| typedef void(* Comparator_CloseFxn) (Comparator_Handle handle) |
A function pointer to a driver specific implementation of Comparator_close().
| typedef uint32_t(* Comparator_GetLevelFxn) (Comparator_Handle handle) |
A function pointer to a driver specific implementation of Comparator_getLevel().
| typedef void(* Comparator_InitFxn) (Comparator_Handle handle) |
A function pointer to a driver specific implementation of Comparator_init().
| typedef Comparator_Handle(* Comparator_OpenFxn) (Comparator_Handle handle, Comparator_Params *params) |
A function pointer to a driver specific implementation of Comparator_open().
| typedef int32_t(* Comparator_StartFxn) (Comparator_Handle handle) |
A function pointer to a driver specific implementation of Comparator_start().
| typedef void(* Comparator_StopFxn) (Comparator_Handle handle) |
A function pointer to a driver specific implementation of Comparator_stop().
| typedef int32_t(* Comparator_GetParamsFxn) (Comparator_Handle handle, Comparator_Params *params) |
A function pointer to a driver specific implementation of Comparator_getParams().
| typedef int32_t(* Comparator_SetParamsFxn) (Comparator_Handle handle, Comparator_Params *params) |
A function pointer to a driver specific implementation of Comparator_setParams().
| typedef struct Comparator_Config_ Comparator_Config |
Comparator driver's custom configuration structure.
Comparator Output Polarity.
This enum defines the polarity of the comparator output (inverted/normal)
Comparator Output Level.
This enum defines the level of the output. This level has a direct correlation to the by the outputPolarity parameter passed into the Comparator_Params while opening the device with Comparator_open().
Comparator Interrupt Level.
This enum defines the comparator output condition that will trigger an interrupt. Not all output conditions are supported on all devices, refer to the device documentation to see which interrupt levels are supported.
| void Comparator_close | ( | Comparator_Handle | handle | ) |
Function to close a Comparator driver instance.
| [in] | handle | A Comparator_Handle returned from Comparator_open(). |
| int_fast16_t Comparator_control | ( | Comparator_Handle | handle, |
| uint_fast16_t | cmd, | ||
| void * | arg | ||
| ) |
Function performs implementation specific features on a given Comparator_Handle.
| [in] | handle | A Comparator_Handle returned from Comparator_open(). |
| [in] | cmd | A command value defined by the driver specific implementation. |
| [in] | arg | A pointer to an optional R/W (read/write) argument that is accompanied with cmd. |
| Comparator_OutputLevel Comparator_getLevel | ( | Comparator_Handle | handle | ) |
Function returns the level of the comparator output. The output level correlates to the polarity specified by the parameter passed into the Comparator_Params.outputPolarity parameter while opening the device with Comparator_open().
| [in] | handle | A Comparator handle returned from Comparator_open(). |
| void Comparator_init | ( | void | ) |
Function to initialize the Comparator driver.
This function must also be called before any other Comparator driver APIs.
| Comparator_Handle Comparator_open | ( | uint32_t | index, |
| Comparator_Params * | params | ||
| ) |
Function to initialize the Comparator peripheral.
Function to initialize the Comparator peripheral specified by the particular index value.
| [in] | index | Index in the Comparator_Config[] array. |
| [in] | params | Pointer to an initialized Comparator_Params structure. If NULL, the default Comparator_Params values are used. |
| void Comparator_Params_init | ( | Comparator_Params * | params | ) |
Function to initialize the Comparator_Params structure to its default values.
| [in] | params | A pointer to Comparator_Params structure for initialization. |
Defaults values are:
| int32_t Comparator_start | ( | Comparator_Handle | handle | ) |
Function to start the comparator instance.
| [in] | handle | A Comparator_Handle returned from Comparator_open(). |
| Comparator_STATUS_SUCCESS | The comparator successfully started. |
| Comparator_STATUS_ERROR | The comparator failed to start. |
| void Comparator_stop | ( | Comparator_Handle | handle | ) |
Function to stop a comparator instance. If the comparator instance is already stopped this function has no effect.
| [in] | handle | A Comparator_Handle returned from Comparator_open(). |
| int32_t Comparator_getParams | ( | Comparator_Handle | handle, |
| Comparator_Params * | params | ||
| ) |
Function to get the parameters of a comparator instance.
| [in] | handle | A Comparator_Handle returned from Comparator_open(). |
| [in] | params | A pointer to a Comparator_Params structure to be filled with the current comparator settings. |
| Comparator_STATUS_SUCCESS | The params were obtained successfully. |
| Comparator_STATUS_ERROR | The params were unable to be obtained. |
| int32_t Comparator_setParams | ( | Comparator_Handle | handle, |
| Comparator_Params * | params | ||
| ) |
Function to get the parameters of a comparator instance.
| [in] | handle | A Comparator_Handle returned from Comparator_open(). |
| [in] | params | A pointer to a Comparator_Params structure holding the new comparator settings. |
| Comparator_STATUS_SUCCESS | The params were set successfully. |
| Comparator_STATUS_ERROR | The params were unable to be set. |