![]() |
![]() |
|
MSP432E4 DriverLib API Guide
1.11.00.03
|
#include <stdint.h>#include <stdbool.h>

Go to the source code of this file.
Macros | |
| #define | SYSEXC_INT_FP_IXC 0x00000020 |
| #define | SYSEXC_INT_FP_OFC 0x00000010 |
| #define | SYSEXC_INT_FP_UFC 0x00000008 |
| #define | SYSEXC_INT_FP_IOC 0x00000004 |
| #define | SYSEXC_INT_FP_DZC 0x00000002 |
| #define | SYSEXC_INT_FP_IDC 0x00000001 |
Functions | |
| void | SysExcIntRegister (void(*pfnHandler)(void)) |
| void | SysExcIntUnregister (void) |
| void | SysExcIntEnable (uint32_t ui32IntFlags) |
| void | SysExcIntDisable (uint32_t ui32IntFlags) |
| uint32_t | SysExcIntStatus (bool bMasked) |
| void | SysExcIntClear (uint32_t ui32IntFlags) |
| #define SYSEXC_INT_FP_IXC 0x00000020 |
| #define SYSEXC_INT_FP_OFC 0x00000010 |
| #define SYSEXC_INT_FP_UFC 0x00000008 |
| #define SYSEXC_INT_FP_IOC 0x00000004 |
| #define SYSEXC_INT_FP_DZC 0x00000002 |
| #define SYSEXC_INT_FP_IDC 0x00000001 |