![]() |
![]() |
USBLib API Guide
1.00.00.01
|
#include <usbdmsc.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const uint8_t | pui8Vendor [8] |
8 byte vendor string. More... | |
const uint8_t | pui8Product [16] |
16 byte vendor string. More... | |
const uint8_t | pui8Version [4] |
4 byte vendor string. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps. More... | |
const uint8_t | ui8PwrAttributes |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
const tMSCDMedia | sMediaFunctions |
const tUSBCallback | pfnEventCallback |
tMSCInstance | sPrivateData |
The structure used by the application to define operating parameters for the mass storage device.
const uint16_t tUSBDMSCDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
const uint16_t tUSBDMSCDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
const uint8_t tUSBDMSCDevice::pui8Vendor[8] |
8 byte vendor string.
const uint8_t tUSBDMSCDevice::pui8Product[16] |
16 byte vendor string.
const uint8_t tUSBDMSCDevice::pui8Version[4] |
4 byte vendor string.
const uint16_t tUSBDMSCDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps.
const uint8_t tUSBDMSCDevice::ui8PwrAttributes |
Indicates whether the device is self or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
const uint8_t* const* tUSBDMSCDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1), MSC Interface description string (language 1), Configuration description string (language 1).
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
Referenced by USBDMSCCompositeInit(), and USBDMSCInit().
const uint32_t tUSBDMSCDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be 1 + ((5 + (num HID strings)) * (num languages)).
const tMSCDMedia tUSBDMSCDevice::sMediaFunctions |
This structure holds the access functions for the media used by this instance of the mass storage class device. All of the functions in this structure are required to be filled out with valid functions.
Referenced by USBDMSCTerm().
const tUSBCallback tUSBDMSCDevice::pfnEventCallback |
This is the callback function for various events that occur during mass storage class operation.
tMSCInstance tUSBDMSCDevice::sPrivateData |
The private instance data for this device. This memory must remain accessible for as long as the MSC device is in use and must not be modified by any code outside the MSC class driver.
Referenced by USBDMSCCompositeInit(), USBDMSCMediaChange(), USBDMSCTerm(), and USBDSCSICommand().