![]() |
![]() |
USBLib API Guide
1.00.00.01
|
![]() |
Data Structures | |
struct | tUSBDGamepadInstance |
struct | tUSBDHIDGamepadDevice |
struct | PACKED |
USB_CDC_GET/SET_LINE_CODING request-specific data. More... | |
Macros | |
#define | NUM_HID_SECTIONS |
#define | USBDGAMEPAD_SUCCESS 0 |
The USBDHIDGamepadSendReport() call successfully scheduled the report. More... | |
#define | USBDGAMEPAD_TX_ERROR 1 |
#define | USBDGAMEPAD_NOT_CONFIGURED 2 |
The device is not currently configured and cannot perform any operations. More... | |
Enumerations | |
enum | tGamepadState { eHIDGamepadStateNotConnected, eHIDGamepadStateIdle, eHIDGamepadStateSending } |
Functions | |
tUSBDHIDGamepadDevice * | USBDHIDGamepadInit (uint32_t ui32Index, tUSBDHIDGamepadDevice *psGamepad) |
tUSBDHIDGamepadDevice * | USBDHIDGamepadCompositeInit (uint32_t ui32Index, tUSBDHIDGamepadDevice *psGamepad, tCompositeEntry *psCompEntry) |
uint32_t | USBDHIDGamepadSendReport (tUSBDHIDGamepadDevice *psHIDGamepad, void *pvReport, uint32_t ui32Size) |
void | USBDHIDGamepadTerm (tUSBDHIDGamepadDevice *psGamepad) |
#define NUM_HID_SECTIONS |
#define USBDGAMEPAD_SUCCESS 0 |
The USBDHIDGamepadSendReport() call successfully scheduled the report.
Referenced by USBDHIDGamepadSendReport().
#define USBDGAMEPAD_TX_ERROR 1 |
The USBDHIDGamepadSendReport() function could not send the report at this time.
Referenced by USBDHIDGamepadSendReport().
#define USBDGAMEPAD_NOT_CONFIGURED 2 |
The device is not currently configured and cannot perform any operations.
Referenced by USBDHIDGamepadSendReport().
enum tGamepadState |
tUSBDHIDGamepadDevice * USBDHIDGamepadInit | ( | uint32_t | ui32Index, |
tUSBDHIDGamepadDevice * | psGamepad | ||
) |
Initializes HID gamepad device operation for a given USB controller.
ui32Index | is the index of the USB controller that is to be initialized for HID gamepad device operation. |
psGamepad | points to a structure containing parameters customizing the operation of the HID gamepad device. |
An application that enables a USB HID gamepad interface to a USB host must call this function to initialize the USB controller and attach the gamepad device to the USB bus. This function performs all required USB initialization, and the device is ready for operation on the function return.
On successful completion, this function returns the modified psGamepad pointer passed to it or returns a NULL pointer if there was a problem. This pointer must be passed on all future calls to the HID gamepad device driver.
When a host connects and configures the device, the application callback receives USB_EVENT_CONNECTED, after which calls can be made to USBDHIDGamepadSendReport() to report changes to the gamepad interface to the USB host when it requests them.
References tUSBDHIDGamepadDevice::pfnCallback, tUSBDHIDGamepadDevice::ppui8StringDescriptors, tUSBDGamepadInstance::sHIDDevice, tUSBDHIDGamepadDevice::sPrivateData, and USBDHIDGamepadCompositeInit().
tUSBDHIDGamepadDevice * USBDHIDGamepadCompositeInit | ( | uint32_t | ui32Index, |
tUSBDHIDGamepadDevice * | psGamepad, | ||
tCompositeEntry * | psCompEntry | ||
) |
Initializes HID gamepad device operation for a given USB controller.
ui32Index | is the index of the USB controller that is to be initialized for HID gamepad device operation. |
psGamepad | points to a structure containing parameters customizing the operation of the HID gamepad device. |
psCompEntry | is the composite device entry to initialize when creating a composite device. |
This call is very similar to USBDHIDGamepadInit() except that it is used for initializing an instance of the HID gamepad device for use in a composite device. If this HID gamepad is part of a composite device, then the psCompEntry should point to the composite device entry to initialize. This entry is part of the array that is passed to the USBDCompositeInit() function to start up and complete configuration of a composite USB device.
References eHIDGamepadStateNotConnected, tUSBDGamepadInstance::iState, tUSBDHIDGamepadDevice::pfnCallback, tUSBDHIDDevice::pfnTxCallback, tUSBDHIDGamepadDevice::ppui8StringDescriptors, tUSBDHIDDevice::psReportIdle, tUSBDGamepadInstance::sHIDDevice, tUSBDHIDGamepadDevice::sPrivateData, tUSBDGamepadInstance::sReportIdle, tUSBDHIDGamepadDevice::ui16MaxPowermA, tUSBDHIDDevice::ui16MaxPowermA, tUSBDHIDGamepadDevice::ui16PID, tUSBDHIDDevice::ui16PID, tHIDReportIdle::ui16TimeTillNextmS, tUSBDHIDGamepadDevice::ui16VID, tUSBDHIDDevice::ui16VID, tHIDReportIdle::ui32TimeSinceReportmS, tHIDReportIdle::ui8Duration4mS, tUSBDHIDDevice::ui8NumInputReports, tUSBDHIDDevice::ui8Protocol, tUSBDHIDGamepadDevice::ui8PwrAttributes, tUSBDHIDDevice::ui8PwrAttributes, tHIDReportIdle::ui8ReportID, and tUSBDHIDDevice::ui8Subclass.
Referenced by USBDHIDGamepadInit().
uint32_t USBDHIDGamepadSendReport | ( | tUSBDHIDGamepadDevice * | psHIDGamepad, |
void * | pvReport, | ||
uint32_t | ui32Size | ||
) |
Schedules a report to be sent once the host requests more data.
psHIDGamepad | is the structure pointer that is returned from the USBDHIDGamepadCompositeInit() or USBDHIDGamepadInit() functions. |
pvReport | is the data to send to the host. |
ui32Size | is the number of bytes in the pvReport buffer. |
This call is made by an application to schedule data to be sent to the host when the host requests an update from the device. The application must then wait for a USB_EVENT_TX_COMPLETE event in the function provided in the pfnCallback pointer in the tUSBDHIDGamepadDevice structure before being able to send more data with this function. The pointer passed in the pvReport can be updated once this call returns as the data has been copied from the buffer. The function returns USBDGAMEPAD_SUCCESS if the transmission was successfully scheduled or USBDGAMEPAD_TX_ERROR if the report could not be sent at this time. If the call is made before the device is connected or ready to communicate with the host, then the function can return USBDGAMEPAD_NOT_CONFIGURED.
References eHIDGamepadStateNotConnected, eHIDGamepadStateSending, tUSBDGamepadInstance::iState, tUSBDGamepadInstance::sHIDDevice, tUSBDHIDGamepadDevice::sPrivateData, USBDGAMEPAD_NOT_CONFIGURED, USBDGAMEPAD_SUCCESS, USBDGAMEPAD_TX_ERROR, USBDHIDReportWrite(), and USBDHIDTxPacketAvailable().
void USBDHIDGamepadTerm | ( | tUSBDHIDGamepadDevice * | psGamepad | ) |
Shuts down the HID gamepad device.
psGamepad | is the pointer to the device instance structure as returned by USBDHIDGamepadInit() or USBDHIDGamepadCompositeInit(). |
This function terminates HID gamepad operation for the instance supplied and removes the device from the USB bus. Following this call, the psGamepad instance may not me used in any other call to the HID gamepad device other than to reinitialize by calling USBDHIDGamepadInit() or USBDHIDGamepadCompositeInit().
References eHIDGamepadStateNotConnected, tUSBDGamepadInstance::iState, tUSBDGamepadInstance::sHIDDevice, tUSBDHIDGamepadDevice::sPrivateData, and USBDHIDTerm().