![]() |
![]() |
Struct containing the parameters required for calculating the CRC of a data block. Default values can be set with CRC_Params_init. More...
#include <CRC.h>
Data Fields | |
CRC_ReturnBehavior | returnBehavior |
CRC_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
uint32_t | seed |
CRC_Polynomial | polynomial |
uint32_t | programmablePoly |
uint32_t | programmablePolyOrder |
CRC_DataSize | dataSize |
CRC_ByteSwap | byteSwapInput |
uint8_t | reverseInputBits |
uint8_t | invertOutputBits |
uint8_t | reverseOutputBits |
uint32_t | finalXorValue |
Struct containing the parameters required for calculating the CRC of a data block. Default values can be set with CRC_Params_init.
CRC_ReturnBehavior CRC_Params_::returnBehavior |
Blocking, callback, or polling return behavior
CRC_CallbackFxn CRC_Params_::callbackFxn |
Callback function pointer
uint32_t CRC_Params_::timeout |
Maximum time in ticks the driver will wait for hardware to become available. Also limits maximum operation time, but only in BLOCKING mode.
void* CRC_Params_::custom |
Custom argument used by driver implementation
uint32_t CRC_Params_::seed |
Typically 0x0000... or 0xFFFF... This value should always be the width of the polynomial.
CRC_Polynomial CRC_Params_::polynomial |
Which polynomial to use for calculation
uint32_t CRC_Params_::programmablePoly |
If programmable polynomials are supported, set the polynomial here
uint32_t CRC_Params_::programmablePolyOrder |
If programmable polynomials are supported, set the order of the polynomial here
CRC_DataSize CRC_Params_::dataSize |
Determines the width of the operation (i.e. is data consumed in 8, 16 or 32-bit blocks). Does not impact the width of the result, which is always the same as the polynomial order.
CRC_ByteSwap CRC_Params_::byteSwapInput |
If endianness processing is needed on the input.
uint8_t CRC_Params_::reverseInputBits |
This reverses the bits in the input register
uint8_t CRC_Params_::invertOutputBits |
This inverts the output bits of the final result
uint8_t CRC_Params_::reverseOutputBits |
This reverses the bits of the final result
uint32_t CRC_Params_::finalXorValue |
After calculation is complete, the result will be XORed with this field