![]() |
![]() |
The definition of a CAN function table that contains the required set of functions to control a specific CAN driver implementation. More...
#include <CAN.h>
Data Fields | |
CAN_CloseFxn | closeFxn |
CAN_ControlFxn | controlFxn |
CAN_InitFxn | initFxn |
CAN_OpenFxn | openFxn |
CAN_ReadFxn | readFxn |
CAN_WriteFxn | writeFxn |
CAN_TxMsgFxn | txMsgFxn |
The definition of a CAN function table that contains the required set of functions to control a specific CAN driver implementation.
CAN_CloseFxn CAN_FxnTable_::closeFxn |
Function to close the specified peripheral
CAN_ControlFxn CAN_FxnTable_::controlFxn |
Function to implementation specific control function
CAN_InitFxn CAN_FxnTable_::initFxn |
Function to initialize the given data object
CAN_OpenFxn CAN_FxnTable_::openFxn |
Function to open the specified peripheral
CAN_ReadFxn CAN_FxnTable_::readFxn |
Function to read from the specified peripheral
CAN_WriteFxn CAN_FxnTable_::writeFxn |
Function to write from the specified peripheral
CAN_TxMsgFxn CAN_FxnTable_::txMsgFxn |
Function to kick the transmitter