#include <stddef.h>
#include <stdint.h>
Go to the source code of this file.
§ CAN_EFF_FLAG
#define CAN_EFF_FLAG 0x80000000U |
SocketCAN compatible bit flag.
- See also
- CAN_frame
-
struct can_frame
§ CAN_RTR_FLAG
#define CAN_RTR_FLAG 0x40000000U |
SocketCAN compatible bit flag.
- See also
- CAN_frame
-
struct can_frame
§ CAN_ERR_FLAG
#define CAN_ERR_FLAG 0x20000000U |
SocketCAN compatible bit flag.
- See also
- CAN_frame
-
struct can_frame
§ CAN_SFF_MASK
#define CAN_SFF_MASK 0x000007FFU |
SocketCAN compatible bit mask.
- See also
- CAN_frame
-
struct can_frame
§ CAN_EFF_MASK
#define CAN_EFF_MASK 0x1FFFFFFFU |
SocketCAN compatible bit mask.
- See also
- CAN_frame
-
struct can_frame
§ CAN_ERR_MASK
#define CAN_ERR_MASK 0x1FFFFFFFU |
SocketCAN compatible bit mask.
- See also
- CAN_frame
-
struct can_frame
§ canid_t
CAN identifier structure.
bit 0-28 : CAN identifier (11/29 bit) bit 29 : error message frame flag (0 = data frame, 1 = error message) bit 30 : remote transmission request flag (1 = rtr frame) bit 31 : frame format flag (0 = standard 11 bit, 1 = extended 29 bit)