![]() |
![]() |
CRC driver implementation for MSP432E4.
============================================================================
The CRC header file should be included in an application as follows:
This driver supports the following CRCs:
This driver supports only the following size options. Data processing is only supported for CRC_DATA_SIZE_32BIT.
Go to the source code of this file.
Data Structures | |
struct | CRCMSP432E4_Object_ |
CRCMSP432E4 Hardware Attributes. More... | |
Typedefs | |
typedef struct CRCMSP432E4_Object_ | CRCMSP432E4_Object |
CRCMSP432E4 Hardware Attributes. More... | |
typedef struct CRCMSP432E4_Object_ CRCMSP432E4_Object |
CRCMSP432E4 Hardware Attributes.
The CRCMSP432E4 driver does not have any configurable hardware attributes. NULL should be used for the hwAttrs parameter of the CRC_Config struct.
CRCMSP432E4 Object
The application must not access any member variables of this structure!