Network Services API  2.60.01.06
Data Fields
SlNetSock_In6Addr_t Struct Reference

IpV6 or Ipv6 EUI64. More...

#include <ti/net/slnetsock.h>

Collaboration diagram for SlNetSock_In6Addr_t:
Collaboration graph

Data Fields

union {
   uint8_t   _S6_u8 [16]
 
   uint16_t   _S6_u16 [8]
 
   uint32_t   _S6_u32 [4]
 
} _S6_un
 

Detailed Description

IpV6 or Ipv6 EUI64.

Field Documentation

§ _S6_u8

uint8_t SlNetSock_In6Addr_t::_S6_u8[16]

§ _S6_u16

uint16_t SlNetSock_In6Addr_t::_S6_u16[8]

§ _S6_u32

uint32_t SlNetSock_In6Addr_t::_S6_u32[4]

§ _S6_un

union { ... } SlNetSock_In6Addr_t::_S6_un

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale