Network Services API  2.60.01.06
Data Structures | Macros | Typedefs | Enumerations | Functions
MQTT Client

The MQTTClient Module provides an easy-to-use API to enable constrained and deeply embedded micro-controller based products to interact with cloud or network based MQTT servers. The users of MQTTClient services, while benefiting from the abstraction of the MQTT protocol, will find them suitable for varied deployments of MQTT subscribers and/or publishers. More...

Data Structures

struct  MQTTClient_OperationMetaDataCB
 
struct  MQTTClient_RecvMetaDataCB
 
struct  MQTTClient_ConnParams
 
struct  MQTTClient_Params
 
struct  MQTTClient_SubscribeParams
 
struct  MQTTClient_UnsubscribeParams
 
struct  MQTTClient_Will
 

Macros

#define MQTTCLIENT_ERR_NETWORK   MQTT_PACKET_ERR_NETWORK
 
#define MQTTCLIENT_ERR_TIMEOUT   MQTT_PACKET_ERR_TIMEOUT
 
#define MQTTCLIENT_ERR_NET_OPS   MQTT_PACKET_ERR_NET_OPS
 
#define MQTTCLIENT_ERR_FNPARAM   MQTT_PACKET_ERR_FNPARAM
 
#define MQTTCLIENT_ERR_PKT_AVL   MQTT_PACKET_ERR_PKT_AVL
 
#define MQTTCLIENT_ERR_PKT_LEN   MQTT_PACKET_ERR_PKT_LEN
 
#define MQTTCLIENT_ERR_NOTCONN   MQTT_PACKET_ERR_NOTCONN
 
#define MQTTCLIENT_ERR_BADCALL   MQTT_PACKET_ERR_BADCALL
 
#define MQTTCLIENT_ERR_CONTENT   MQTT_PACKET_ERR_CONTENT
 
#define MQTTCLIENT_ERR_LIBQUIT   MQTT_PACKET_ERR_LIBQUIT
 
#define MQTTCLIENT_ERR_REMLSTN   MQTT_PACKET_ERR_REMLSTN
 
#define MQTTCLIENT_OPERATION_CONNACK   MQTT_CONNACK
 
#define MQTTCLIENT_OPERATION_EVT_PUBACK   MQTT_PUBACK
 
#define MQTTCLIENT_OPERATION_PUBCOMP   MQTT_PUBCOMP
 
#define MQTTCLIENT_OPERATION_SUBACK   MQTT_SUBACK
 
#define MQTTCLIENT_OPERATION_UNSUBACK   MQTT_UNSUBACK
 
#define MQTTCLIENT_NETCONN_IP4   MQTT_DEV_NETCONN_OPT_IP4
 
#define MQTTCLIENT_NETCONN_IP6   MQTT_DEV_NETCONN_OPT_IP6
 
#define MQTTCLIENT_NETCONN_URL   MQTT_DEV_NETCONN_OPT_URL
 
#define MQTTCLIENT_NETCONN_SEC   MQTT_DEV_NETCONN_OPT_SEC
 
#define MQTTCLIENT_NETCONN_SKIP_DOMAIN_NAME_VERIFICATION   MQTT_DEV_NETCONN_OPT_SKIP_DOMAIN_NAME_VERIFICATION
 
#define MQTTCLIENT_NETCONN_SKIP_CERTIFICATE_CATALOG_VERIFICATION   MQTT_DEV_NETCONN_OPT_SKIP_CERTIFICATE_CATALOG_VERIFICATION
 
#define MQTTCLIENT_NETCONN_SKIP_DATE_VERIFICATION   MQTT_DEV_NETCONN_OPT_SKIP_DATE_VERIFICATION
 

Typedefs

typedef struct MQTTClient_OperationMetaDataCB MQTTClient_OperationMetaDataCB
 
typedef struct MQTTClient_RecvMetaDataCB MQTTClient_RecvMetaDataCB
 
typedef struct MQTTClient_ConnParams MQTTClient_ConnParams
 
typedef struct MQTTClient_Params MQTTClient_Params
 
typedef void(* MQTTClient_CallBack) (int32_t event, void *metaData, uint32_t metaDateLen, void *data, uint32_t dataLen)
 
typedef void * MQTTClient_Handle
 
typedef struct MQTTClient_SubscribeParams MQTTClient_SubscribeParams
 
typedef struct MQTTClient_UnsubscribeParams MQTTClient_UnsubscribeParams
 
typedef struct MQTTClient_Will MQTTClient_Will
 

Enumerations

enum  MQTTClient_Option {
  MQTTClient_USER_NAME = 0,
  MQTTClient_PASSWORD = 1,
  MQTTClient_WILL_PARAM = 2,
  MQTTClient_CALLBACKS = 3,
  MQTTClient_KEEPALIVE_TIME = 4,
  MQTTClient_CLEAN_CONNECT = 5,
  MQTTClient_MAX_PARAM = 6
}
 
enum  MQTTClient_EventCB {
  MQTTClient_RECV_CB_EVENT = 0,
  MQTTClient_OPERATION_CB_EVENT = 1,
  MQTTClient_DISCONNECT_CB_EVENT = 2
}
 

Functions

MQTTClient_Handle MQTTClient_create (MQTTClient_CallBack defaultCallback, MQTTClient_Params *params)
 Create an MQTTClient instance. More...
 
int16_t MQTTClient_delete (MQTTClient_Handle handle)
 Delete an MQTTClient instance. More...
 
int16_t MQTTClient_run (MQTTClient_Handle handle)
 MQTTClient state machine. More...
 
int16_t MQTTClient_connect (MQTTClient_Handle handle)
 Connect to a broker. More...
 
int16_t MQTTClient_disconnect (MQTTClient_Handle handle)
 Disconnect from a broker. More...
 
int16_t MQTTClient_publish (MQTTClient_Handle handle, char *topic, uint16_t topicLen, char *msg, uint16_t msgLen, uint32_t flags)
 Publish a named message to the broker. More...
 
int16_t MQTTClient_subscribe (MQTTClient_Handle handle, MQTTClient_SubscribeParams *value, uint8_t numberOfTopics)
 Subscribe to a set of topics. More...
 
int16_t MQTTClient_unsubscribe (MQTTClient_Handle handle, MQTTClient_UnsubscribeParams *value, uint8_t numberOfTopics)
 Unsubscribe from a set of topics. More...
 
int16_t MQTTClient_set (MQTTClient_Handle handle, uint16_t option, void *value, uint16_t valueLength)
 Set client parameters. More...
 
int16_t MQTTClient_get (MQTTClient_Handle handle, uint16_t option, void *value, uint16_t valueLength)
 Get client parameters. More...
 

Detailed Description

The MQTTClient Module provides an easy-to-use API to enable constrained and deeply embedded micro-controller based products to interact with cloud or network based MQTT servers. The users of MQTTClient services, while benefiting from the abstraction of the MQTT protocol, will find them suitable for varied deployments of MQTT subscribers and/or publishers.

Description

In addition to providing services to the application, each MQTTClient instance encompasses a RTOS task to handle the incoming messages from the server. Such a dedicated context to process the messages from the server facilitates the apps to receive data (i.e. PUBLISH messages) even when they are blocked, whilst awaiting ACK for a previous transaction with the server. The receive task in the MQTT Layer can not be disabled anytime, however its system wide priority is configurable and can be set.

Some of the salient features of the MQTTClient Layer are

Configuration

The implementation enables the application developers to configure the following parameters using the compile line flags (-D option)

Typical Sequences:

Library Usage

To use the MQTTClient APIs, the application should include its header file as follows:

And, add the following MQTT library to the link line:

.../source/ti/net/mqtt/{toolchain}/{isa}/mqtt_{profile}.a

Macro Definition Documentation

§ MQTTCLIENT_ERR_NETWORK

#define MQTTCLIENT_ERR_NETWORK   MQTT_PACKET_ERR_NETWORK

Problem in network (sock err)

§ MQTTCLIENT_ERR_TIMEOUT

#define MQTTCLIENT_ERR_TIMEOUT   MQTT_PACKET_ERR_TIMEOUT

Net transaction has timed out

§ MQTTCLIENT_ERR_NET_OPS

#define MQTTCLIENT_ERR_NET_OPS   MQTT_PACKET_ERR_NET_OPS

Platform Net Ops un-available

§ MQTTCLIENT_ERR_FNPARAM

#define MQTTCLIENT_ERR_FNPARAM   MQTT_PACKET_ERR_FNPARAM

Invalid parameter(s) provided

§ MQTTCLIENT_ERR_PKT_AVL

#define MQTTCLIENT_ERR_PKT_AVL   MQTT_PACKET_ERR_PKT_AVL

No pkts are available in pool

§ MQTTCLIENT_ERR_PKT_LEN

#define MQTTCLIENT_ERR_PKT_LEN   MQTT_PACKET_ERR_PKT_LEN

Inadequate free buffer in pkt

§ MQTTCLIENT_ERR_NOTCONN

#define MQTTCLIENT_ERR_NOTCONN   MQTT_PACKET_ERR_NOTCONN

Lib isn't CONNECTED to server

§ MQTTCLIENT_ERR_BADCALL

#define MQTTCLIENT_ERR_BADCALL   MQTT_PACKET_ERR_BADCALL

Irrelevant call for LIB state

§ MQTTCLIENT_ERR_CONTENT

#define MQTTCLIENT_ERR_CONTENT   MQTT_PACKET_ERR_CONTENT

MSG / Data content has errors

§ MQTTCLIENT_ERR_LIBQUIT

#define MQTTCLIENT_ERR_LIBQUIT   MQTT_PACKET_ERR_LIBQUIT

Needs reboot library has quit

§ MQTTCLIENT_ERR_REMLSTN

#define MQTTCLIENT_ERR_REMLSTN   MQTT_PACKET_ERR_REMLSTN

No remote listener for socket

§ MQTTCLIENT_OPERATION_CONNACK

#define MQTTCLIENT_OPERATION_CONNACK   MQTT_CONNACK

CONNACK has been received from the server

§ MQTTCLIENT_OPERATION_EVT_PUBACK

#define MQTTCLIENT_OPERATION_EVT_PUBACK   MQTT_PUBACK

PUBACK has been received from the server

§ MQTTCLIENT_OPERATION_PUBCOMP

#define MQTTCLIENT_OPERATION_PUBCOMP   MQTT_PUBCOMP

PUBCOMP has been received from the server

§ MQTTCLIENT_OPERATION_SUBACK

#define MQTTCLIENT_OPERATION_SUBACK   MQTT_SUBACK

SUBACK has been received from the server

§ MQTTCLIENT_OPERATION_UNSUBACK

#define MQTTCLIENT_OPERATION_UNSUBACK   MQTT_UNSUBACK

UNSUBACK has been received from the server

§ MQTTCLIENT_NETCONN_IP4

#define MQTTCLIENT_NETCONN_IP4   MQTT_DEV_NETCONN_OPT_IP4

Assert for IPv4 connection

§ MQTTCLIENT_NETCONN_IP6

#define MQTTCLIENT_NETCONN_IP6   MQTT_DEV_NETCONN_OPT_IP6

Assert for IPv6 connection, otherwise IPv4

§ MQTTCLIENT_NETCONN_URL

#define MQTTCLIENT_NETCONN_URL   MQTT_DEV_NETCONN_OPT_URL

Server address is an URL and not IP address

§ MQTTCLIENT_NETCONN_SEC

#define MQTTCLIENT_NETCONN_SEC   MQTT_DEV_NETCONN_OPT_SEC

Connection to server must be secure (TLS)

§ MQTTCLIENT_NETCONN_SKIP_DOMAIN_NAME_VERIFICATION

#define MQTTCLIENT_NETCONN_SKIP_DOMAIN_NAME_VERIFICATION   MQTT_DEV_NETCONN_OPT_SKIP_DOMAIN_NAME_VERIFICATION

Assert to skip domain name verification

§ MQTTCLIENT_NETCONN_SKIP_CERTIFICATE_CATALOG_VERIFICATION

#define MQTTCLIENT_NETCONN_SKIP_CERTIFICATE_CATALOG_VERIFICATION   MQTT_DEV_NETCONN_OPT_SKIP_CERTIFICATE_CATALOG_VERIFICATION

Assert to skip certificate catalog verification

§ MQTTCLIENT_NETCONN_SKIP_DATE_VERIFICATION

#define MQTTCLIENT_NETCONN_SKIP_DATE_VERIFICATION   MQTT_DEV_NETCONN_OPT_SKIP_DATE_VERIFICATION

Assert to skip date verification

Typedef Documentation

§ MQTTClient_OperationMetaDataCB

§ MQTTClient_RecvMetaDataCB

§ MQTTClient_ConnParams

Secure Socket Parameters to open a secure connection

§ MQTTClient_Params

§ MQTTClient_CallBack

typedef void(* MQTTClient_CallBack) (int32_t event, void *metaData, uint32_t metaDateLen, void *data, uint32_t dataLen)

§ MQTTClient_Handle

typedef void* MQTTClient_Handle

§ MQTTClient_SubscribeParams

§ MQTTClient_UnsubscribeParams

§ MQTTClient_Will

Enumeration Type Documentation

§ MQTTClient_Option

Enumerator
MQTTClient_USER_NAME 
MQTTClient_PASSWORD 
MQTTClient_WILL_PARAM 
MQTTClient_CALLBACKS 
MQTTClient_KEEPALIVE_TIME 
MQTTClient_CLEAN_CONNECT 
MQTTClient_MAX_PARAM 

§ MQTTClient_EventCB

Enumerator
MQTTClient_RECV_CB_EVENT 
MQTTClient_OPERATION_CB_EVENT 
MQTTClient_DISCONNECT_CB_EVENT 

Function Documentation

§ MQTTClient_create()

MQTTClient_Handle MQTTClient_create ( MQTTClient_CallBack  defaultCallback,
MQTTClient_Params *  params 
)

Create an MQTTClient instance.

Parameters
[in]defaultCallbackasync event handler
[in]paramsparameters
Returns
Success Handle or Failure NULL
See also
MQTTClient_delete()

§ MQTTClient_delete()

int16_t MQTTClient_delete ( MQTTClient_Handle  handle)

Delete an MQTTClient instance.

Parameters
[in]handlehandle to the MQTTClient instance
Remarks
If the MQTTClient instance has an existing connection, it is dropped.
Returns
Success (0) or Failure (-1)
See also
MQTTClient_create()

§ MQTTClient_run()

int16_t MQTTClient_run ( MQTTClient_Handle  handle)

MQTTClient state machine.

This function need to be called from the context created by the user in case of OS environment.

Parameters
[in]handlehandle to the MQTTClient instance
Returns
Success (0) or Failure (Negative number)

§ MQTTClient_connect()

int16_t MQTTClient_connect ( MQTTClient_Handle  handle)

Connect to a broker.

Parameters
[in]handlehandle to the MQTTClient instance
Returns
Success (0) or Failure (Negative number)

§ MQTTClient_disconnect()

int16_t MQTTClient_disconnect ( MQTTClient_Handle  handle)

Disconnect from a broker.

Parameters
[in]handlehandle to the MQTTClient instance
Returns
Success (0) or Failure (Negative number)

§ MQTTClient_publish()

int16_t MQTTClient_publish ( MQTTClient_Handle  handle,
char *  topic,
uint16_t  topicLen,
char *  msg,
uint16_t  msgLen,
uint32_t  flags 
)

Publish a named message to the broker.

In addition to the PUBLISH specific parameters, the caller can indicate whether the routine should block until the time, the message has been acknowledged by the server. This is applicable only for non-QoS0 messages.

In case, the app has chosen not to await for the ACK from the server, the MQTT implementation will notify the app about the subscription through the callback routine.

Parameters
[in]handlehandle to the MQTTClient instance
[in]topictopic of the data to be published. It is NULL terminated.
[in]topicLentopic length.
[in]msgbinary data to be published
[in]msgLenlength of the msg
[in]flagsQOS define MQTT_PUBLISH_QOS_0, MQTT_PUBLISH_QOS_1 or MQTT_PUBLISH_QOS_2 use MQTT_PUBLISH_RETAIN is message should be retained
Returns
Success(transaction Message ID) or Failure(Negative number)

§ MQTTClient_subscribe()

int16_t MQTTClient_subscribe ( MQTTClient_Handle  handle,
MQTTClient_SubscribeParams *  value,
uint8_t  numberOfTopics 
)

Subscribe to a set of topics.

To receive data about a set of topics from the server, the app through this routine must subscribe to those topic names with the server. The caller can indicate whether the routine should block until a time, the message has been acknowledged by the server.

In case, the app has chosen not to await for the ACK from the server, the MQTT implementation will notify the app about the subscription through the callback routine.

Parameters
[in]handlehandle to the MQTTClient instance
[in]valuea pointer to a struct of subscribe parameters which hold:
Topic name to subscribe. It is a pointer to NULL terminated strings.
Qos value for the topic.
persistent session flag in order to enable or disable persistent session.
callback function which is optional - if NULL use the default callback
[in]numberOfTopicsnumber of such topics
Returns
Success(transaction Message ID) or Failure(Negative number)

§ MQTTClient_unsubscribe()

int16_t MQTTClient_unsubscribe ( MQTTClient_Handle  handle,
MQTTClient_UnsubscribeParams *  value,
uint8_t  numberOfTopics 
)

Unsubscribe from a set of topics.

The app should use this service to stop receiving data for the named topics from the server.

Parameters
[in]handlehandle to the MQTTClient instance
[in]valuetopics set of topics to be unsubscribed. It is an array of pointers to NULL terminated strings.
[in]numberOfTopicscount number of topics to be unsubscribed
Returns
Success(transaction Message ID) or Failure(Negative number)

§ MQTTClient_set()

int16_t MQTTClient_set ( MQTTClient_Handle  handle,
uint16_t  option,
void *  value,
uint16_t  valueLength 
)

Set client parameters.

This function can set different parameters to the client. Will message params, user name and password, keep alive time and clean/persistent session.

Parameters
[in]handlehandle to the MQTTClient instance
[in]optionDefine the actual option to set. Applicable values:
[in]valueSpecifies a value for the option
[in]valueLengthSpecifies the length of the value
Returns
Success(0) or Failure(Negative number)
See also
MQTTClient_Will

§ MQTTClient_get()

int16_t MQTTClient_get ( MQTTClient_Handle  handle,
uint16_t  option,
void *  value,
uint16_t  valueLength 
)

Get client parameters.

This function can get different parameters from the client. Will message params, user name and password, keep alive time and clean/persistent session.

Parameters
[in]handlehandle to the MQTTClient instance
[in]optionDefine the actual option to set. Applicable values:
[in]valueSpecifies a value for the option
[in]valueLengthSpecifies the length of the value
Returns
Success(0) or Failure(Negative number)
See also
MQTTClient_Will
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale