Data Fields
TimerMSP432E4_Object_ Struct Reference

TimerMSP432E4_Object. More...

#include <TimerMSP432E4.h>

Collaboration diagram for TimerMSP432E4_Object_:
Collaboration graph
[legend]

Data Fields

HwiP_Handle hwiHandle
 
Power_NotifyObj notifyObj
 
SemaphoreP_Handle timerSem
 
Timer_CallBackFxn callBack
 
Timer_Mode mode
 
uint32_t timer
 
uint32_t period
 
uint32_t prescaler
 
bool isRunning
 

Detailed Description

TimerMSP432E4_Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwiHandle

HwiP_Handle TimerMSP432E4_Object_::hwiHandle

§ notifyObj

Power_NotifyObj TimerMSP432E4_Object_::notifyObj

§ timerSem

SemaphoreP_Handle TimerMSP432E4_Object_::timerSem

§ callBack

Timer_CallBackFxn TimerMSP432E4_Object_::callBack

§ mode

Timer_Mode TimerMSP432E4_Object_::mode

§ timer

uint32_t TimerMSP432E4_Object_::timer

§ period

uint32_t TimerMSP432E4_Object_::period

§ prescaler

uint32_t TimerMSP432E4_Object_::prescaler

§ isRunning

bool TimerMSP432E4_Object_::isRunning

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale