![]() |
![]() |
|
Network Services API
2.60.00.07
|
Structure containing URL Handler components. More...
#include <ti/net/http/urlhandler.h>

Data Fields | |
| void * | params |
| Parameters needed for URL Handler instantiation. More... | |
| URLHandler_CreateFxn | create |
| URL Handler Create function. More... | |
| URLHandler_DeleteFxn | del |
| URL Handler Delete function. More... | |
| URLHandler_ProcessFxn | process |
| URL Handler Process function. More... | |
| URLHandler_ScanFieldFxn | scanField |
| Scan field function. More... | |
| void * | reserved1 |
| This field is reserved - set to NULL. More... | |
Structure containing URL Handler components.
This structure contains parameters needed for setup of a user- defined URLHandler object and pointers to associated user-defined URLHandler_* functions. The created HTTP Server maintains a table of this data structure for each unique URL Handler.
| void* URLHandler_Setup::params |
Parameters needed for URL Handler instantiation.
| URLHandler_CreateFxn URLHandler_Setup::create |
URL Handler Create function.
| URLHandler_DeleteFxn URLHandler_Setup::del |
URL Handler Delete function.
| URLHandler_ProcessFxn URLHandler_Setup::process |
URL Handler Process function.
| URLHandler_ScanFieldFxn URLHandler_Setup::scanField |
Scan field function.
| void* URLHandler_Setup::reserved1 |
This field is reserved - set to NULL.