Macros | Functions
Pwm_api

Macros

#define PWM_GEN_BADDR(_mod_, _gen_)   ((_mod_) + (_gen_))
 
#define PWM_GEN_EXT_BADDR(_mod_, _gen_)
 
#define PWM_OUT_BADDR(_mod_, _out_)   ((_mod_) + ((_out_) & 0xFFFFFFC0))
 
#define PWM_IS_OUTPUT_ODD(_out_)   ((_out_) & 0x00000001)
 

Functions

void PWMGenConfigure (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Config)
 
void PWMGenPeriodSet (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Period)
 
uint32_t PWMGenPeriodGet (uint32_t ui32Base, uint32_t ui32Gen)
 
void PWMGenEnable (uint32_t ui32Base, uint32_t ui32Gen)
 
void PWMGenDisable (uint32_t ui32Base, uint32_t ui32Gen)
 
void PWMPulseWidthSet (uint32_t ui32Base, uint32_t ui32PWMOut, uint32_t ui32Width)
 
uint32_t PWMPulseWidthGet (uint32_t ui32Base, uint32_t ui32PWMOut)
 
void PWMDeadBandEnable (uint32_t ui32Base, uint32_t ui32Gen, uint16_t ui16Rise, uint16_t ui16Fall)
 
void PWMDeadBandDisable (uint32_t ui32Base, uint32_t ui32Gen)
 
void PWMSyncUpdate (uint32_t ui32Base, uint32_t ui32GenBits)
 
void PWMSyncTimeBase (uint32_t ui32Base, uint32_t ui32GenBits)
 
void PWMOutputState (uint32_t ui32Base, uint32_t ui32PWMOutBits, bool bEnable)
 
void PWMOutputInvert (uint32_t ui32Base, uint32_t ui32PWMOutBits, bool bInvert)
 
void PWMOutputFaultLevel (uint32_t ui32Base, uint32_t ui32PWMOutBits, bool bDriveHigh)
 
void PWMOutputFault (uint32_t ui32Base, uint32_t ui32PWMOutBits, bool bFaultSuppress)
 
void PWMGenIntRegister (uint32_t ui32Base, uint32_t ui32Gen, void(*pfnIntHandler)(void))
 
void PWMGenIntUnregister (uint32_t ui32Base, uint32_t ui32Gen)
 
void PWMFaultIntRegister (uint32_t ui32Base, void(*pfnIntHandler)(void))
 
void PWMFaultIntUnregister (uint32_t ui32Base)
 
void PWMGenIntTrigEnable (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32IntTrig)
 
void PWMGenIntTrigDisable (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32IntTrig)
 
uint32_t PWMGenIntStatus (uint32_t ui32Base, uint32_t ui32Gen, bool bMasked)
 
void PWMGenIntClear (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Ints)
 
void PWMIntEnable (uint32_t ui32Base, uint32_t ui32GenFault)
 
void PWMIntDisable (uint32_t ui32Base, uint32_t ui32GenFault)
 
uint32_t PWMIntStatus (uint32_t ui32Base, bool bMasked)
 
void PWMFaultIntClearExt (uint32_t ui32Base, uint32_t ui32FaultInts)
 
void PWMGenFaultConfigure (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32MinFaultPeriod, uint32_t ui32FaultSenses)
 
void PWMGenFaultTriggerSet (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Group, uint32_t ui32FaultTriggers)
 
uint32_t PWMGenFaultTriggerGet (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Group)
 
uint32_t PWMGenFaultStatus (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Group)
 
void PWMGenFaultClear (uint32_t ui32Base, uint32_t ui32Gen, uint32_t ui32Group, uint32_t ui32FaultTriggers)
 
void PWMClockSet (uint32_t ui32Base, uint32_t ui32Config)
 
uint32_t PWMClockGet (uint32_t ui32Base)
 
void PWMOutputUpdateMode (uint32_t ui32Base, uint32_t ui32PWMOutBits, uint32_t ui32Mode)
 

Detailed Description

Macro Definition Documentation

§ PWM_GEN_BADDR

#define PWM_GEN_BADDR (   _mod_,
  _gen_ 
)    ((_mod_) + (_gen_))

§ PWM_GEN_EXT_BADDR

#define PWM_GEN_EXT_BADDR (   _mod_,
  _gen_ 
)
Value:
((_mod_) + PWM_GEN_EXT_0 + \
((_gen_) - PWM_GEN_0) * 2)
#define PWM_GEN_0
Definition: pwm.h:135
#define PWM_GEN_EXT_0
Definition: pwm.h:145

Referenced by PWMGenFaultClear(), PWMGenFaultConfigure(), and PWMGenFaultStatus().

§ PWM_OUT_BADDR

#define PWM_OUT_BADDR (   _mod_,
  _out_ 
)    ((_mod_) + ((_out_) & 0xFFFFFFC0))

§ PWM_IS_OUTPUT_ODD

#define PWM_IS_OUTPUT_ODD (   _out_)    ((_out_) & 0x00000001)

Function Documentation

§ PWMGenConfigure()

void PWMGenConfigure ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Config 
)

Configures a PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to configure. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Configis the configuration for the PWM generator.

This function is used to set the mode of operation for a PWM generator. The counting mode, synchronization mode, and debug behavior are all configured. After configuration, the generator is left in the disabled state.

A PWM generator can count in two different modes: count down mode or count up/down mode. In count down mode, it counts from a value down to zero, and then resets to the preset value, producing left-aligned PWM signals (that is, the rising edge of the two PWM signals produced by the generator occur at the same time). In count up/down mode, it counts up from zero to the preset value, counts back down to zero, and then repeats the process, producing center-aligned PWM signals (that is, the middle of the high/low period of the PWM signals produced by the generator occurs at the same time).

When the PWM generator parameters (period and pulse width) are modified, their effect on the output PWM signals can be delayed. In synchronous mode, the parameter updates are not applied until a synchronization event occurs. This mode allows multiple parameters to be modified and take effect simultaneously, instead of one at a time. Additionally, parameters to multiple PWM generators in synchronous mode can be updated simultaneously, allowing them to be treated as if they were a unified generator. In non-synchronous mode, the parameter updates are not delayed until a synchronization event. In either mode, the parameter updates only occur when the counter is at zero to help prevent oddly formed PWM signals during the update (that is, a PWM pulse that is too short or too long).

The PWM generator can either pause or continue running when the processor is stopped via the debugger. If configured to pause, it continues to count until it reaches zero, at which point it pauses until the processor is restarted. If configured to continue running, it keeps counting as if nothing had happened.

The ui32Config parameter contains the desired configuration. It is the logical OR of the following:

  • PWM_GEN_MODE_DOWN or PWM_GEN_MODE_UP_DOWN to specify the counting mode
  • PWM_GEN_MODE_SYNC or PWM_GEN_MODE_NO_SYNC to specify the counter load and comparator update synchronization mode
  • PWM_GEN_MODE_DBG_RUN or PWM_GEN_MODE_DBG_STOP to specify the debug behavior
  • PWM_GEN_MODE_GEN_NO_SYNC, PWM_GEN_MODE_GEN_SYNC_LOCAL, or PWM_GEN_MODE_GEN_SYNC_GLOBAL to specify the update synchronization mode for generator counting mode changes
  • PWM_GEN_MODE_DB_NO_SYNC, PWM_GEN_MODE_DB_SYNC_LOCAL, or PWM_GEN_MODE_DB_SYNC_GLOBAL to specify the deadband parameter synchronization mode
  • PWM_GEN_MODE_FAULT_LATCHED or PWM_GEN_MODE_FAULT_UNLATCHED to specify whether fault conditions are latched or not
  • PWM_GEN_MODE_FAULT_MINPER or PWM_GEN_MODE_FAULT_NO_MINPER to specify whether minimum fault period support is required
  • PWM_GEN_MODE_FAULT_EXT or PWM_GEN_MODE_FAULT_LEGACY to specify whether extended fault source selection support is enabled or not

Setting PWM_GEN_MODE_FAULT_MINPER allows an application to set the minimum duration of a PWM fault signal. Faults are signaled for at least this time even if the external fault pin deasserts earlier. Care should be taken when using this mode because during the fault signal period, the fault interrupt from the PWM generator remains asserted. The fault interrupt handler may, therefore, reenter immediately if it exits prior to expiration of the fault timer.

Note
Changes to the counter mode affect the period of the PWM signals produced. PWMGenPeriodSet() and PWMPulseWidthSet() should be called after any changes to the counter mode of a generator.
Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_CTL, PWM_O_X_GENA, PWM_O_X_GENB, PWM_X_CTL_CMPAUPD, PWM_X_CTL_CMPBUPD, PWM_X_CTL_DBCTLUPD_M, PWM_X_CTL_DBFALLUPD_M, PWM_X_CTL_DBRISEUPD_M, PWM_X_CTL_DEBUG, PWM_X_CTL_FLTSRC, PWM_X_CTL_GENAUPD_M, PWM_X_CTL_GENBUPD_M, PWM_X_CTL_LATCH, PWM_X_CTL_LOADUPD, PWM_X_CTL_MINFLTPER, PWM_X_CTL_MODE, PWM_X_GENA_ACTCMPAD_ZERO, PWM_X_GENA_ACTCMPAU_ONE, PWM_X_GENA_ACTLOAD_ONE, PWM_X_GENB_ACTCMPBD_ZERO, PWM_X_GENB_ACTCMPBU_ONE, and PWM_X_GENB_ACTLOAD_ONE.

§ PWMGenPeriodSet()

void PWMGenPeriodSet ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Period 
)

Sets the period of a PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to be modified. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Periodspecifies the period of PWM generator output, measured in clock ticks.

This function sets the period of the specified PWM generator block, where the period of the generator block is defined as the number of PWM clock ticks between pulses on the generator block zero signal.

Note
Any subsequent calls made to this function before an update occurs cause the previous values to be overwritten.
Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_CTL, PWM_O_X_LOAD, and PWM_X_CTL_MODE.

§ PWMGenPeriodGet()

uint32_t PWMGenPeriodGet ( uint32_t  ui32Base,
uint32_t  ui32Gen 
)

Gets the period of a PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to query. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.

This function gets the period of the specified PWM generator block. The period of the generator block is defined as the number of PWM clock ticks between pulses on the generator block zero signal.

If the update of the counter for the specified PWM generator has yet to be completed, the value returned may not be the active period. The value returned is the programmed period, measured in PWM clock ticks.

Returns
Returns the programmed period of the specified generator block in PWM clock ticks.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_CTL, PWM_O_X_LOAD, and PWM_X_CTL_MODE.

§ PWMGenEnable()

void PWMGenEnable ( uint32_t  ui32Base,
uint32_t  ui32Gen 
)

Enables the timer/counter for a PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to be enabled. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.

This function allows the PWM clock to drive the timer/counter for the specified generator block.

Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_CTL, and PWM_X_CTL_ENABLE.

§ PWMGenDisable()

void PWMGenDisable ( uint32_t  ui32Base,
uint32_t  ui32Gen 
)

Disables the timer/counter for a PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to be disabled. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.

This function blocks the PWM clock from driving the timer/counter for the specified generator block.

Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_CTL, and PWM_X_CTL_ENABLE.

§ PWMPulseWidthSet()

void PWMPulseWidthSet ( uint32_t  ui32Base,
uint32_t  ui32PWMOut,
uint32_t  ui32Width 
)

Sets the pulse width for the specified PWM output.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutis the PWM output to modify. This parameter must be one of PWM_OUT_0, PWM_OUT_1, PWM_OUT_2, PWM_OUT_3, PWM_OUT_4, PWM_OUT_5, PWM_OUT_6, or PWM_OUT_7.
ui32Widthspecifies the width of the positive portion of the pulse.

This function sets the pulse width for the specified PWM output, where the pulse width is defined as the number of PWM clock ticks.

Note
Any subsequent calls made to this function before an update occurs cause the previous values to be overwritten.
Returns
None.

References ASSERT, HWREG, PWM_IS_OUTPUT_ODD, PWM_O_X_CMPA, PWM_O_X_CMPB, PWM_O_X_CTL, PWM_O_X_LOAD, PWM_OUT_BADDR, and PWM_X_CTL_MODE.

§ PWMPulseWidthGet()

uint32_t PWMPulseWidthGet ( uint32_t  ui32Base,
uint32_t  ui32PWMOut 
)

Gets the pulse width of a PWM output.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutis the PWM output to query. This parameter must be one of PWM_OUT_0, PWM_OUT_1, PWM_OUT_2, PWM_OUT_3, PWM_OUT_4, PWM_OUT_5, PWM_OUT_6, or PWM_OUT_7.

This function gets the currently programmed pulse width for the specified PWM output. If the update of the comparator for the specified output has yet to be completed, the value returned may not be the active pulse width. The value returned is the programmed pulse width, measured in PWM clock ticks.

Returns
Returns the width of the pulse in PWM clock ticks.

References ASSERT, HWREG, PWM_IS_OUTPUT_ODD, PWM_O_X_CMPA, PWM_O_X_CMPB, PWM_O_X_CTL, PWM_O_X_LOAD, PWM_OUT_BADDR, and PWM_X_CTL_MODE.

§ PWMDeadBandEnable()

void PWMDeadBandEnable ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint16_t  ui16Rise,
uint16_t  ui16Fall 
)

Enables the PWM dead band output and sets the dead band delays.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to modify. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui16Risespecifies the width of delay from the rising edge.
ui16Fallspecifies the width of delay from the falling edge.

This function sets the dead bands for the specified PWM generator, where the dead bands are defined as the number of PWM clock ticks from the rising or falling edge of the generator's OutA signal. Note that this function causes the coupling of OutB to OutA.

Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_DBCTL, PWM_O_X_DBFALL, PWM_O_X_DBRISE, and PWM_X_DBCTL_ENABLE.

§ PWMDeadBandDisable()

void PWMDeadBandDisable ( uint32_t  ui32Base,
uint32_t  ui32Gen 
)

Disables the PWM dead band output.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to modify. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.

This function disables the dead band mode for the specified PWM generator. Doing so decouples the OutA and OutB signals.

Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_DBCTL, and PWM_X_DBCTL_ENABLE.

§ PWMSyncUpdate()

void PWMSyncUpdate ( uint32_t  ui32Base,
uint32_t  ui32GenBits 
)

Synchronizes all pending updates.

Parameters
ui32Baseis the base address of the PWM module.
ui32GenBitsare the PWM generator blocks to be updated. This parameter must be the logical OR of any of PWM_GEN_0_BIT, PWM_GEN_1_BIT, PWM_GEN_2_BIT, or PWM_GEN_3_BIT.

For the selected PWM generators, this function causes all queued updates to the period or pulse width to be applied the next time the corresponding counter becomes zero.

Returns
None.

References ASSERT, HWREG, PWM_GEN_0_BIT, PWM_GEN_1_BIT, PWM_GEN_2_BIT, PWM_GEN_3_BIT, and PWM_O_CTL.

§ PWMSyncTimeBase()

void PWMSyncTimeBase ( uint32_t  ui32Base,
uint32_t  ui32GenBits 
)

Synchronizes the counters in one or multiple PWM generator blocks.

Parameters
ui32Baseis the base address of the PWM module.
ui32GenBitsare the PWM generator blocks to be synchronized. This parameter must be the logical OR of any of PWM_GEN_0_BIT, PWM_GEN_1_BIT, PWM_GEN_2_BIT, or PWM_GEN_3_BIT.

For the selected PWM module, this function synchronizes the time base of the generator blocks by causing the specified generator counters to be reset to zero.

Returns
None.

References ASSERT, HWREG, PWM_GEN_0_BIT, PWM_GEN_1_BIT, PWM_GEN_2_BIT, PWM_GEN_3_BIT, and PWM_O_SYNC.

§ PWMOutputState()

void PWMOutputState ( uint32_t  ui32Base,
uint32_t  ui32PWMOutBits,
bool  bEnable 
)

Enables or disables PWM outputs.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutBitsare the PWM outputs to be modified. This parameter must be the logical OR of any of PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, or PWM_OUT_7_BIT.
bEnabledetermines if the signal is enabled or disabled.

This function enables or disables the selected PWM outputs. The outputs are selected using the parameter ui32PWMOutBits. The parameter bEnable determines the state of the selected outputs. If bEnable is true, then the selected PWM outputs are enabled, or placed in the active state. If bEnable is false, then the selected outputs are disabled or placed in the inactive state.

Returns
None.

References ASSERT, HWREG, PWM_O_ENABLE, PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, and PWM_OUT_7_BIT.

§ PWMOutputInvert()

void PWMOutputInvert ( uint32_t  ui32Base,
uint32_t  ui32PWMOutBits,
bool  bInvert 
)

Selects the inversion mode for PWM outputs.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutBitsare the PWM outputs to be modified. This parameter must be the logical OR of any of PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, or PWM_OUT_7_BIT.
bInvertdetermines if the signal is inverted or passed through.

This function is used to select the inversion mode for the selected PWM outputs. The outputs are selected using the parameter ui32PWMOutBits. The parameter bInvert determines the inversion mode for the selected outputs. If bInvert is true, this function causes the specified PWM output signals to be inverted or made active low. If bInvert is false, the specified outputs are passed through as is or made active high.

Returns
None.

References ASSERT, HWREG, PWM_O_INVERT, PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, and PWM_OUT_7_BIT.

§ PWMOutputFaultLevel()

void PWMOutputFaultLevel ( uint32_t  ui32Base,
uint32_t  ui32PWMOutBits,
bool  bDriveHigh 
)

Specifies the level of PWM outputs suppressed in response to a fault condition.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutBitsare the PWM outputs to be modified. This parameter must be the logical OR of any of PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, or PWM_OUT_7_BIT.
bDriveHighdetermines if the signal is driven high or low during an active fault condition.

This function determines whether a PWM output pin that is suppressed in response to a fault condition is driven high or low. The affected outputs are selected using the parameter ui32PWMOutBits. The parameter bDriveHigh determines the output level for the pins identified by ui32PWMOutBits. If bDriveHigh is true then the selected outputs are driven high when a fault is detected. If it is false, the pins are driven low.

In a fault condition, pins which have not been configured to be suppressed via a call to PWMOutputFault() are unaffected by this function.

Returns
None.

References ASSERT, HWREG, PWM_O_FAULTVAL, PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, and PWM_OUT_7_BIT.

§ PWMOutputFault()

void PWMOutputFault ( uint32_t  ui32Base,
uint32_t  ui32PWMOutBits,
bool  bFaultSuppress 
)

Specifies the state of PWM outputs in response to a fault condition.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutBitsare the PWM outputs to be modified. This parameter must be the logical OR of any of PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, or PWM_OUT_7_BIT.
bFaultSuppressdetermines if the signal is suppressed or passed through during an active fault condition.

This function sets the fault handling characteristics of the selected PWM outputs. The outputs are selected using the parameter ui32PWMOutBits. The parameter bFaultSuppress determines the fault handling characteristics for the selected outputs. If bFaultSuppress is true, then the selected outputs are made inactive. If bFaultSuppress is false, then the selected outputs are unaffected by the detected fault.

The state the affected output pins are driven to can be configured with PWMOutputFaultLevel(). If not configured, affected outputs are driven low on a fault condition.

Returns
None.

References ASSERT, HWREG, PWM_O_FAULT, PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, and PWM_OUT_7_BIT.

§ PWMGenIntRegister()

void PWMGenIntRegister ( uint32_t  ui32Base,
uint32_t  ui32Gen,
void(*)(void)  pfnIntHandler 
)

Registers an interrupt handler for the specified PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator in question. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
pfnIntHandleris a pointer to the function to be called when the PWM generator interrupt occurs.

This function ensures that the interrupt handler specified by pfnIntHandler is called when an interrupt is detected for the specified PWM generator block. This function also enables the corresponding PWM generator interrupt in the interrupt controller; individual generator interrupts and interrupt sources must be enabled with PWMIntEnable() and PWMGenIntTrigEnable().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References ASSERT.

§ PWMGenIntUnregister()

void PWMGenIntUnregister ( uint32_t  ui32Base,
uint32_t  ui32Gen 
)

Removes an interrupt handler for the specified PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator in question. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.

This function unregisters the interrupt handler for the specified PWM generator block. This function also disables the corresponding PWM generator interrupt in the interrupt controller; individual generator interrupts and interrupt sources must be disabled with PWMIntDisable() and PWMGenIntTrigDisable().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References ASSERT.

§ PWMFaultIntRegister()

void PWMFaultIntRegister ( uint32_t  ui32Base,
void(*)(void)  pfnIntHandler 
)

Registers an interrupt handler for a fault condition detected in a PWM module.

Parameters
ui32Baseis the base address of the PWM module.
pfnIntHandleris a pointer to the function to be called when the PWM fault interrupt occurs.

This function ensures that the interrupt handler specified by pfnIntHandler is called when a fault interrupt is detected for the selected PWM module. This function also enables the PWM fault interrupt in the NVIC; the PWM fault interrupt must also be enabled at the module level using PWMIntEnable().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References ASSERT.

§ PWMFaultIntUnregister()

void PWMFaultIntUnregister ( uint32_t  ui32Base)

Removes the PWM fault condition interrupt handler.

Parameters
ui32Baseis the base address of the PWM module.

This function removes the interrupt handler for a PWM fault interrupt from the selected PWM module. This function also disables the PWM fault interrupt in the NVIC; the PWM fault interrupt must also be disabled at the module level using PWMIntDisable().

See also
IntRegister() for important information about registering interrupt handlers.
Returns
None.

References ASSERT.

§ PWMGenIntTrigEnable()

void PWMGenIntTrigEnable ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32IntTrig 
)

Enables interrupts and triggers for the specified PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to have interrupts and triggers enabled. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32IntTrigspecifies the interrupts and triggers to be enabled.

This function unmasks the specified interrupt(s) and trigger(s) by setting the specified bits of the interrupt/trigger enable register for the specified PWM generator. The ui32IntTrig parameter is the logical OR of PWM_INT_CNT_ZERO, PWM_INT_CNT_LOAD, PWM_INT_CNT_AU, PWM_INT_CNT_AD, PWM_INT_CNT_BU, PWM_INT_CNT_BD, PWM_TR_CNT_ZERO, PWM_TR_CNT_LOAD, PWM_TR_CNT_AU, PWM_TR_CNT_AD, PWM_TR_CNT_BU, or PWM_TR_CNT_BD.

Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_INT_CNT_AD, PWM_INT_CNT_AU, PWM_INT_CNT_BD, PWM_INT_CNT_BU, PWM_INT_CNT_LOAD, PWM_INT_CNT_ZERO, PWM_O_X_INTEN, PWM_TR_CNT_AD, PWM_TR_CNT_AU, PWM_TR_CNT_BD, PWM_TR_CNT_BU, PWM_TR_CNT_LOAD, and PWM_TR_CNT_ZERO.

§ PWMGenIntTrigDisable()

void PWMGenIntTrigDisable ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32IntTrig 
)

Disables interrupts for the specified PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to have interrupts and triggers disabled. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32IntTrigspecifies the interrupts and triggers to be disabled.

This function masks the specified interrupt(s) and trigger(s) by clearing the specified bits of the interrupt/trigger enable register for the specified PWM generator. The ui32IntTrig parameter is the logical OR of PWM_INT_CNT_ZERO, PWM_INT_CNT_LOAD, PWM_INT_CNT_AU, PWM_INT_CNT_AD, PWM_INT_CNT_BU, PWM_INT_CNT_BD, PWM_TR_CNT_ZERO, PWM_TR_CNT_LOAD, PWM_TR_CNT_AU, PWM_TR_CNT_AD, PWM_TR_CNT_BU, or PWM_TR_CNT_BD.

Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_INT_CNT_AD, PWM_INT_CNT_AU, PWM_INT_CNT_BD, PWM_INT_CNT_BU, PWM_INT_CNT_LOAD, PWM_INT_CNT_ZERO, PWM_O_X_INTEN, PWM_TR_CNT_AD, PWM_TR_CNT_AU, PWM_TR_CNT_BD, PWM_TR_CNT_BU, PWM_TR_CNT_LOAD, and PWM_TR_CNT_ZERO.

§ PWMGenIntStatus()

uint32_t PWMGenIntStatus ( uint32_t  ui32Base,
uint32_t  ui32Gen,
bool  bMasked 
)

Gets interrupt status for the specified PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to query. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
bMaskedspecifies whether masked or raw interrupt status is returned.

If bMasked is set as true, then the masked interrupt status is returned; otherwise, the raw interrupt status is returned.

Returns
Returns the contents of the interrupt status register or the contents of the raw interrupt status register for the specified PWM generator.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_O_X_ISC, and PWM_O_X_RIS.

§ PWMGenIntClear()

void PWMGenIntClear ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Ints 
)

Clears the specified interrupt(s) for the specified PWM generator block.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator to query. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Intsspecifies the interrupts to be cleared.

This function clears the specified interrupt(s) by writing a 1 to the specified bits of the interrupt status register for the specified PWM generator. The ui32Ints parameter is the logical OR of PWM_INT_CNT_ZERO, PWM_INT_CNT_LOAD, PWM_INT_CNT_AU, PWM_INT_CNT_AD, PWM_INT_CNT_BU, or PWM_INT_CNT_BD.

Note
Because there is a write buffer in the Cortex-M processor, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately reentered (because the interrupt controller still sees the interrupt source asserted).
Returns
None.

References ASSERT, HWREG, PWM_GEN_BADDR, PWM_INT_CNT_AD, PWM_INT_CNT_AU, PWM_INT_CNT_BD, PWM_INT_CNT_BU, PWM_INT_CNT_LOAD, PWM_INT_CNT_ZERO, and PWM_O_X_ISC.

§ PWMIntEnable()

void PWMIntEnable ( uint32_t  ui32Base,
uint32_t  ui32GenFault 
)

Enables generator and fault interrupts for a PWM module.

Parameters
ui32Baseis the base address of the PWM module.
ui32GenFaultcontains the interrupts to be enabled. This parameter must be a logical OR of any of PWM_INT_GEN_0, PWM_INT_GEN_1, PWM_INT_GEN_2, PWM_INT_GEN_3, PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, or PWM_INT_FAULT3.

This function unmasks the specified interrupt(s) by setting the specified bits of the interrupt enable register for the selected PWM module.

Returns
None.

References ASSERT, HWREG, PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, PWM_INT_FAULT3, PWM_INT_GEN_0, PWM_INT_GEN_1, PWM_INT_GEN_2, PWM_INT_GEN_3, and PWM_O_INTEN.

§ PWMIntDisable()

void PWMIntDisable ( uint32_t  ui32Base,
uint32_t  ui32GenFault 
)

Disables generator and fault interrupts for a PWM module.

Parameters
ui32Baseis the base address of the PWM module.
ui32GenFaultcontains the interrupts to be disabled. This parameter must be a logical OR of any of PWM_INT_GEN_0, PWM_INT_GEN_1, PWM_INT_GEN_2, PWM_INT_GEN_3, PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, or PWM_INT_FAULT3.

This function masks the specified interrupt(s) by clearing the specified bits of the interrupt enable register for the selected PWM module.

Returns
None.

References ASSERT, HWREG, PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, PWM_INT_FAULT3, PWM_INT_GEN_0, PWM_INT_GEN_1, PWM_INT_GEN_2, PWM_INT_GEN_3, and PWM_O_INTEN.

§ PWMIntStatus()

uint32_t PWMIntStatus ( uint32_t  ui32Base,
bool  bMasked 
)

Gets the interrupt status for a PWM module.

Parameters
ui32Baseis the base address of the PWM module.
bMaskedspecifies whether masked or raw interrupt status is returned.

If bMasked is set as true, then the masked interrupt status is returned; otherwise, the raw interrupt status is returned.

Returns
The current interrupt status, enumerated as a bit field of PWM_INT_GEN_0, PWM_INT_GEN_1, PWM_INT_GEN_2, PWM_INT_GEN_3, PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, and PWM_INT_FAULT3.

References ASSERT, HWREG, PWM_O_ISC, and PWM_O_RIS.

§ PWMFaultIntClearExt()

void PWMFaultIntClearExt ( uint32_t  ui32Base,
uint32_t  ui32FaultInts 
)

Clears the fault interrupt for a PWM module.

Parameters
ui32Baseis the base address of the PWM module.
ui32FaultIntsspecifies the fault interrupts to clear.

This function clears one or more fault interrupts by writing to the appropriate bit of the PWM interrupt status register. The parameter ui32FaultInts must be the logical OR of any of PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, or PWM_INT_FAULT3.

The fault interrupts are derived by performing a logical OR of each of the configured fault trigger signals for a given generator. Therefore, these interrupts are not directly related to the four possible FAULTn inputs to the device but indicate that a fault has been signaled to one of the four possible PWM generators.

Note
Because there is a write buffer in the Cortex-M processor, it may take several clock cycles before the interrupt source is actually cleared. Therefore, it is recommended that the interrupt source be cleared early in the interrupt handler (as opposed to the very last action) to avoid returning from the interrupt handler before the interrupt source is actually cleared. Failure to do so may result in the interrupt handler being immediately reentered (because the interrupt controller still sees the interrupt source asserted).
Returns
None.

References ASSERT, HWREG, PWM_INT_FAULT0, PWM_INT_FAULT1, PWM_INT_FAULT2, PWM_INT_FAULT3, and PWM_O_ISC.

§ PWMGenFaultConfigure()

void PWMGenFaultConfigure ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32MinFaultPeriod,
uint32_t  ui32FaultSenses 
)

Configures the minimum fault period and fault pin senses for a given PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator for which fault configuration is being set. This function must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32MinFaultPeriodis the minimum fault active period expressed in PWM clock cycles.
ui32FaultSensesindicates which sense of each FAULT input should be considered the ``asserted'' state. Valid values are logical OR combinations of PWM_FAULTn_SENSE_HIGH and PWM_FAULTn_SENSE_LOW.

This function configures the minimum fault period for a given generator along with the sense of each of the 4 possible fault inputs. The minimum fault period is expressed in PWM clock cycles and takes effect only if PWMGenConfigure() is called with flag PWM_GEN_MODE_FAULT_PER set in the ui32Config parameter. When a fault input is asserted, the minimum fault period timer ensures that it remains asserted for at least the number of clock cycles specified.

Returns
None.

References ASSERT, HWREG, PWM_FAULT0_SENSE_HIGH, PWM_FAULT0_SENSE_LOW, PWM_FAULT1_SENSE_HIGH, PWM_FAULT1_SENSE_LOW, PWM_FAULT2_SENSE_HIGH, PWM_FAULT2_SENSE_LOW, PWM_FAULT3_SENSE_HIGH, PWM_FAULT3_SENSE_LOW, PWM_GEN_BADDR, PWM_GEN_EXT_BADDR, PWM_O_X_FLTSEN, PWM_O_X_MINFLTPER, and PWM_X_MINFLTPER_M.

§ PWMGenFaultTriggerSet()

void PWMGenFaultTriggerSet ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Group,
uint32_t  ui32FaultTriggers 
)

Configures the set of fault triggers for a given PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator for which fault triggers are being set. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Groupindicates the subset of possible faults that are to be configured. This parameter must be PWM_FAULT_GROUP_0 or PWM_FAULT_GROUP_1.
ui32FaultTriggersdefines the set of inputs that are to contribute towards generation of the fault signal to the given PWM generator. For PWM_FAULT_GROUP_0, this is the logical OR of PWM_FAULT_FAULT0, PWM_FAULT_FAULT1, PWM_FAULT_FAULT2, or PWM_FAULT_FAULT3. For PWM_FAULT_GROUP_1, this is the logical OR of PWM_FAULT_DCMP0, PWM_FAULT_DCMP1, PWM_FAULT_DCMP2, PWM_FAULT_DCMP3, PWM_FAULT_DCMP4, PWM_FAULT_DCMP5, PWM_FAULT_DCMP6, or PWM_FAULT_DCMP7.

This function allows selection of the set of fault inputs that is combined to generate a fault condition to a given PWM generator. By default, all generators use only FAULT0 (for backwards compatibility) but if PWMGenConfigure() is called with flag PWM_GEN_MODE_FAULT_SRC in the ui32Config parameter, extended fault handling is enabled and this function must be called to configure the fault triggers.

The fault signal to the PWM generator is generated by ORing together each of the signals specified in the ui32FaultTriggers parameter after having adjusted the sense of each FAULTn input based on the configuration previously set using a call to PWMGenFaultConfigure().

Returns
None.

References ASSERT, HWREG, PWM_FAULT_DCMP0, PWM_FAULT_DCMP1, PWM_FAULT_DCMP2, PWM_FAULT_DCMP3, PWM_FAULT_DCMP4, PWM_FAULT_DCMP5, PWM_FAULT_DCMP6, PWM_FAULT_DCMP7, PWM_FAULT_FAULT0, PWM_FAULT_FAULT1, PWM_FAULT_FAULT2, PWM_FAULT_FAULT3, PWM_FAULT_GROUP_0, PWM_FAULT_GROUP_1, PWM_GEN_BADDR, PWM_O_X_FLTSRC0, and PWM_O_X_FLTSRC1.

§ PWMGenFaultTriggerGet()

uint32_t PWMGenFaultTriggerGet ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Group 
)

Returns the set of fault triggers currently configured for a given PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator for which fault triggers are being queried. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Groupindicates the subset of faults that are being queried. This parameter must be PWM_FAULT_GROUP_0 or PWM_FAULT_GROUP_1.

This function allows an application to query the current set of inputs that contribute to the generation of a fault condition to a given PWM generator.

Returns
Returns the current fault triggers configured for the fault group provided. For PWM_FAULT_GROUP_0, the returned value is a logical OR of PWM_FAULT_FAULT0, PWM_FAULT_FAULT1, PWM_FAULT_FAULT2, or PWM_FAULT_FAULT3. For PWM_FAULT_GROUP_1, the return value is the logical OR of PWM_FAULT_DCMP0, PWM_FAULT_DCMP1, PWM_FAULT_DCMP2, PWM_FAULT_DCMP3, PWM_FAULT_DCMP4, PWM_FAULT_DCMP5, PWM_FAULT_DCMP6, or PWM_FAULT_DCMP7.

References ASSERT, HWREG, PWM_FAULT_GROUP_0, PWM_FAULT_GROUP_1, PWM_GEN_BADDR, PWM_O_X_FLTSRC0, and PWM_O_X_FLTSRC1.

§ PWMGenFaultStatus()

uint32_t PWMGenFaultStatus ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Group 
)

Returns the current state of the fault triggers for a given PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator for which fault trigger states are being queried. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Groupindicates the subset of faults that are being queried. This parameter must be PWM_FAULT_GROUP_0 or PWM_FAULT_GROUP_1.

This function allows an application to query the current state of each of the fault trigger inputs to a given PWM generator. The current state of each fault trigger input is returned unless PWMGenConfigure() has previously been called with flag PWM_GEN_MODE_FAULT_LATCHED in the ui32Config parameter, in which case the returned status is the latched fault trigger status.

If latched faults are configured, the application must call PWMGenFaultClear() to clear each trigger.

Returns
Returns the current state of the fault triggers for the given PWM generator. A set bit indicates that the associated trigger is active. For PWM_FAULT_GROUP_0, the returned value is a logical OR of PWM_FAULT_FAULT0, PWM_FAULT_FAULT1, PWM_FAULT_FAULT2, or PWM_FAULT_FAULT3. For PWM_FAULT_GROUP_1, the return value is the logical OR of PWM_FAULT_DCMP0, PWM_FAULT_DCMP1, PWM_FAULT_DCMP2, PWM_FAULT_DCMP3, PWM_FAULT_DCMP4, PWM_FAULT_DCMP5, PWM_FAULT_DCMP6, or PWM_FAULT_DCMP7.

References ASSERT, HWREG, PWM_FAULT_GROUP_0, PWM_FAULT_GROUP_1, PWM_GEN_EXT_BADDR, PWM_O_X_FLTSTAT0, and PWM_O_X_FLTSTAT1.

§ PWMGenFaultClear()

void PWMGenFaultClear ( uint32_t  ui32Base,
uint32_t  ui32Gen,
uint32_t  ui32Group,
uint32_t  ui32FaultTriggers 
)

Clears one or more latched fault triggers for a given PWM generator.

Parameters
ui32Baseis the base address of the PWM module.
ui32Genis the PWM generator for which fault trigger states are being queried. This parameter must be one of PWM_GEN_0, PWM_GEN_1, PWM_GEN_2, or PWM_GEN_3.
ui32Groupindicates the subset of faults that are being queried. This parameter must be PWM_FAULT_GROUP_0 or PWM_FAULT_GROUP_1.
ui32FaultTriggersis the set of fault triggers which are to be cleared.

This function allows an application to clear the fault triggers for a given PWM generator. This function is only required if PWMGenConfigure() has previously been called with flag PWM_GEN_MODE_FAULT_LATCHED in parameter ui32Config.

Returns
None.

References ASSERT, HWREG, PWM_FAULT_DCMP0, PWM_FAULT_DCMP1, PWM_FAULT_DCMP2, PWM_FAULT_DCMP3, PWM_FAULT_DCMP4, PWM_FAULT_DCMP5, PWM_FAULT_DCMP6, PWM_FAULT_DCMP7, PWM_FAULT_FAULT0, PWM_FAULT_FAULT1, PWM_FAULT_FAULT2, PWM_FAULT_FAULT3, PWM_FAULT_GROUP_0, PWM_FAULT_GROUP_1, PWM_GEN_EXT_BADDR, PWM_O_X_FLTSTAT0, and PWM_O_X_FLTSTAT1.

§ PWMClockSet()

void PWMClockSet ( uint32_t  ui32Base,
uint32_t  ui32Config 
)

Sets the PWM clock configuration.

Parameters
ui32Baseis the base address of the PWM module.
ui32Configis the configuration for the PWM clock; it must be one of PWM_SYSCLK_DIV_1, PWM_SYSCLK_DIV_2, PWM_SYSCLK_DIV_4, PWM_SYSCLK_DIV_8, PWM_SYSCLK_DIV_16, PWM_SYSCLK_DIV_32, or PWM_SYSCLK_DIV_64.

This function sets the PWM clock divider as the PWM clock source. It also configures the clock frequency to the PWM module as a division of the system clock. This clock is used by the PWM module to generate PWM signals; its rate forms the basis for all PWM signals.

Note
The clocking of the PWM is dependent upon the system clock rate as configured by SysCtlClockFreqSet().
Returns
None.

References ASSERT, HWREG, PWM_CC_PWMDIV_M, PWM_CC_USEPWM, PWM_O_CC, PWM_SYSCLK_DIV_16, PWM_SYSCLK_DIV_2, PWM_SYSCLK_DIV_32, PWM_SYSCLK_DIV_4, PWM_SYSCLK_DIV_64, and PWM_SYSCLK_DIV_8.

§ PWMClockGet()

uint32_t PWMClockGet ( uint32_t  ui32Base)

Gets the current PWM clock configuration.

Parameters
ui32Baseis the base address of the PWM module.

This function returns the current PWM clock configuration.

Returns
Returns the current PWM clock configuration; is one of PWM_SYSCLK_DIV_1, PWM_SYSCLK_DIV_2, PWM_SYSCLK_DIV_4, PWM_SYSCLK_DIV_8, PWM_SYSCLK_DIV_16, PWM_SYSCLK_DIV_32, or PWM_SYSCLK_DIV_64.

References ASSERT, HWREG, PWM_CC_PWMDIV_M, PWM_CC_USEPWM, PWM_O_CC, and PWM_SYSCLK_DIV_1.

§ PWMOutputUpdateMode()

void PWMOutputUpdateMode ( uint32_t  ui32Base,
uint32_t  ui32PWMOutBits,
uint32_t  ui32Mode 
)

Sets the update mode or synchronization mode to the PWM outputs.

Parameters
ui32Baseis the base address of the PWM module.
ui32PWMOutBitsare the PWM outputs to be modified. This parameter must be the logical OR of any of PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, or PWM_OUT_7_BIT.
ui32Modespecifies the enable update mode to use when enabling or disabling PWM outputs.

This function sets one of three possible update modes to enable or disable the requested PWM outputs. The ui32Mode parameter controls when changes made via calls to PWMOutputState() take effect. Possible values are:

  • PWM_OUTPUT_MODE_NO_SYNC, which enables/disables changes to take effect immediately.
  • PWM_OUTPUT_MODE_SYNC_LOCAL, which causes changes to take effect when the local PWM generator's count next reaches 0.
  • PWM_OUTPUT_MODE_SYNC_GLOBAL, which causes changes to take effect when the local PWM generator's count next reaches 0 following a call to PWMSyncUpdate() which specifies the same generator in its ui32GenBits parameter.
Returns
None.

References ASSERT, HWREG, PWM_O_ENUPD, PWM_OUT_0_BIT, PWM_OUT_1_BIT, PWM_OUT_2_BIT, PWM_OUT_3_BIT, PWM_OUT_4_BIT, PWM_OUT_5_BIT, PWM_OUT_6_BIT, PWM_OUT_7_BIT, PWM_OUTPUT_MODE_NO_SYNC, PWM_OUTPUT_MODE_SYNC_GLOBAL, and PWM_OUTPUT_MODE_SYNC_LOCAL.

Copyright 2018, Texas Instruments Incorporated