The HTTP server provides APIs to instantiate an HTTP server, and handle requests from HTTP clients.
More...
|
| void | HTTPServer_init (void) |
| | Initialize the HTTPServer module. More...
|
| |
| void | HTTPServer_Params_init (HTTPServer_Params *params) |
| | Initialize the instance create params structure. More...
|
| |
| HTTPServer_Handle | HTTPServer_create (const URLHandler_Setup *urlh, int numURLh, HTTPServer_Params *params) |
| | Create an HTTPServer instance. More...
|
| |
| void | HTTPServer_delete (HTTPServer_Handle *srv) |
| | Delete an HTTPServer instance. More...
|
| |
| void | HTTPServer_sendSimpleResponse (int s, int status, const char *type, size_t len, const void *buf) |
| | Send a simple, complete response to a client. More...
|
| |
| void | HTTPServer_sendResponse (int s, int status, const char *headers[], int numHeaders, size_t len, const void *buf) |
| | Send a complete response to a client. More...
|
| |
| void | HTTPServer_sendErrorResponse (int s, int status) |
| | Send an error response to a client. More...
|
| |
| void | HTTPServer_sendResponseChunked (int s, int status, const char *type) |
| | Begin the process of sending a chunked response to a client. More...
|
| |
| void | HTTPServer_sendChunk (int s, const void *buf, size_t len) |
| | Continue and complete the process of sending a chunked response to a client. More...
|
| |
| int | HTTPServer_serveSelect (HTTPServer_Handle srv, const struct sockaddr *addr, int len, int backlog) |
| | Begin the HTTP Server's main processing loop. More...
|
| |
| bool | HTTPServer_stop (HTTPServer_Handle srv, uint32_t timeout) |
| | Stop a currently running server. More...
|
| |
The HTTP server provides APIs to instantiate an HTTP server, and handle requests from HTTP clients.
Library Usage
To use the HTTPServer APIs, the application should include its header file as follows:
And, add the following HTTP library to the link line:
.../source/ti/net/http/{toolchain}/{isa}/httpserver_{profile}.a
§ HTTPServer_EACCEPTFAIL
| #define HTTPServer_EACCEPTFAIL (-2) |
Internal accept() call failed.
§ HTTPServer_ESOCKETFAIL
| #define HTTPServer_ESOCKETFAIL (-3) |
Internal network socket creation failure.
§ HTTPServer_EBINDFAIL
| #define HTTPServer_EBINDFAIL (-4) |
Internal bind() call failed.
§ HTTPServer_ELISTENFAIL
| #define HTTPServer_ELISTENFAIL (-5) |
Internal listen() call failed.
§ HTTPServer_EMEMFAIL
| #define HTTPServer_EMEMFAIL (-6) |
Internal memory allocation or object creation failure.
§ HTTPServer_EMQFAIL
| #define HTTPServer_EMQFAIL (-7) |
Internal mq creation failure.
§ HTTPServer_EMUTEXFAIL
| #define HTTPServer_EMUTEXFAIL (-8) |
Internal mutex-related failure.
§ URLHandler_GET
§ URLHandler_POST
| #define URLHandler_POST 2 |
§ URLHandler_PUT
§ URLHandler_PATCH
| #define URLHandler_PATCH 4 |
§ URLHandler_DELETE
| #define URLHandler_DELETE 5 |
§ URLHandler_ENOTHANDLED
| #define URLHandler_ENOTHANDLED 0 |
§ URLHandler_EHANDLED
| #define URLHandler_EHANDLED 1 |
§ URLHandler_EERRORHANDLED
| #define URLHandler_EERRORHANDLED 2 |
§ URLHandler_EHANDLEDSTOP
| #define URLHandler_EHANDLEDSTOP 3 |
§ HTTPServer_Params
HTTPServer instance create parameters.
§ HTTPServer_Handle
HTTPServer instance object handle.
§ URLHandler_Handle
A placeholder used to refer to a user-defined type.
This object handle is the type returned from the URLHandler_CreateFxn and passed to all other URLHandler_* functions.
§ URLHandler_Session
§ URLHandler_CreateFxn
Create a user-defined URLHandler_Object.
This function (if used) should be used to instantiate a user-defined URLHandler_Handle object that contains whatever information is deemed necessary to pass to other URLHandler_* functions while the server is running. The handle of the user- defined type should be cast as a URLHandler_Handle before returning it from this function. The handle should be recast as the user- defined type before accessing it in other URLHandler_* functions.
- Parameters
-
| [in] | params | Optional parameters to specify characteristics |
| [in] | session | Handler to current client session |
- Return values
-
| URLHandler | instance handle |
- See also
- URLHandler_DeleteFxn()
§ URLHandler_ProcessFxn
| typedef int(* URLHandler_ProcessFxn) (URLHandler_Handle u, int method, const char *url, const char *urlArgs, int contentLength, int s) |
Process an HTTP request.
This method is called once per URL Handler, for every request received by the server. Its purpose is to fetch the resource requested and have it sent to the client via HTTPServer_send* methods.
- Parameters
-
| [in] | u | Handle to the URL Handler containing relevant data |
| [in] | method | HTTP method of the request being parsed |
| [in] | url | URI of the current request |
| [in] | urlArgs | The query string, if present |
| [in] | contentLength | Content-Length (body length) header value, if present |
| [in] | s | TCP/IP socket connected to a client |
- Return values
-
- See also
- HTTPServer_sendResponse()
§ URLHandler_ScanFieldFxn
| typedef void(* URLHandler_ScanFieldFxn) (URLHandler_Handle u, int method, const char *url, const char *field) |
Scan for specific request headers.
This function can be used to process headers of incoming requests. Every URL Handler with this function defined will have each header passed into this function, one by one. It is called when a request is received by the server, before the request is sent to the URLHandler_ProcessFxn.
- Parameters
-
| [in] | u | Handle to the URL Handler containing relevant data |
| [in] | method | HTTP method of the request being parsed |
| [in] | url | URI of the current request |
| [in] | field | Specific request line containing the header |
- See also
- URLHandler_ProcessFxn()
§ URLHandler_DeleteFxn
Delete a URLHandler.
This function is called when the session associated with the input handler is closed.
- Parameters
-
| [in] | u | The Handler for deletion |
§ URLHandler_Setup
Structure containing URL Handler components.
This structure contains parameters needed for setup of a user- defined URLHandler object and pointers to associated user-defined URLHandler_* functions. The created HTTP Server maintains a table of this data structure for each unique URL Handler.
§ HTTPServer_init()
| void HTTPServer_init |
( |
void |
| ) |
|
Initialize the HTTPServer module.
§ HTTPServer_Params_init()
Initialize the instance create params structure.
- Parameters
-
| [in] | params | params structure to initialize |
§ HTTPServer_create()
Create an HTTPServer instance.
- Parameters
-
| [in] | urlh | Array of URLHandler setup descriptors |
| numURLh | Number of elements in the urlh array |
| [in] | params | Optional parameters to specify characteristics - use NULL for defaults |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
- Return values
-
| HTTPServer | instance handle |
| NULL | if unable to create the instance |
- See also
- HTTPServer_Params_init()
-
HTTPServer_delete()
§ HTTPServer_delete()
Delete an HTTPServer instance.
- Parameters
-
| [in,out] | srv | Pointer containing a handle to the instance to delete. |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
§ HTTPServer_sendSimpleResponse()
| void HTTPServer_sendSimpleResponse |
( |
int |
s, |
|
|
int |
status, |
|
|
const char * |
type, |
|
|
size_t |
len, |
|
|
const void * |
buf |
|
) |
| |
Send a simple, complete response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
| [in] | s | TCP/IP socket connected to a client |
| [in] | status | Status Code associated with the response |
| [in] | type | Content-type of the response |
| [in] | len | Number of bytes in the response buffer buf |
| [in] | buf | Response buffer |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendErrorResponse()
-
HTTPServer_sendResponseChunked()
§ HTTPServer_sendResponse()
| void HTTPServer_sendResponse |
( |
int |
s, |
|
|
int |
status, |
|
|
const char * |
headers[], |
|
|
int |
numHeaders, |
|
|
size_t |
len, |
|
|
const void * |
buf |
|
) |
| |
Send a complete response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
| [in] | s | TCP/IP socket connected to a client |
| [in] | status | Status Code associated with the response |
| [in] | headers | Optional response headers |
| [in] | numHeaders | number of elements in headers |
| [in] | len | Number of bytes in the response buffer buf |
| [in] | buf | Response buffer |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendErrorResponse()
-
HTTPServer_sendResponseChunked()
§ HTTPServer_sendErrorResponse()
| void HTTPServer_sendErrorResponse |
( |
int |
s, |
|
|
int |
status |
|
) |
| |
Send an error response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
| [in] | s | TCP/IP socket connected to a client |
| [in] | status | Status Code associated with the response |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendResponse()
§ HTTPServer_sendResponseChunked()
| void HTTPServer_sendResponseChunked |
( |
int |
s, |
|
|
int |
status, |
|
|
const char * |
type |
|
) |
| |
Begin the process of sending a chunked response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
| [in] | s | TCP/IP socket connected to a client |
| [in] | status | Status Code associated with the response |
| [in] | type | Content-type of the response |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendChunk()
§ HTTPServer_sendChunk()
| void HTTPServer_sendChunk |
( |
int |
s, |
|
|
const void * |
buf, |
|
|
size_t |
len |
|
) |
| |
Continue and complete the process of sending a chunked response to a client.
This function is typically called by a URL Handler, in response to handling a URL request.
- Parameters
-
| [in] | s | TCP/IP socket connected to a client |
| [in] | buf | Response buffer |
| [in] | len | Number of bytes in the response buffer buf |
- Precondition
As with all HTTPServer API's, HTTPServer_init() must have previously been called.
- See also
- HTTPServer_sendChunkedResponse()
§ HTTPServer_serveSelect()
| int HTTPServer_serveSelect |
( |
HTTPServer_Handle |
srv, |
|
|
const struct sockaddr * |
addr, |
|
|
int |
len, |
|
|
int |
backlog |
|
) |
| |
Begin the HTTP Server's main processing loop.
- Parameters
-
| [in] | srv | Handle to the server |
| [in] | addr | Address information for server startup |
| [in] | len | Length of the address information structure |
| [in] | backlog | Maximum number of pending connections to server |
- Return values
-
| 0 | Server received stop command |
| -1 | Server shutdown unexpectedly |
| <-1 | See HTTPServer_E error codes |
§ HTTPServer_stop()
Stop a currently running server.
In order to stop the server using this function, this must be called from an outside thread.
- Parameters
-
| [in] | srv | Handle to the server being stopped |
| timeout | The time in which the server is expected to halt |