USBLib API Guide  1.00.00.01
Data Fields
tUSBRingBufObject Struct Reference

#include <usblib.h>

Data Fields

uint32_t ui32Size
 The ring buffer size. More...
 
volatile uint32_t ui32WriteIndex
 The ring buffer write index. More...
 
volatile uint32_t ui32ReadIndex
 The ring buffer read index. More...
 
uint8_t * pui8Buf
 The ring buffer. More...
 

Detailed Description

The structure used for encapsulating all the items associated with a ring buffer.

Field Documentation

§ ui32Size

uint32_t tUSBRingBufObject::ui32Size

§ ui32WriteIndex

volatile uint32_t tUSBRingBufObject::ui32WriteIndex

§ ui32ReadIndex

volatile uint32_t tUSBRingBufObject::ui32ReadIndex

§ pui8Buf

uint8_t* tUSBRingBufObject::pui8Buf

The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale