![]() |
![]() |
SPIMSP432E4DMA Object. More...
#include <SPIMSP432E4DMA.h>
Data Fields | |
HwiP_Handle | hwiHandle |
SemaphoreP_Handle | transferComplete |
SPI_CallbackFxn | transferCallbackFxn |
UDMAMSP432E4_Handle | dmaHandle |
SPI_Transaction * | headPtr |
SPI_Transaction * | tailPtr |
uint32_t | activeChannel |
size_t | framesQueued |
size_t | framesTransferred |
size_t | priTransferSize |
size_t | altTransferSize |
uint32_t | bitRate |
uint32_t | dataSize |
uint32_t | transferTimeout |
uint16_t | rxScratchBuf |
SPI_Mode | spiMode |
SPI_TransferMode | transferMode |
uint8_t | format |
bool | isOpen |
SPIMSP432E4DMA Object.
The application must not access any member variables of this structure!
HwiP_Handle SPIMSP432E4DMA_Object::hwiHandle |
SemaphoreP_Handle SPIMSP432E4DMA_Object::transferComplete |
SPI_CallbackFxn SPIMSP432E4DMA_Object::transferCallbackFxn |
UDMAMSP432E4_Handle SPIMSP432E4DMA_Object::dmaHandle |
SPI_Transaction* SPIMSP432E4DMA_Object::headPtr |
SPI_Transaction* SPIMSP432E4DMA_Object::tailPtr |
uint32_t SPIMSP432E4DMA_Object::activeChannel |
size_t SPIMSP432E4DMA_Object::framesQueued |
size_t SPIMSP432E4DMA_Object::framesTransferred |
size_t SPIMSP432E4DMA_Object::priTransferSize |
size_t SPIMSP432E4DMA_Object::altTransferSize |
uint32_t SPIMSP432E4DMA_Object::bitRate |
uint32_t SPIMSP432E4DMA_Object::dataSize |
uint32_t SPIMSP432E4DMA_Object::transferTimeout |
uint16_t SPIMSP432E4DMA_Object::rxScratchBuf |
SPI_Mode SPIMSP432E4DMA_Object::spiMode |
SPI_TransferMode SPIMSP432E4DMA_Object::transferMode |
uint8_t SPIMSP432E4DMA_Object::format |
bool SPIMSP432E4DMA_Object::isOpen |