![]() |
![]() |
NVS attributes. More...
#include <NVS.h>
Data Fields | |
void * | regionBase |
size_t | regionSize |
size_t | sectorSize |
NVS attributes.
The address of an NVS_Attrs structure is passed to NVS_getAttrs().
void* NVS_Attrs::regionBase |
Base address of the NVS region. If the NVS region is not directly accessible by the MCU (such as SPI flash), this field will be set to NVS_REGION_NOT_ADDRESSABLE.
size_t NVS_Attrs::regionSize |
NVS region size in bytes.
size_t NVS_Attrs::sectorSize |
Erase sector size in bytes. This attribute is device specific.