![]() |
![]() |
|
Network Services API
2.40.00.11
|
#include <string.h>#include <stdbool.h>
Go to the source code of this file.
Data Structures | |
| struct | _MQTTServer_SubscribeParams_ |
| struct | _MQTTServer_UnSubscribeParams_ |
| struct | _MQTTServer_LocalAuthenticationData_ |
| struct | _MQTTServer_ConnectMetaDataCB_ |
| struct | _MQTTServer_RecvMetaDataCB_ |
| struct | _MQTTServer_DisconnectMetaDataCB_ |
| struct | _MQTTServer_ConnParams_ |
| struct | MQTTServer_Params |
Typedefs | |
| typedef void(* | MQTTServer_CallBack) (int32_t event, void *metaData, uint32_t metaDateLen, void *data, uint32_t dataLen) |
| typedef void * | MQTTServer_Handle |
| typedef struct _MQTTServer_SubscribeParams_ | MQTTServer_SubscribeParams |
| typedef struct _MQTTServer_UnSubscribeParams_ | MQTTServer_UnSubscribeParams |
| typedef struct _MQTTServer_LocalAuthenticationData_ | MQTTServer_LocalAuthenticationData |
| typedef struct _MQTTServer_ConnectMetaDataCB_ | MQTTServer_ConnectMetaDataCB |
| typedef struct _MQTTServer_RecvMetaDataCB_ | MQTTServer_RecvMetaDataCB |
| typedef struct _MQTTServer_DisconnectMetaDataCB_ | MQTTServer_DisconnectMetaDataCB |
| typedef struct _MQTTServer_ConnParams_ | MQTTServer_ConnParams |
Enumerations | |
| enum | MQTTServer_Option { MQTTServer_USER_NAME = 0, MQTTServer_PASSWORD = 1 } |
| enum | MQTTServer_EventCB { MQTTServer_RECV_CB_EVENT = 0, MQTTServer_CONNECT_CB_EVENT = 1, MQTTServer_DISCONNECT_CB_EVENT = 2 } |
Functions | |
| int16_t | MQTTServer_delete (MQTTServer_Handle handle) |
| MQTTServer_Handle | MQTTServer_create (MQTTServer_CallBack defaultCallback, MQTTServer_Params *attrib) |
| int16_t | MQTTServer_run (MQTTServer_Handle handle) |
| int16_t | MQTTServer_subscribe (MQTTServer_Handle handle, MQTTServer_SubscribeParams *value, uint8_t numberOfTopics) |
| int16_t | MQTTServer_unsubscribe (MQTTServer_Handle handle, MQTTServer_UnSubscribeParams *value, uint8_t numberOfTopics) |
| int16_t | MQTTServer_publish (MQTTServer_Handle handle, char *topic, uint16_t topicLen, char *msg, uint16_t msgLen, uint32_t flags) |
| int16_t | MQTTServer_set (MQTTServer_Handle handle, uint16_t option, void *value, uint16_t valueLength) |