![]() |
![]() |
#include <stdint.h>#include <stdbool.h>

Go to the source code of this file.
Macros | |
| #define | SSI_TXEOT 0x00000040 |
| #define | SSI_DMATX 0x00000020 |
| #define | SSI_DMARX 0x00000010 |
| #define | SSI_TXFF 0x00000008 |
| #define | SSI_RXFF 0x00000004 |
| #define | SSI_RXTO 0x00000002 |
| #define | SSI_RXOR 0x00000001 |
| #define | SSI_FRF_MOTO_MODE_0 0x00000000 |
| #define | SSI_FRF_MOTO_MODE_1 0x00000002 |
| #define | SSI_FRF_MOTO_MODE_2 0x00000001 |
| #define | SSI_FRF_MOTO_MODE_3 0x00000003 |
| #define | SSI_FRF_TI 0x00000010 |
| #define | SSI_MODE_MASTER 0x00000000 |
| #define | SSI_MODE_SLAVE 0x00000001 |
| #define | SSI_DMA_TX 0x00000002 |
| #define | SSI_DMA_RX 0x00000001 |
| #define | SSI_CLOCK_SYSTEM 0x00000000 |
| #define | SSI_CLOCK_ALTCLK 0x00000005 |
| #define | SSI_ADV_MODE_LEGACY 0x00000000 |
| #define | SSI_ADV_MODE_READ_WRITE 0x000001c0 |
| #define | SSI_ADV_MODE_WRITE 0x000000c0 |
| #define | SSI_ADV_MODE_BI_READ 0x00000140 |
| #define | SSI_ADV_MODE_BI_WRITE 0x00000040 |
| #define | SSI_ADV_MODE_QUAD_READ 0x00000180 |
| #define | SSI_ADV_MODE_QUAD_WRITE 0x00000080 |
Functions | |
| void | SSIConfigSetExpClk (uint32_t ui32Base, uint32_t ui32SSIClk, uint32_t ui32Protocol, uint32_t ui32Mode, uint32_t ui32BitRate, uint32_t ui32DataWidth) |
| void | SSIDataGet (uint32_t ui32Base, uint32_t *pui32Data) |
| int32_t | SSIDataGetNonBlocking (uint32_t ui32Base, uint32_t *pui32Data) |
| void | SSIDataPut (uint32_t ui32Base, uint32_t ui32Data) |
| int32_t | SSIDataPutNonBlocking (uint32_t ui32Base, uint32_t ui32Data) |
| void | SSIDisable (uint32_t ui32Base) |
| void | SSIEnable (uint32_t ui32Base) |
| void | SSIIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| void | SSIIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| void | SSIIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| void | SSIIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| uint32_t | SSIIntStatus (uint32_t ui32Base, bool bMasked) |
| void | SSIIntUnregister (uint32_t ui32Base) |
| void | SSIDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| void | SSIDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| bool | SSIBusy (uint32_t ui32Base) |
| void | SSIClockSourceSet (uint32_t ui32Base, uint32_t ui32Source) |
| uint32_t | SSIClockSourceGet (uint32_t ui32Base) |
| void | SSIAdvModeSet (uint32_t ui32Base, uint32_t ui32Mode) |
| void | SSIAdvDataPutFrameEnd (uint32_t ui32Base, uint32_t ui32Data) |
| int32_t | SSIAdvDataPutFrameEndNonBlocking (uint32_t ui32Base, uint32_t ui32Data) |
| void | SSIAdvFrameHoldEnable (uint32_t ui32Base) |
| void | SSIAdvFrameHoldDisable (uint32_t ui32Base) |
| #define SSI_TXEOT 0x00000040 |
| #define SSI_DMATX 0x00000020 |
| #define SSI_DMARX 0x00000010 |
| #define SSI_TXFF 0x00000008 |
| #define SSI_RXFF 0x00000004 |
| #define SSI_RXTO 0x00000002 |
| #define SSI_RXOR 0x00000001 |
| #define SSI_FRF_MOTO_MODE_0 0x00000000 |
Referenced by SSIConfigSetExpClk().
| #define SSI_FRF_MOTO_MODE_1 0x00000002 |
Referenced by SSIConfigSetExpClk().
| #define SSI_FRF_MOTO_MODE_2 0x00000001 |
Referenced by SSIConfigSetExpClk().
| #define SSI_FRF_MOTO_MODE_3 0x00000003 |
Referenced by SSIConfigSetExpClk().
| #define SSI_FRF_TI 0x00000010 |
Referenced by SSIConfigSetExpClk().
| #define SSI_MODE_MASTER 0x00000000 |
Referenced by SSIConfigSetExpClk().
| #define SSI_MODE_SLAVE 0x00000001 |
Referenced by SSIConfigSetExpClk().
| #define SSI_DMA_TX 0x00000002 |
| #define SSI_DMA_RX 0x00000001 |
| #define SSI_CLOCK_SYSTEM 0x00000000 |
Referenced by SSIClockSourceSet().
| #define SSI_CLOCK_ALTCLK 0x00000005 |
Referenced by SSIClockSourceSet().
| #define SSI_ADV_MODE_LEGACY 0x00000000 |
Referenced by SSIAdvModeSet().
| #define SSI_ADV_MODE_READ_WRITE 0x000001c0 |
Referenced by SSIAdvModeSet().
| #define SSI_ADV_MODE_WRITE 0x000000c0 |
Referenced by SSIAdvModeSet().
| #define SSI_ADV_MODE_BI_READ 0x00000140 |
Referenced by SSIAdvModeSet().
| #define SSI_ADV_MODE_BI_WRITE 0x00000040 |
Referenced by SSIAdvModeSet().
| #define SSI_ADV_MODE_QUAD_READ 0x00000180 |
Referenced by SSIAdvModeSet().
| #define SSI_ADV_MODE_QUAD_WRITE 0x00000080 |
Referenced by SSIAdvModeSet().