![]() |
![]() |
#include <stdint.h>

Go to the source code of this file.
Functions | |
| uint32_t | CPUcpsid (void) |
| uint32_t | CPUcpsie (void) |
| uint32_t | CPUprimask (void) |
| void | CPUwfi (void) |
| uint32_t | CPUbasepriGet (void) |
| void | CPUbasepriSet (uint32_t ui32NewBasepri) |
| uint32_t CPUcpsid | ( | void | ) |
Referenced by IntMasterDisable().
| uint32_t CPUcpsie | ( | void | ) |
| uint32_t CPUprimask | ( | void | ) |
| void CPUwfi | ( | void | ) |
Referenced by SysCtlDeepSleep(), and SysCtlSleep().
| uint32_t CPUbasepriGet | ( | void | ) |
Referenced by IntPriorityMaskGet().
| void CPUbasepriSet | ( | uint32_t | ui32NewBasepri | ) |
Referenced by IntPriorityMaskSet().