![]() |
![]() |
TimerMSP432E4_Object. More...
#include <TimerMSP432E4.h>
Data Fields | |
HwiP_Handle | hwiHandle |
Power_NotifyObj | notifyObj |
SemaphoreP_Handle | timerSem |
Timer_CallBackFxn | callBack |
Timer_Mode | mode |
uint32_t | timer |
uint32_t | period |
uint32_t | prescaler |
bool | isRunning |
TimerMSP432E4_Object.
The application must not access any member variables of this structure!
HwiP_Handle TimerMSP432E4_Object_::hwiHandle |
Power_NotifyObj TimerMSP432E4_Object_::notifyObj |
SemaphoreP_Handle TimerMSP432E4_Object_::timerSem |
Timer_CallBackFxn TimerMSP432E4_Object_::callBack |
Timer_Mode TimerMSP432E4_Object_::mode |
uint32_t TimerMSP432E4_Object_::timer |
uint32_t TimerMSP432E4_Object_::period |
uint32_t TimerMSP432E4_Object_::prescaler |
bool TimerMSP432E4_Object_::isRunning |