Data Fields
tEMACDES3 Union Reference

#include <emac.h>

Collaboration diagram for tEMACDES3:
Collaboration graph
[legend]

Data Fields

tEMACDMADescriptorpLink
 
void * pvBuffer2
 

Detailed Description

A union used to describe the two overlapping fields forming the third word of the Ethernet DMA descriptor.

Field Documentation

§ pLink

tEMACDMADescriptor* tEMACDES3::pLink

When DMA descriptors are used in chained mode, this field is used to provide a link to the next descriptor.

§ pvBuffer2

void* tEMACDES3::pvBuffer2

When the DMA descriptors are unchained, this field may be used to point to a second buffer containing data for transmission or providing storage for a received frame.


The documentation for this union was generated from the following file:
Copyright 2018, Texas Instruments Incorporated