Go to the source code of this file.
|
| void * | USBDBulkInit (uint32_t ui32Index, tUSBDBulkDevice *psBulkDevice) |
| |
| void * | USBDBulkCompositeInit (uint32_t ui32Index, tUSBDBulkDevice *psBulkDevice, tCompositeEntry *psCompEntry) |
| |
| void | USBDBulkTerm (void *pvBulkDevice) |
| |
| void * | USBDBulkSetRxCBData (void *pvBulkDevice, void *pvCBData) |
| |
| void * | USBDBulkSetTxCBData (void *pvBulkDevice, void *pvCBData) |
| |
| uint32_t | USBDBulkPacketWrite (void *pvBulkDevice, uint8_t *pi8Data, uint32_t ui32Length, bool bLast) |
| |
| uint32_t | USBDBulkPacketRead (void *pvBulkDevice, uint8_t *pi8Data, uint32_t ui32Length, bool bLast) |
| |
| uint32_t | USBDBulkTxPacketAvailable (void *pvBulkDevice) |
| |
| uint32_t | USBDBulkRxPacketAvailable (void *pvBulkDevice) |
| |
| bool | USBDBulkRemoteWakeupRequest (void *pvBulkDevice) |
| |
| void | USBDBulkPowerStatusSet (void *pvBulkInstance, uint8_t ui8Power) |
| |