#include <usbdbulk.h>
§ ui32USBBase
| uint32_t tBulkInstance::ui32USBBase |
§ sDevInfo
§ iBulkRxState
§ iBulkTxState
§ ui16DeferredOpFlags
| volatile uint16_t tBulkInstance::ui16DeferredOpFlags |
§ ui16LastTxSize
| uint16_t tBulkInstance::ui16LastTxSize |
§ bConnected
| volatile bool tBulkInstance::bConnected |
§ ui8INEndpoint
| uint8_t tBulkInstance::ui8INEndpoint |
§ ui8OUTEndpoint
| uint8_t tBulkInstance::ui8OUTEndpoint |
§ ui8Interface
| uint8_t tBulkInstance::ui8Interface |
The documentation for this struct was generated from the following file: