Data Fields
tUSBHostDevice Struct Reference

#include <usbhostpriv.h>

Data Fields

uint32_t ui32Address
 
uint32_t ui32Interface
 
bool bLowSpeed
 
uint32_t ui32Speed
 
bool bConfigRead
 
uint8_t ui8Hub
 
uint8_t ui8HubPort
 
tDeviceDescriptor sDeviceDescriptor
 
tConfigDescriptor * psConfigDescriptor
 
uint32_t ui32ConfigDescriptorSize
 
uint32_t ui32Flags
 

Field Documentation

§ ui32Address

uint32_t tUSBHostDevice::ui32Address

§ ui32Interface

uint32_t tUSBHostDevice::ui32Interface

Referenced by USBHCDSetInterface().

§ bLowSpeed

bool tUSBHostDevice::bLowSpeed

§ ui32Speed

uint32_t tUSBHostDevice::ui32Speed

§ bConfigRead

bool tUSBHostDevice::bConfigRead

§ ui8Hub

uint8_t tUSBHostDevice::ui8Hub

§ ui8HubPort

uint8_t tUSBHostDevice::ui8HubPort

§ sDeviceDescriptor

tDeviceDescriptor tUSBHostDevice::sDeviceDescriptor

§ psConfigDescriptor

tConfigDescriptor* tUSBHostDevice::psConfigDescriptor

§ ui32ConfigDescriptorSize

uint32_t tUSBHostDevice::ui32ConfigDescriptorSize

§ ui32Flags

uint32_t tUSBHostDevice::ui32Flags

The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated