![]() |
![]() |
#include <usbdhidmouse.h>
Data Fields | |
const uint16_t | ui16VID |
The vendor ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16PID |
The product ID that this device is to present in the device descriptor. More... | |
const uint16_t | ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps. More... | |
const uint8_t | ui8PwrAttributes |
const tUSBCallback | pfnCallback |
void * | pvCBData |
const uint8_t *const * | ppui8StringDescriptors |
const uint32_t | ui32NumStringDescriptors |
tHIDMouseInstance | sPrivateData |
This structure is used by the application to define operating parameters for the HID mouse device.
const uint16_t tUSBDHIDMouseDevice::ui16VID |
The vendor ID that this device is to present in the device descriptor.
Referenced by USBDHIDMouseCompositeInit().
const uint16_t tUSBDHIDMouseDevice::ui16PID |
The product ID that this device is to present in the device descriptor.
Referenced by USBDHIDMouseCompositeInit().
const uint16_t tUSBDHIDMouseDevice::ui16MaxPowermA |
The maximum power consumption of the device, expressed in milliamps.
Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().
const uint8_t tUSBDHIDMouseDevice::ui8PwrAttributes |
Indicates whether the device is self- or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.
Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().
const tUSBCallback tUSBDHIDMouseDevice::pfnCallback |
A pointer to the callback function which is called to notify the application of events relating to the operation of the mouse.
Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().
void* tUSBDHIDMouseDevice::pvCBData |
A client-supplied pointer which is sent as the first parameter in all calls made to the mouse callback, pfnCallback.
Referenced by USBDHIDMouseSetCBData().
const uint8_t* const* tUSBDHIDMouseDevice::ppui8StringDescriptors |
A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1),HID Interface description string (language 1), Configuration description string (language 1).
If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.
Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().
const uint32_t tUSBDHIDMouseDevice::ui32NumStringDescriptors |
The number of descriptors provided in the ppStringDescriptors array. This must be (1 + (5 * (num languages))).
tHIDMouseInstance tUSBDHIDMouseDevice::sPrivateData |
The private instance data for this device. This memory must remain accessible for as long as the mouse device is in use and must not be modified by any code outside the HID mouse driver.
Referenced by USBDHIDMouseCompositeInit(), USBDHIDMouseInit(), USBDHIDMousePowerStatusSet(), USBDHIDMouseRemoteWakeupRequest(), USBDHIDMouseStateChange(), and USBDHIDMouseTerm().