Data Fields
SPIMSP432E4DMA_Object Struct Reference

SPIMSP432E4DMA Object. More...

#include <SPIMSP432E4DMA.h>

Data Fields

HwiP_Handle hwiHandle
 
SemaphoreP_Handle transferComplete
 
SPI_CallbackFxn transferCallbackFxn
 
SPI_Transactiontransaction
 
UDMAMSP432E4_Handle dmaHandle
 
size_t amtDataXferred
 
size_t currentXferAmt
 
uint32_t bitRate
 
uint32_t dataSize
 
uint32_t transferTimeout
 
SPI_Mode spiMode
 
SPI_TransferMode transferMode
 
bool cancelInProgress
 
bool isOpen
 
uint8_t format
 

Detailed Description

SPIMSP432E4DMA Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwiHandle

HwiP_Handle SPIMSP432E4DMA_Object::hwiHandle

§ transferComplete

SemaphoreP_Handle SPIMSP432E4DMA_Object::transferComplete

§ transferCallbackFxn

SPI_CallbackFxn SPIMSP432E4DMA_Object::transferCallbackFxn

§ transaction

SPI_Transaction* SPIMSP432E4DMA_Object::transaction

§ dmaHandle

UDMAMSP432E4_Handle SPIMSP432E4DMA_Object::dmaHandle

§ amtDataXferred

size_t SPIMSP432E4DMA_Object::amtDataXferred

§ currentXferAmt

size_t SPIMSP432E4DMA_Object::currentXferAmt

§ bitRate

uint32_t SPIMSP432E4DMA_Object::bitRate

§ dataSize

uint32_t SPIMSP432E4DMA_Object::dataSize

§ transferTimeout

uint32_t SPIMSP432E4DMA_Object::transferTimeout

§ spiMode

SPI_Mode SPIMSP432E4DMA_Object::spiMode

§ transferMode

SPI_TransferMode SPIMSP432E4DMA_Object::transferMode

§ cancelInProgress

bool SPIMSP432E4DMA_Object::cancelInProgress

§ isOpen

bool SPIMSP432E4DMA_Object::isOpen

§ format

uint8_t SPIMSP432E4DMA_Object::format

The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated