Data Fields
PowerMSP432E4_Config Struct Reference

Power global configuration structure. More...

#include <PowerMSP432E4.h>

Data Fields

Power_PolicyFxn policyFxn
 The Power Policy function. More...
 
bool enablePolicy
 Boolean specifying if the Power Policy function is enabled. More...
 

Detailed Description

Power global configuration structure.

Field Documentation

§ policyFxn

Power_PolicyFxn PowerMSP432E4_Config::policyFxn

The Power Policy function.

When enabled, this function is invoked in the idle loop, to opportunistically select and activate sleep states.

§ enablePolicy

bool PowerMSP432E4_Config::enablePolicy

Boolean specifying if the Power Policy function is enabled.

If 'true', the policy function will be invoked once for each pass of the idle loop.

If 'false', the policy will not be invoked.

In addition to this static setting, the Power Policy can be dynamically enabled and disabled at runtime, via the Power_enablePolicy() and Power_disablePolicy() functions, respectively.


The documentation for this struct was generated from the following file:
Copyright 2018, Texas Instruments Incorporated