![]() |
![]() |
|
Network Services API
2.20.00.11
|
The SimpleLink MQTTClient Module provides an easy-to-use API to enable constrained and deeply embedded micro-controller based products to interact with cloud or network based MQTT servers. The users of MQTTClient services, while benefiting from the abstraction of the MQTT protocol, will find them suitable for varied deployments of MQTT subscribers and/or publishers. More...
Macros | |
| #define | MQTTCLIENT_ERR_NETWORK MQTT_PACKET_ERR_NETWORK |
| #define | MQTTCLIENT_ERR_TIMEOUT MQTT_PACKET_ERR_TIMEOUT |
| #define | MQTTCLIENT_ERR_NET_OPS MQTT_PACKET_ERR_NET_OPS |
| #define | MQTTCLIENT_ERR_FNPARAM MQTT_PACKET_ERR_FNPARAM |
| #define | MQTTCLIENT_ERR_PKT_AVL MQTT_PACKET_ERR_PKT_AVL |
| #define | MQTTCLIENT_ERR_PKT_LEN MQTT_PACKET_ERR_PKT_LEN |
| #define | MQTTCLIENT_ERR_NOTCONN MQTT_PACKET_ERR_NOTCONN |
| #define | MQTTCLIENT_ERR_BADCALL MQTT_PACKET_ERR_BADCALL |
| #define | MQTTCLIENT_ERR_CONTENT MQTT_PACKET_ERR_CONTENT |
| #define | MQTTCLIENT_ERR_LIBQUIT MQTT_PACKET_ERR_LIBQUIT |
| #define | MQTTCLIENT_ERR_REMLSTN MQTT_PACKET_ERR_REMLSTN |
| #define | MQTTCLIENT_OPERATION_CONNACK MQTT_CONNACK |
| #define | MQTTCLIENT_OPERATION_EVT_PUBACK MQTT_PUBACK |
| #define | MQTTCLIENT_OPERATION_PUBCOMP MQTT_PUBCOMP |
| #define | MQTTCLIENT_OPERATION_SUBACK MQTT_SUBACK |
| #define | MQTTCLIENT_OPERATION_UNSUBACK MQTT_UNSUBACK |
| #define | MQTTCLIENT_NETCONN_IP4 MQTT_DEV_NETCONN_OPT_IP4 |
| #define | MQTTCLIENT_NETCONN_IP6 MQTT_DEV_NETCONN_OPT_IP6 |
| #define | MQTTCLIENT_NETCONN_URL MQTT_DEV_NETCONN_OPT_URL |
| #define | MQTTCLIENT_NETCONN_SEC MQTT_DEV_NETCONN_OPT_SEC |
| #define | MQTTCLIENT_NETCONN_SKIP_DOMAIN_NAME_VERIFICATION MQTT_DEV_NETCONN_OPT_SKIP_DOMAIN_NAME_VERIFICATION |
| #define | MQTTCLIENT_NETCONN_SKIP_CERTIFICATE_CATALOG_VERIFICATION MQTT_DEV_NETCONN_OPT_SKIP_CERTIFICATE_CATALOG_VERIFICATION |
| #define | MQTTCLIENT_NETCONN_SKIP_DATE_VERIFICATION MQTT_DEV_NETCONN_OPT_SKIP_DATE_VERIFICATION |
The SimpleLink MQTTClient Module provides an easy-to-use API to enable constrained and deeply embedded micro-controller based products to interact with cloud or network based MQTT servers. The users of MQTTClient services, while benefiting from the abstraction of the MQTT protocol, will find them suitable for varied deployments of MQTT subscribers and/or publishers.
The SL MQTT Client Layer, in addition to providing services to the application, encompasses a RTOS task to handle the incoming messages from the server. Such a dedicated context to process the messages from the server facilitates the apps to receive data (i.e. PUBLISH messages) even when they are blocked, whilst awaiting ACK for a previous transaction with the server. The receive task in the SL MQTT Layer can not be disabled anytime, however its system wide priority is configurable and can be set.
Some of the salient features of the SL MQTT Layer are
The SL implementation enables the application developers to configure the following parameters using the compile line flags (-D option)
To use the MQTTClient APIs, the application should include its header file as follows:
And, add the following MQTT library to the link line:
| #define MQTTCLIENT_ERR_NETWORK MQTT_PACKET_ERR_NETWORK |
Problem in network (sock err)
| #define MQTTCLIENT_ERR_TIMEOUT MQTT_PACKET_ERR_TIMEOUT |
Net transaction has timed out
| #define MQTTCLIENT_ERR_NET_OPS MQTT_PACKET_ERR_NET_OPS |
Platform Net Ops un-available
| #define MQTTCLIENT_ERR_FNPARAM MQTT_PACKET_ERR_FNPARAM |
Invalid parameter(s) provided
| #define MQTTCLIENT_ERR_PKT_AVL MQTT_PACKET_ERR_PKT_AVL |
No pkts are available in pool
| #define MQTTCLIENT_ERR_PKT_LEN MQTT_PACKET_ERR_PKT_LEN |
Inadequate free buffer in pkt
| #define MQTTCLIENT_ERR_NOTCONN MQTT_PACKET_ERR_NOTCONN |
Lib isn't CONNECTED to server
| #define MQTTCLIENT_ERR_BADCALL MQTT_PACKET_ERR_BADCALL |
Irrelevant call for LIB state
| #define MQTTCLIENT_ERR_CONTENT MQTT_PACKET_ERR_CONTENT |
MSG / Data content has errors
| #define MQTTCLIENT_ERR_LIBQUIT MQTT_PACKET_ERR_LIBQUIT |
Needs reboot library has quit
| #define MQTTCLIENT_ERR_REMLSTN MQTT_PACKET_ERR_REMLSTN |
No remote listener for socket
| #define MQTTCLIENT_OPERATION_CONNACK MQTT_CONNACK |
CONNACK has been received from the server
| #define MQTTCLIENT_OPERATION_EVT_PUBACK MQTT_PUBACK |
PUBACK has been received from the server
| #define MQTTCLIENT_OPERATION_PUBCOMP MQTT_PUBCOMP |
PUBCOMP has been received from the server
| #define MQTTCLIENT_OPERATION_SUBACK MQTT_SUBACK |
SUBACK has been received from the server
| #define MQTTCLIENT_OPERATION_UNSUBACK MQTT_UNSUBACK |
UNSUBACK has been received from the server
| #define MQTTCLIENT_NETCONN_IP4 MQTT_DEV_NETCONN_OPT_IP4 |
Assert for IPv4 connection
| #define MQTTCLIENT_NETCONN_IP6 MQTT_DEV_NETCONN_OPT_IP6 |
Assert for IPv6 connection, otherwise IPv4
| #define MQTTCLIENT_NETCONN_URL MQTT_DEV_NETCONN_OPT_URL |
Server address is an URL and not IP address
| #define MQTTCLIENT_NETCONN_SEC MQTT_DEV_NETCONN_OPT_SEC |
Connection to server must be secure (TLS)
| #define MQTTCLIENT_NETCONN_SKIP_DOMAIN_NAME_VERIFICATION MQTT_DEV_NETCONN_OPT_SKIP_DOMAIN_NAME_VERIFICATION |
Assert to skip domain name verification
| #define MQTTCLIENT_NETCONN_SKIP_CERTIFICATE_CATALOG_VERIFICATION MQTT_DEV_NETCONN_OPT_SKIP_CERTIFICATE_CATALOG_VERIFICATION |
Assert to skip certificate catalog verification
| #define MQTTCLIENT_NETCONN_SKIP_DATE_VERIFICATION MQTT_DEV_NETCONN_OPT_SKIP_DATE_VERIFICATION |
Assert to skip date verification