![]() |
![]() |
#include <stdint.h>#include <stdbool.h>Go to the source code of this file.
Macros | |
| #define | WATCHDOG_INT_TYPE_INT 0x00000000 |
| #define | WATCHDOG_INT_TYPE_NMI 0x00000004 |
Functions | |
| bool | WatchdogRunning (uint32_t ui32Base) |
| void | WatchdogEnable (uint32_t ui32Base) |
| void | WatchdogResetEnable (uint32_t ui32Base) |
| void | WatchdogResetDisable (uint32_t ui32Base) |
| void | WatchdogLock (uint32_t ui32Base) |
| void | WatchdogUnlock (uint32_t ui32Base) |
| bool | WatchdogLockState (uint32_t ui32Base) |
| void | WatchdogReloadSet (uint32_t ui32Base, uint32_t ui32LoadVal) |
| uint32_t | WatchdogReloadGet (uint32_t ui32Base) |
| uint32_t | WatchdogValueGet (uint32_t ui32Base) |
| void | WatchdogIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| void | WatchdogIntUnregister (uint32_t ui32Base) |
| void | WatchdogIntEnable (uint32_t ui32Base) |
| uint32_t | WatchdogIntStatus (uint32_t ui32Base, bool bMasked) |
| void | WatchdogIntClear (uint32_t ui32Base) |
| void | WatchdogIntTypeSet (uint32_t ui32Base, uint32_t ui32Type) |
| void | WatchdogStallEnable (uint32_t ui32Base) |
| void | WatchdogStallDisable (uint32_t ui32Base) |
| #define WATCHDOG_INT_TYPE_INT 0x00000000 |
Referenced by WatchdogIntTypeSet().
| #define WATCHDOG_INT_TYPE_NMI 0x00000004 |
Referenced by WatchdogIntTypeSet().