|
| void | USBHostSuspend (uint32_t ui32Base) |
| |
| void | USBHostReset (uint32_t ui32Base, bool bStart) |
| |
| void | USBHighSpeed (uint32_t ui32Base, bool bEnable) |
| |
| void | USBHostResume (uint32_t ui32Base, bool bStart) |
| |
| uint32_t | USBHostSpeedGet (uint32_t ui32Base) |
| |
| uint32_t | USBDevSpeedGet (uint32_t ui32Base) |
| |
| void | USBIntDisableControl (uint32_t ui32Base, uint32_t ui32Flags) |
| |
| void | USBIntEnableControl (uint32_t ui32Base, uint32_t ui32Flags) |
| |
| uint32_t | USBIntStatusControl (uint32_t ui32Base) |
| |
| void | USBIntDisableEndpoint (uint32_t ui32Base, uint32_t ui32Flags) |
| |
| void | USBIntEnableEndpoint (uint32_t ui32Base, uint32_t ui32Flags) |
| |
| uint32_t | USBIntStatusEndpoint (uint32_t ui32Base) |
| |
| void | USBIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| |
| void | USBIntUnregister (uint32_t ui32Base) |
| |
| uint32_t | USBEndpointStatus (uint32_t ui32Base, uint32_t ui32Endpoint) |
| |
| void | USBHostEndpointStatusClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBDevEndpointStatusClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBHostEndpointDataToggle (uint32_t ui32Base, uint32_t ui32Endpoint, bool bDataToggle, uint32_t ui32Flags) |
| |
| void | USBEndpointDataToggleClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBHostEndpointPing (uint32_t ui32Base, uint32_t ui32Endpoint, bool bEnable) |
| |
| void | USBDevEndpointStall (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBDevEndpointStallClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBDevConnect (uint32_t ui32Base) |
| |
| void | USBDevDisconnect (uint32_t ui32Base) |
| |
| void | USBDevAddrSet (uint32_t ui32Base, uint32_t ui32Address) |
| |
| uint32_t | USBDevAddrGet (uint32_t ui32Base) |
| |
| void | USBHostEndpointConfig (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32MaxPayload, uint32_t ui32NAKPollInterval, uint32_t ui32TargetEndpoint, uint32_t ui32Flags) |
| |
| void | USBHostEndpointSpeed (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBDevEndpointConfigSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32MaxPacketSize, uint32_t ui32Flags) |
| |
| void | USBDevEndpointConfigGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t *pui32MaxPacketSize, uint32_t *pui32Flags) |
| |
| void | USBFIFOConfigSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32FIFOAddress, uint32_t ui32FIFOSize, uint32_t ui32Flags) |
| |
| void | USBFIFOConfigGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t *pui32FIFOAddress, uint32_t *pui32FIFOSize, uint32_t ui32Flags) |
| |
| void | USBEndpointDMAConfigSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Config) |
| |
| void | USBEndpointDMAEnable (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBEndpointDMADisable (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| uint32_t | USBEndpointDataAvail (uint32_t ui32Base, uint32_t ui32Endpoint) |
| |
| int32_t | USBEndpointDataGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint8_t *pui8Data, uint32_t *pui32Size) |
| |
| void | USBDevEndpointDataAck (uint32_t ui32Base, uint32_t ui32Endpoint, bool bIsLastPacket) |
| |
| void | USBHostEndpointDataAck (uint32_t ui32Base, uint32_t ui32Endpoint) |
| |
| int32_t | USBEndpointDataPut (uint32_t ui32Base, uint32_t ui32Endpoint, uint8_t *pui8Data, uint32_t ui32Size) |
| |
| int32_t | USBEndpointDataSend (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32TransType) |
| |
| void | USBFIFOFlush (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBHostRequestIN (uint32_t ui32Base, uint32_t ui32Endpoint) |
| |
| void | USBHostRequestINClear (uint32_t ui32Base, uint32_t ui32Endpoint) |
| |
| void | USBHostRequestStatus (uint32_t ui32Base) |
| |
| void | USBHostAddrSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Addr, uint32_t ui32Flags) |
| |
| uint32_t | USBHostAddrGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBHostHubAddrSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Addr, uint32_t ui32Flags) |
| |
| uint32_t | USBHostHubAddrGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags) |
| |
| void | USBHostPwrConfig (uint32_t ui32Base, uint32_t ui32Flags) |
| |
| void | USBHostPwrFaultEnable (uint32_t ui32Base) |
| |
| void | USBHostPwrFaultDisable (uint32_t ui32Base) |
| |
| void | USBHostPwrEnable (uint32_t ui32Base) |
| |
| void | USBHostPwrDisable (uint32_t ui32Base) |
| |
| uint32_t | USBFrameNumberGet (uint32_t ui32Base) |
| |
| void | USBOTGSessionRequest (uint32_t ui32Base, bool bStart) |
| |
| uint32_t | USBFIFOAddrGet (uint32_t ui32Base, uint32_t ui32Endpoint) |
| |
| uint32_t | USBModeGet (uint32_t ui32Base) |
| |
| void | USBHostMode (uint32_t ui32Base) |
| |
| void | USBDevMode (uint32_t ui32Base) |
| |
| void | USBOTGMode (uint32_t ui32Base) |
| |
| void | USBModeConfig (uint32_t ui32Base, uint32_t ui32Mode) |
| |
| void | USBPHYPowerOff (uint32_t ui32Base) |
| |
| void | USBPHYPowerOn (uint32_t ui32Base) |
| |
| void | USBEndpointPacketCountSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Count) |
| |
| uint32_t | USBNumEndpointsGet (uint32_t ui32Base) |
| |
| void | USBClockEnable (uint32_t ui32Base, uint32_t ui32Div, uint32_t ui32Flags) |
| |
| void | USBClockDisable (uint32_t ui32Base) |
| |
| void | USBDMAChannelIntEnable (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| void | USBDMAChannelIntDisable (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| uint32_t | USBDMAChannelIntStatus (uint32_t ui32Base) |
| |
| void | USBDMAChannelEnable (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| void | USBDMAChannelDisable (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| void | USBDMAChannelConfigSet (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Endpoint, uint32_t ui32Config) |
| |
| uint32_t | USBDMAChannelStatus (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| void | USBDMAChannelStatusClear (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Status) |
| |
| void | USBDMAChannelAddressSet (uint32_t ui32Base, uint32_t ui32Channel, void *pvAddress) |
| |
| void * | USBDMAChannelAddressGet (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| void | USBDMAChannelCountSet (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Count) |
| |
| uint32_t | USBDMAChannelCountGet (uint32_t ui32Base, uint32_t ui32Channel) |
| |
| uint32_t | USBDMANumChannels (uint32_t ui32Base) |
| |
| void | USBULPIConfig (uint32_t ui32Base, uint32_t ui32Config) |
| |
| void | USBULPIEnable (uint32_t ui32Base) |
| |
| void | USBULPIDisable (uint32_t ui32Base) |
| |
| uint8_t | USBULPIRegRead (uint32_t ui32Base, uint8_t ui8Reg) |
| |
| void | USBULPIRegWrite (uint32_t ui32Base, uint8_t ui8Reg, uint8_t ui8Data) |
| |
| void | USBHostLPMSend (uint32_t ui32Base, uint32_t ui32Address, uint32_t ui32Endpoint) |
| |
| void | USBHostLPMConfig (uint32_t ui32Base, uint32_t ui32ResumeTime, uint32_t ui32Config) |
| |
| void | USBHostLPMResume (uint32_t ui32Base) |
| |
| void | USBDevLPMRemoteWake (uint32_t ui32Base) |
| |
| void | USBDevLPMConfig (uint32_t ui32Base, uint32_t ui32Config) |
| |
| void | USBDevLPMEnable (uint32_t ui32Base) |
| |
| void | USBDevLPMDisable (uint32_t ui32Base) |
| |
| uint32_t | USBLPMLinkStateGet (uint32_t ui32Base) |
| |
| uint32_t | USBLPMEndpointGet (uint32_t ui32Base) |
| |
| bool | USBLPMRemoteWakeEnabled (uint32_t ui32Base) |
| |
| uint32_t | USBLPMIntStatus (uint32_t ui32Base) |
| |
| void | USBLPMIntEnable (uint32_t ui32Base, uint32_t ui32Ints) |
| |
| void | USBLPMIntDisable (uint32_t ui32Base, uint32_t ui32Ints) |
| |