![]() |
![]() |
Functions | |
| void | USBDMAChannelIntEnable (uint32_t ui32Base, uint32_t ui32Channel) |
| void | USBDMAChannelIntDisable (uint32_t ui32Base, uint32_t ui32Channel) |
| uint32_t | USBDMAChannelIntStatus (uint32_t ui32Base) |
| void | USBDMAChannelEnable (uint32_t ui32Base, uint32_t ui32Channel) |
| void | USBDMAChannelDisable (uint32_t ui32Base, uint32_t ui32Channel) |
| void | USBDMAChannelConfigSet (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Endpoint, uint32_t ui32Config) |
| uint32_t | USBDMAChannelStatus (uint32_t ui32Base, uint32_t ui32Channel) |
| void | USBDMAChannelStatusClear (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Status) |
| void | USBDMAChannelAddressSet (uint32_t ui32Base, uint32_t ui32Channel, void *pvAddress) |
| void * | USBDMAChannelAddressGet (uint32_t ui32Base, uint32_t ui32Channel) |
| void | USBDMAChannelCountSet (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Count) |
| uint32_t | USBDMAChannelCountGet (uint32_t ui32Base, uint32_t ui32Channel) |
| uint32_t | USBDMANumChannels (uint32_t ui32Base) |
| void USBDMAChannelIntEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Enable interrupts for a specified integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel interrupt to enable. |
This function enables the USB DMA channel interrupt based on the ui32Channel parameter. The ui32Channel value is a zero-based index of the USB DMA channel. Once enabled, the USBDMAChannelIntStatus() function returns if a DMA channel has generated an interrupt.
Example: Enable the USB DMA channel 3 interrupt.
//! // //! // Enable the USB DMA channel 3 interrupt //! // //! USBDMAChannelIntEnable(USB0_BASE, 3); //!
\return None.
References ASSERT, HWREG, USB_DMACTL0_IE, and USB_O_DMACTL0.
| void USBDMAChannelIntDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Disable interrupts for a specified integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which USB DMA channel interrupt to disable. |
This function disables the USB DMA channel interrupt based on the ui32Channel parameter. The ui32Channel value is a zero-based index of the USB DMA channel.
Example: Disable the USB DMA channel 3 interrupt.
//! // //! // Disable the USB DMA channel 3 interrupt //! // //! USBDMAChannelIntDisable(USB0_BASE, 3); //!
\return None.
References ASSERT, HWREG, USB_DMACTL0_IE, and USB_O_DMACTL0.
| uint32_t USBDMAChannelIntStatus | ( | uint32_t | ui32Base | ) |
Return the current status of the integrated USB DMA interrupts.
| ui32Base | specifies the USB module base address. |
This function returns the current bit-mapped interrupt status for all USB DMA channel interrupt sources. Calling this function automatically clears all currently pending USB DMA interrupts.
Example: Get the pending USB DMA interrupts.
//! uint32_t ui32Ints; //! //! // //! // Get the pending USB DMA interrupts. //! // //! ui32Ints = USBDMAChannelIntStatus(USB0_BASE); //!
\return The bit-mapped interrupts for the DMA channels.
References ASSERT, HWREG, and USB_O_DMAINTR.
| void USBDMAChannelEnable | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Enables integrated USB DMA for a specified channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies the USB DMA channel to enable. |
This function enables the USB DMA channel passed in the ui32Channel parameter. The ui32Channel value is a zero-based index of the USB DMA channel.
Example: Enable USB DMA channel 2.
//! // //! // Enable USB DMA channel 2. //! // //! USBDMAChannelEnable(2); //!
\return None.
References ASSERT, HWREG, USB_DMACTL0_ENABLE, and USB_O_DMACTL0.
| void USBDMAChannelDisable | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Disables integrated USB DMA for a specified channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies the USB DMA channel to disable. |
This function disables the USB DMA channel passed in the ui32Channel parameter. The ui32Channel parameter is a zero-based index of the DMA channel.
Example: Disable USB DMA channel 2.
//! // //! // Disable USB DMA channel 2. //! // //! USBDMAChannelDisable(2); //!
\return None.
References ASSERT, HWREG, USB_DMACTL0_ENABLE, and USB_O_DMACTL0.
| void USBDMAChannelConfigSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel, | ||
| uint32_t | ui32Endpoint, | ||
| uint32_t | ui32Config | ||
| ) |
Assigns and configures an endpoint to a specified integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel to access. |
| ui32Endpoint | is the endpoint to assign to the USB DMA channel. |
| ui32Config | is used to specify the configuration of the USB DMA channel. |
This function assigns an endpoint and configures the settings for a USB DMA channel. The ui32Endpoint parameter is one of the USB_EP_* values and the ui32Channel value is a zero-based index of the DMA channel to configure. The ui32Config parameter is a combination of the USB_DMA_CFG_* values using the following guidelines.
Use one of the following to set the DMA burst mode:
Use one of the following to set the DMA mode:
Use one of the following to set the direction of the transfer:
The following two optional settings allow an application to immediately enable the DMA transfer and/or DMA interrupts when configuring the DMA channel:
Example: Assign channel 0 to endpoint 1 in DMA mode 0, 4 word burst, enable interrupts and immediately enable the transfer.
//! // //! // Assign channel 0 to endpoint 1 in DMA mode 0, 4 word bursts, //! // enable interrupts and immediately enable the transfer. //! // //! USBDMAChannelConfigSet(USB0_BASE, 0, USB_EP_1, //! (USB_DMA_CFG_BURST_4 | USB_DMA_CFG_MODE0 | //! USB_DMA_CFG_DIR_RX | USB_DMA_CFG_INT_EN | //! USB_DMA_CFG_EN)); //!
\return None.
References ASSERT, HWREG, USB_EP_7, and USB_O_DMACTL0.
| uint32_t USBDMAChannelStatus | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Returns the current status for an integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel to query. |
This function returns the current status for the USB DMA channel specified by the ui32Channel parameter. The ui32Channel value is a zero-based index of the USB DMA channel to query.
Example: Get the current USB DMA status for channel 2.
//! uint32_t ui32Status; //! //! // //! // Get the current USB DMA status for channel 2. //! // //! ui32Status = USBDMAChannelStatus(USB0_BASE, 2); //!
\return Returns zero or \b USB_DMACTL0_ERR if there is a pending error condition on a DMA channel.
References ASSERT, HWREG, USB_DMACTL0_ERR, and USB_O_DMACTL0.
| void USBDMAChannelStatusClear | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel, | ||
| uint32_t | ui32Status | ||
| ) |
Clears the integrated USB DMA status for a specified channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel to clear. |
| ui32Status | holds the status bits to clear. |
This function clears the USB DMA channel status for the channel specified by the ui32Channel parameter. The ui32Channel value is a zero-based index of the USB DMA channel to query. The ui32Status parameter specifies the status bits to clear and must be the valid values that are returned from a call to the USBDMAChannelStatus() function.
Example: Clear the current USB DMA status for channel 2.
//! // //! // Clear the any pending USB DMA status for channel 2. //! // //! USBDMAChannelStatusClear(USB0_BASE, 2, USBDMAChannelStatus(USB0_BASE, 2)); //!
\return None.
References ASSERT, HWREG, USB_DMACTL0_ERR, and USB_O_DMACTL0.
| void USBDMAChannelAddressSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel, | ||
| void * | pvAddress | ||
| ) |
Sets the source or destination address for an integrated USB DMA transfer on a specified channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel to configure. |
| pvAddress | specifies the source or destination address for the USB DMA transfer. |
This function sets the source or destination address for the USB DMA channel number specified in the ui32Channel parameter. The ui32Channel value is a zero-based index of the USB DMA channel. The pvAddress parameter is a source address if the transfer type for the DMA channel is transmit and a destination address if the transfer type is receive.
Example: Set the transfer address for USB DMA channel 1.
//! void *pvBuffer; //! //! // //! // Set the address for USB DMA channel 1. //! // //! USBDMAChannelAddressSet(USB0_BASE, 1, pvBuffer); //!
\return None.
References ASSERT, HWREG, and USB_O_DMAADDR0.
| void* USBDMAChannelAddressGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Returns the source or destination address for the specified integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies the USB DMA channel. |
This function returns the DMA address for the channel number specified in the ui32Channel parameter. The ui32Channel value is a zero-based index of the DMA channel to query.
Example: Get the transfer address for USB DMA channel 1.
//! void *pvBuffer; //! //! // //! // Retrieve the current DMA address for channel 1. //! // //! pvBuffer = USBDMAChannelAddressGet(USB0_BASE, 1); //!
\return The current DMA address for a USB DMA channel.
References ASSERT, HWREG, and USB_O_DMAADDR0.
| void USBDMAChannelCountSet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel, | ||
| uint32_t | ui32Count | ||
| ) |
Sets the transfer count for an integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel to access. |
| ui32Count | specifies the number of bytes to transfer. |
This function sets the USB DMA transfer count in bytes for the channel number specified in the ui32Channel parameter. The ui32Channel value is a zero-based index of the DMA channel.
Example: Set the transfer count to 512 bytes for USB DMA channel 1.
//! // //! // Set the transfer count to 512 bytes for USB DMA channel 1. //! // //! USBDMAChannelCountSet(USB0_BASE, 1, 512); //!
\return None.
References ASSERT, HWREG, and USB_O_DMACOUNT0.
| uint32_t USBDMAChannelCountGet | ( | uint32_t | ui32Base, |
| uint32_t | ui32Channel | ||
| ) |
Returns the transfer count for an integrated USB DMA channel.
| ui32Base | specifies the USB module base address. |
| ui32Channel | specifies which DMA channel to access. |
This function returns the USB DMA transfer count in bytes for the channel number specified in the ui32Channel parameter. The ui32Channel value is a zero-based index of the DMA channel to query.
Example: Get the transfer count for USB DMA channel 1.
//! uint32_t ui32Count; //! //! // //! // Get the transfer count for USB DMA channel 1. //! // //! ui32Count = USBDMAChannelCountGet(USB0_BASE, 1); //!
\return The current count for a USB DMA channel.
References ASSERT, HWREG, and USB_O_DMACOUNT0.
| uint32_t USBDMANumChannels | ( | uint32_t | ui32Base | ) |
Returns the available number of integrated USB DMA channels.
| ui32Base | specifies the USB module base address. |
This function returns the total number of DMA channels available when using the integrated USB DMA controller. This function returns 0 if the integrated controller is not present.
Example: Get the number of integrated DMA channels.
//! uint32_t ui32Count; //! //! // //! // Get the number of integrated DMA channels. //! // //! ui32Count = USBDMANumChannels(USB0_BASE); //!
\return The number of integrated USB DMA channels or zero if the integrated USB DMA controller is not present.
References ASSERT, HWREG, USB_O_RAMINFO, and USB_RAMINFO_DMACHAN_S.