![]() |
![]() |
Macros | |
| #define | CRC8_ITER(crc, data) g_pui8Crc8CCITT[(uint8_t)((crc) ^ (data))] |
| #define | CRC16_ITER(crc, data) |
| #define | CRC32_ITER(crc, data) |
Functions | |
| uint8_t | Crc8CCITT (uint8_t ui8Crc, const uint8_t *pui8Data, uint32_t ui32Count) |
| uint16_t | Crc16 (uint16_t ui16Crc, const uint8_t *pui8Data, uint32_t ui32Count) |
| uint16_t | Crc16Array (uint32_t ui32WordLen, const uint32_t *pui32Data) |
| void | Crc16Array3 (uint32_t ui32WordLen, const uint32_t *pui32Data, uint16_t *pui16Crc3) |
| uint32_t | Crc32 (uint32_t ui32Crc, const uint8_t *pui8Data, uint32_t ui32Count) |
| #define CRC8_ITER | ( | crc, | |
| data | |||
| ) | g_pui8Crc8CCITT[(uint8_t)((crc) ^ (data))] |
Referenced by Crc8CCITT().
| #define CRC16_ITER | ( | crc, | |
| data | |||
| ) |
Referenced by Crc16(), and Crc16Array3().
| #define CRC32_ITER | ( | crc, | |
| data | |||
| ) |
Referenced by Crc32().
| uint8_t Crc8CCITT | ( | uint8_t | ui8Crc, |
| const uint8_t * | pui8Data, | ||
| uint32_t | ui32Count | ||
| ) |
Calculates the CRC-8-CCITT of an array of bytes.
| ui8Crc | is the starting CRC-8-CCITT value. |
| pui8Data | is a pointer to the data buffer. |
| ui32Count | is the number of bytes in the data buffer. |
This function is used to calculate the CRC-8-CCITT of the input buffer. The CRC-8-CCITT is computed in a running fashion, meaning that the entire data block that is to have its CRC-8-CCITT computed does not need to be supplied all at once. If the input buffer contains the entire block of data, then ui8Crc should be set to 0. If, however, the entire block of data is not available, then ui8Crc should be set to 0 for the first portion of the data, and then the returned value should be passed back in as ui8Crc for the next portion of the data.
For example, to compute the CRC-8-CCITT of a block that has been split into three pieces, use the following:
//! ui8Crc = Crc8CCITT(0, pui8Data1, ui32Len1); //! ui8Crc = Crc8CCITT(ui8Crc, pui8Data2, ui32Len2); //! ui8Crc = Crc8CCITT(ui8Crc, pui8Data3, ui32Len3); //!
Computing a CRC-8-CCITT in a running fashion is useful in cases where the data is arriving via a serial link (for example) and is therefore not all available at one time. \return The CRC-8-CCITT of the input data.
References CRC8_ITER.
| uint16_t Crc16 | ( | uint16_t | ui16Crc, |
| const uint8_t * | pui8Data, | ||
| uint32_t | ui32Count | ||
| ) |
Calculates the CRC-16 of an array of bytes.
| ui16Crc | is the starting CRC-16 value. |
| pui8Data | is a pointer to the data buffer. |
| ui32Count | is the number of bytes in the data buffer. |
This function is used to calculate the CRC-16 of the input buffer. The CRC-16 is computed in a running fashion, meaning that the entire data block that is to have its CRC-16 computed does not need to be supplied all at once. If the input buffer contains the entire block of data, then ui16Crc should be set to 0. If, however, the entire block of data is not available, then ui16Crc should be set to 0 for the first portion of the data, and then the returned value should be passed back in as ui16Crc for the next portion of the data.
For example, to compute the CRC-16 of a block that has been split into three pieces, use the following:
//! ui16Crc = Crc16(0, pui8Data1, ui32Len1); //! ui16Crc = Crc16(ui16Crc, pui8Data2, ui32Len2); //! ui16Crc = Crc16(ui16Crc, pui8Data3, ui32Len3); //!
Computing a CRC-16 in a running fashion is useful in cases where the data is arriving via a serial link (for example) and is therefore not all available at one time. \return The CRC-16 of the input data.
References CRC16_ITER.
Referenced by Crc16Array().
| uint16_t Crc16Array | ( | uint32_t | ui32WordLen, |
| const uint32_t * | pui32Data | ||
| ) |
Calculates the CRC-16 of an array of words.
| ui32WordLen | is the length of the array in words (the number of bytes divided by 4). |
| pui32Data | is a pointer to the data buffer. |
This function is a wrapper around the running CRC-16 function, providing the CRC-16 for a single block of data.
References Crc16().
| void Crc16Array3 | ( | uint32_t | ui32WordLen, |
| const uint32_t * | pui32Data, | ||
| uint16_t * | pui16Crc3 | ||
| ) |
Calculates three CRC-16s of an array of words.
| ui32WordLen | is the length of the array in words (the number of bytes divided by 4). |
| pui32Data | is a pointer to the data buffer. |
| pui16Crc3 | is a pointer to an array in which to place the three CRC-16 values. |
This function is used to calculate three CRC-16s of the input buffer; the first uses every byte from the array, the second uses only the even-index bytes from the array (in other words, bytes 0, 2, 4, etc.), and the third uses only the odd-index bytes from the array (in other words, bytes 1, 3, 5, etc.).
References CRC16_ITER.
| uint32_t Crc32 | ( | uint32_t | ui32Crc, |
| const uint8_t * | pui8Data, | ||
| uint32_t | ui32Count | ||
| ) |
Calculates the CRC-32 of an array of bytes.
| ui32Crc | is the starting CRC-32 value. |
| pui8Data | is a pointer to the data buffer. |
| ui32Count | is the number of bytes in the data buffer. |
This function is used to calculate the CRC-32 of the input buffer. The CRC-32 is computed in a running fashion, meaning that the entire data block that is to have its CRC-32 computed does not need to be supplied all at once. If the input buffer contains the entire block of data, then ui32Crc should be set to 0xFFFFFFFF. If, however, the entire block of data is not available, then ui32Crc should be set to 0xFFFFFFFF for the first portion of the data, and then the returned value should be passed back in as ui32Crc for the next portion of the data. Once all data has been passed to the function, the final CRC-32 can be obtained by inverting the last returned value.
For example, to compute the CRC-32 of a block that has been split into three pieces, use the following:
//! ui32Crc = Crc32(0xFFFFFFFF, pui8Data1, ui32Len1); //! ui32Crc = Crc32(ui32Crc, pui8Data2, ui32Len2); //! ui32Crc = Crc32(ui32Crc, pui8Data3, ui32Len3); //! ui32Crc ^= 0xFFFFFFFF; //!
Computing a CRC-32 in a running fashion is useful in cases where the data is arriving via a serial link (for example) and is therefore not all available at one time. \return The accumulated CRC-32 of the input data.
References CRC32_ITER.
Referenced by EMACHashFilterBitCalculate(), and EMACVLANHashFilterBitCalculate().