![]() |
![]() |
Functions | |
| void | GPIODirModeSet (uint32_t ui32Port, uint8_t ui8Pins, uint32_t ui32PinIO) |
| uint32_t | GPIODirModeGet (uint32_t ui32Port, uint8_t ui8Pin) |
| void | GPIOIntTypeSet (uint32_t ui32Port, uint8_t ui8Pins, uint32_t ui32IntType) |
| uint32_t | GPIOIntTypeGet (uint32_t ui32Port, uint8_t ui8Pin) |
| void | GPIOPadConfigSet (uint32_t ui32Port, uint8_t ui8Pins, uint32_t ui32Strength, uint32_t ui32PinType) |
| void | GPIOPadConfigGet (uint32_t ui32Port, uint8_t ui8Pin, uint32_t *pui32Strength, uint32_t *pui32PinType) |
| void | GPIOIntEnable (uint32_t ui32Port, uint32_t ui32IntFlags) |
| void | GPIOIntDisable (uint32_t ui32Port, uint32_t ui32IntFlags) |
| uint32_t | GPIOIntStatus (uint32_t ui32Port, bool bMasked) |
| void | GPIOIntClear (uint32_t ui32Port, uint32_t ui32IntFlags) |
| void | GPIOIntRegister (uint32_t ui32Port, void(*pfnIntHandler)(void)) |
| void | GPIOIntUnregister (uint32_t ui32Port) |
| void | GPIOIntRegisterPin (uint32_t ui32Port, uint32_t ui32Pin, void(*pfnIntHandler)(void)) |
| void | GPIOIntUnregisterPin (uint32_t ui32Port, uint32_t ui32Pin) |
| int32_t | GPIOPinRead (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinWrite (uint32_t ui32Port, uint8_t ui8Pins, uint8_t ui8Val) |
| void | GPIOPinTypeADC (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeCAN (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeComparator (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeComparatorOutput (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeDIVSCLK (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeEPI (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeEthernetLED (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeEthernetMII (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeGPIOInput (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeGPIOOutput (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeGPIOOutputOD (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeHibernateRTCCLK (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeI2C (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeI2CSCL (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeLCD (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeOneWire (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypePWM (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeQEI (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeSSI (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeTimer (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeTrace (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeUART (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeUSBAnalog (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeUSBDigital (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeWakeHigh (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOPinTypeWakeLow (uint32_t ui32Port, uint8_t ui8Pins) |
| uint32_t | GPIOPinWakeStatus (uint32_t ui32Port) |
| void | GPIOPinConfigure (uint32_t ui32PinConfig) |
| void | GPIODMATriggerEnable (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIODMATriggerDisable (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOADCTriggerEnable (uint32_t ui32Port, uint8_t ui8Pins) |
| void | GPIOADCTriggerDisable (uint32_t ui32Port, uint8_t ui8Pins) |
| void GPIODirModeSet | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins, | ||
| uint32_t | ui32PinIO | ||
| ) |
Sets the direction and mode of the specified pin(s).
| ui32Port | is the base address of the GPIO port |
| ui8Pins | is the bit-packed representation of the pin(s). |
| ui32PinIO | is the pin direction and/or mode. |
This function configures the specified pin(s) on the selected GPIO port as either input or output under software control, or it configures the pin to be under hardware control.
The parameter ui32PinIO is an enumerated data type that can be one of the following values:
where GPIO_DIR_MODE_IN specifies that the pin is programmed as a software controlled input, GPIO_DIR_MODE_OUT specifies that the pin is programmed as a software controlled output, and GPIO_DIR_MODE_HW specifies that the pin is placed under hardware control.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_DIR_MODE_IN, GPIO_DIR_MODE_OUT, GPIO_O_AFSEL, GPIO_O_DIR, and HWREG.
Referenced by GPIOPinTypeADC(), GPIOPinTypeCAN(), GPIOPinTypeComparator(), GPIOPinTypeComparatorOutput(), GPIOPinTypeDIVSCLK(), GPIOPinTypeEPI(), GPIOPinTypeEthernetLED(), GPIOPinTypeEthernetMII(), GPIOPinTypeGPIOInput(), GPIOPinTypeGPIOOutput(), GPIOPinTypeGPIOOutputOD(), GPIOPinTypeHibernateRTCCLK(), GPIOPinTypeI2C(), GPIOPinTypeI2CSCL(), GPIOPinTypeLCD(), GPIOPinTypeOneWire(), GPIOPinTypePWM(), GPIOPinTypeQEI(), GPIOPinTypeSSI(), GPIOPinTypeTimer(), GPIOPinTypeTrace(), GPIOPinTypeUART(), GPIOPinTypeUSBAnalog(), GPIOPinTypeUSBDigital(), GPIOPinTypeWakeHigh(), and GPIOPinTypeWakeLow().
| uint32_t GPIODirModeGet | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pin | ||
| ) |
Gets the direction and mode of a pin.
| ui32Port | is the base address of the GPIO port. |
| ui8Pin | is the pin number. |
This function gets the direction and control mode for a specified pin on the selected GPIO port. The pin can be configured as either an input or output under software control, or it can be under hardware control. The type of control and direction are returned as an enumerated data type.
References ASSERT, GPIO_O_AFSEL, GPIO_O_DIR, and HWREG.
| void GPIOIntTypeSet | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins, | ||
| uint32_t | ui32IntType | ||
| ) |
Sets the interrupt type for the specified pin(s).
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
| ui32IntType | specifies the type of interrupt trigger mechanism. |
This function sets up the various interrupt trigger mechanisms for the specified pin(s) on the selected GPIO port.
One of the following flags can be used to define the ui32IntType parameter:
In addition to the above flags, the following flag can be OR'd in to the ui32IntType parameter:
The GPIO_DISCRETE_INT is only available on ports P and Q.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_BOTH_EDGES, GPIO_DISCRETE_INT, GPIO_FALLING_EDGE, GPIO_HIGH_LEVEL, GPIO_LOW_LEVEL, GPIO_O_IBE, GPIO_O_IEV, GPIO_O_IS, GPIO_O_SI, GPIO_RISING_EDGE, and HWREG.
| uint32_t GPIOIntTypeGet | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pin | ||
| ) |
Gets the interrupt type for a pin.
| ui32Port | is the base address of the GPIO port. |
| ui8Pin | is the pin number. |
This function gets the interrupt type for a specified pin on the selected GPIO port. The pin can be configured as a falling-edge, rising-edge, or both-edges detected interrupt, or it can be configured as a low-level or high-level detected interrupt. The type of interrupt detection mechanism is returned and can include the GPIO_DISCRETE_INT flag.
References ASSERT, GPIO_O_IBE, GPIO_O_IEV, GPIO_O_IS, GPIO_O_SI, and HWREG.
| void GPIOPadConfigSet | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins, | ||
| uint32_t | ui32Strength, | ||
| uint32_t | ui32PinType | ||
| ) |
Sets the pad configuration for the specified pin(s).
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
| ui32Strength | specifies the output drive strength. |
| ui32PinType | specifies the pin type. |
This function sets the drive strength and type for the specified pin(s) on the selected GPIO port. For pin(s) configured as input ports, the pad is configured as requested, but the only real effect on the input is the configuration of the pull-up or pull-down termination.
The parameter ui32Strength can be one of the following values:
where GPIO_STRENGTH_xMA specifies either 2, 4, or 8 mA output drive strength, and GPIO_OUT_STRENGTH_8MA_SC specifies 8 mA output drive with slew control.
It can also support output drive strengths of 6, 10, and 12 mA.
The parameter ui32PinType can be one of the following values:
where GPIO_PIN_TYPE_STD* specifies a push-pull pin, GPIO_PIN_TYPE_OD* specifies an open-drain pin, *_WPU specifies a weak pull-up, *_WPD specifies a weak pull-down, and GPIO_PIN_TYPE_ANALOG specifies an analog input.
The GPIO_PIN_TYPE_WAKE_* settings specify the pin to be used as a hibernation wake source. The pin sense level can be high or low.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_O_AMSEL, GPIO_O_DEN, GPIO_O_DR12R, GPIO_O_DR2R, GPIO_O_DR4R, GPIO_O_DR8R, GPIO_O_ODR, GPIO_O_PC, GPIO_O_PDR, GPIO_O_PUR, GPIO_O_SLR, GPIO_O_WAKELVL, GPIO_O_WAKEPEN, GPIO_PIN_TYPE_ANALOG, GPIO_PIN_TYPE_OD, GPIO_PIN_TYPE_STD, GPIO_PIN_TYPE_STD_WPD, GPIO_PIN_TYPE_STD_WPU, GPIO_PIN_TYPE_WAKE_HIGH, GPIO_PIN_TYPE_WAKE_LOW, GPIO_STRENGTH_10MA, GPIO_STRENGTH_12MA, GPIO_STRENGTH_2MA, GPIO_STRENGTH_4MA, GPIO_STRENGTH_6MA, GPIO_STRENGTH_8MA, GPIO_STRENGTH_8MA_SC, and HWREG.
Referenced by GPIOPinTypeADC(), GPIOPinTypeCAN(), GPIOPinTypeComparator(), GPIOPinTypeComparatorOutput(), GPIOPinTypeDIVSCLK(), GPIOPinTypeEPI(), GPIOPinTypeEthernetLED(), GPIOPinTypeEthernetMII(), GPIOPinTypeGPIOInput(), GPIOPinTypeGPIOOutput(), GPIOPinTypeGPIOOutputOD(), GPIOPinTypeHibernateRTCCLK(), GPIOPinTypeI2C(), GPIOPinTypeI2CSCL(), GPIOPinTypeLCD(), GPIOPinTypeOneWire(), GPIOPinTypePWM(), GPIOPinTypeQEI(), GPIOPinTypeSSI(), GPIOPinTypeTimer(), GPIOPinTypeTrace(), GPIOPinTypeUART(), GPIOPinTypeUSBAnalog(), GPIOPinTypeUSBDigital(), GPIOPinTypeWakeHigh(), and GPIOPinTypeWakeLow().
| void GPIOPadConfigGet | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pin, | ||
| uint32_t * | pui32Strength, | ||
| uint32_t * | pui32PinType | ||
| ) |
Gets the pad configuration for a pin.
| ui32Port | is the base address of the GPIO port. |
| ui8Pin | is the pin number. |
| pui32Strength | is a pointer to storage for the output drive strength. |
| pui32PinType | is a pointer to storage for the output drive type. |
This function gets the pad configuration for a specified pin on the selected GPIO port. The values returned in pui32Strength and pui32PinType correspond to the values used in GPIOPadConfigSet(). This function also works for pin(s) configured as input pin(s); however, the only meaningful data returned is whether the pin is terminated with a pull-up or down resistor.
References ASSERT, GPIO_O_DEN, GPIO_O_DR12R, GPIO_O_DR2R, GPIO_O_DR4R, GPIO_O_DR8R, GPIO_O_ODR, GPIO_O_PC, GPIO_O_PDR, GPIO_O_PUR, GPIO_O_SLR, GPIO_O_WAKELVL, GPIO_O_WAKEPEN, and HWREG.
| void GPIOIntEnable | ( | uint32_t | ui32Port, |
| uint32_t | ui32IntFlags | ||
| ) |
Enables the specified GPIO interrupts.
| ui32Port | is the base address of the GPIO port. |
| ui32IntFlags | is the bit mask of the interrupt sources to enable. |
This function enables the indicated GPIO interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ui32IntFlags parameter is the logical OR of any of the following:
| void GPIOIntDisable | ( | uint32_t | ui32Port, |
| uint32_t | ui32IntFlags | ||
| ) |
Disables the specified GPIO interrupts.
| ui32Port | is the base address of the GPIO port. |
| ui32IntFlags | is the bit mask of the interrupt sources to disable. |
This function disables the indicated GPIO interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The ui32IntFlags parameter is the logical OR of any of the following:
| uint32_t GPIOIntStatus | ( | uint32_t | ui32Port, |
| bool | bMasked | ||
| ) |
Gets interrupt status for the specified GPIO port.
| ui32Port | is the base address of the GPIO port. |
| bMasked | specifies whether masked or raw interrupt status is returned. |
If bMasked is set as true, then the masked interrupt status is returned; otherwise, the raw interrupt status is returned.
References ASSERT, GPIO_O_MIS, GPIO_O_RIS, and HWREG.
| void GPIOIntClear | ( | uint32_t | ui32Port, |
| uint32_t | ui32IntFlags | ||
| ) |
Clears the specified interrupt sources.
| ui32Port | is the base address of the GPIO port. |
| ui32IntFlags | is the bit mask of the interrupt sources to disable. |
Clears the interrupt for the specified interrupt source(s).
The ui32IntFlags parameter is the logical OR of the GPIO_INT_* values.
References ASSERT, GPIO_O_ICR, and HWREG.
| void GPIOIntRegister | ( | uint32_t | ui32Port, |
| void(*)(void) | pfnIntHandler | ||
| ) |
Registers an interrupt handler for a GPIO port.
| ui32Port | is the base address of the GPIO port. |
| pfnIntHandler | is a pointer to the GPIO port interrupt handling function. |
This function ensures that the interrupt handler specified by pfnIntHandler is called when an interrupt is detected from the selected GPIO port. This function also enables the corresponding GPIO interrupt in the interrupt controller; individual pin interrupts and interrupt sources must be enabled with GPIOIntEnable().
References ASSERT.
| void GPIOIntUnregister | ( | uint32_t | ui32Port | ) |
Removes an interrupt handler for a GPIO port.
| ui32Port | is the base address of the GPIO port. |
This function unregisters the interrupt handler for the specified GPIO port. This function also disables the corresponding GPIO port interrupt in the interrupt controller; individual GPIO interrupts and interrupt sources must be disabled with GPIOIntDisable().
References ASSERT.
| void GPIOIntRegisterPin | ( | uint32_t | ui32Port, |
| uint32_t | ui32Pin, | ||
| void(*)(void) | pfnIntHandler | ||
| ) |
Registers an interrupt handler for an individual pin of a GPIO port.
| ui32Port | is the base address of the GPIO port. |
| ui32Pin | is the pin whose interrupt is to be registered. |
| pfnIntHandler | is a pointer to the GPIO port interrupt handling function. |
This function ensures that the interrupt handler specified by pfnIntHandler is called when an interrupt is detected from the selected pin of a GPIO port. This function also enables the corresponding GPIO pin interrupt in the interrupt controller.
References ASSERT.
| void GPIOIntUnregisterPin | ( | uint32_t | ui32Port, |
| uint32_t | ui32Pin | ||
| ) |
Removes an interrupt handler for an individual pin of a GPIO port.
| ui32Port | is the base address of the GPIO port. |
| ui32Pin | is the pin whose interrupt is to be unregistered. |
This function unregisters the interrupt handler for the specified pin of a GPIO port. This function also disables the corresponding GPIO pin interrupt in the interrupt controller.
References ASSERT.
| int32_t GPIOPinRead | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Reads the values present of the specified pin(s).
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The values at the specified pin(s) are read, as specified by ui8Pins. Values are returned for both input and output pin(s), and the value for pin(s) that are not specified by ui8Pins are set to 0.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_O_DATA, and HWREG.
| void GPIOPinWrite | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins, | ||
| uint8_t | ui8Val | ||
| ) |
Writes a value to the specified pin(s).
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
| ui8Val | is the value to write to the pin(s). |
Writes the corresponding bit values to the output pin(s) specified by ui8Pins. Writing to a pin configured as an input pin has no effect.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_O_DATA, and HWREG.
| void GPIOPinTypeADC | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as analog-to-digital converter inputs.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The analog-to-digital converter input pins must be properly configured for the analog-to-digital peripheral to function correctly. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_IN, GPIO_PIN_TYPE_ANALOG, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeCAN | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as a CAN device.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The CAN pins must be properly configured for the CAN peripherals to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_8MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeComparator | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as an analog comparator input.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The analog comparator input pins must be properly configured for the analog comparator to function correctly. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_IN, GPIO_PIN_TYPE_ANALOG, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeComparatorOutput | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as an analog comparator output.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The analog comparator output pins must be properly configured for the analog comparator to function correctly. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeDIVSCLK | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as an clock to be output from the device.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The system control output pin must be properly configured for the DIVSCLK to function correctly. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeEPI | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the external peripheral interface.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The external peripheral interface pins must be properly configured for the external peripheral interface to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_8MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeEthernetLED | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the Ethernet peripheral as LED signals.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The Ethernet peripheral provides four signals that can be used to drive an LED (for example, for link status/activity). This function provides a typical configuration for the pins.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_8MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeEthernetMII | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the Ethernet peripheral as MII signals.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The Ethernet peripheral provides a set of MII signals that are used to connect to an external PHY. This function provides a typical configuration for the pins.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_8MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeGPIOInput | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as GPIO inputs.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The GPIO pins must be properly configured in order to function correctly as GPIO inputs. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_IN, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeGPIOOutput | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as GPIO outputs.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The GPIO pins must be properly configured in order to function correctly as GPIO outputs. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_OUT, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeGPIOOutputOD | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as GPIO open drain outputs.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The GPIO pins must be properly configured in order to function correctly as GPIO outputs. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_OUT, GPIO_PIN_TYPE_OD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeHibernateRTCCLK | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as an Hibernate RTC Clock.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The hibernate output pin must be properly configured for the RTCCLK to function correctly. This function provides the proper configuration for the RTC Clock to be output from the device.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeI2C | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin for use as SDA by the I2C peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin. |
The I2C pins must be properly configured for the I2C peripheral to function correctly. This function provides the proper configuration for the SDA pin.
The pin is specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_OD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeI2CSCL | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin for use as SCL by the I2C peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin. |
The I2C pins must be properly configured for the I2C peripheral to function correctly. This function provides the proper configuration for the SCL pin.
The pin is specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeLCD | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the LCD Controller.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The LCD controller pins must be properly configured for the LCD controller to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_8MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeOneWire | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the 1-Wire module.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The 1-Wire pin must be properly configured for the 1-Wire peripheral to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypePWM | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the PWM peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The PWM pins must be properly configured for the PWM peripheral to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeQEI | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the QEI peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The QEI pins must be properly configured for the QEI peripheral to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, not using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD_WPU, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeSSI | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the SSI peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The SSI pins must be properly configured for the SSI peripheral to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeTimer | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the Timer peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The CCP pins must be properly configured for the timer peripheral to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeTrace | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the Trace peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The Trace pins must be properly configured for the Trace peripheral to function correctly. This function provides a typical configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeUART | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the UART peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The UART pins must be properly configured for the UART peripheral to function correctly. This function provides a typical configuration for those pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeUSBAnalog | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the USB peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
USB analog pins must be properly configured for the USB peripheral to function correctly. This function provides the proper configuration for any USB analog pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_IN, GPIO_PIN_TYPE_ANALOG, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeUSBDigital | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use by the USB peripheral.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
USB digital pins must be properly configured for the USB peripheral to function correctly. This function provides a typical configuration for the digital USB pin(s); other configurations may work as well depending upon the board setup (for example, using the on-chip pull-ups).
This function should only be used with EPEN and PFAULT pins as all other USB pins are analog in nature.
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_HW, GPIO_PIN_TYPE_STD, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeWakeHigh | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as a hibernate wake-on-high source.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The GPIO pins must be properly configured in order to function correctly as hibernate wake-high inputs. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_IN, GPIO_PIN_TYPE_WAKE_HIGH, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| void GPIOPinTypeWakeLow | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Configures pin(s) for use as a hibernate wake-on-low source.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
The GPIO pins must be properly configured in order to function correctly as hibernate wake-low inputs. This function provides the proper configuration for those pin(s).
The pin(s) are specified using a bit-packed byte, where each bit that is set identifies the pin to be accessed, and where bit 0 of the byte represents GPIO port pin 0, bit 1 represents GPIO port pin 1, and so on.
References ASSERT, GPIO_DIR_MODE_IN, GPIO_PIN_TYPE_WAKE_LOW, GPIO_STRENGTH_2MA, GPIODirModeSet(), and GPIOPadConfigSet().
| uint32_t GPIOPinWakeStatus | ( | uint32_t | ui32Port | ) |
Retrieves the wake pins status.
| ui32Port | is the base address of the GPIO port. |
This function returns the GPIO wake pin status values. The returned bitfield shows low or high pin state via a value of 0 or 1.
References GPIO_O_WAKESTAT, and HWREG.
| void GPIOPinConfigure | ( | uint32_t | ui32PinConfig | ) |
Configures the alternate function of a GPIO pin.
| ui32PinConfig | is the pin configuration value, specified as only one of the GPIO_P??_??? values. |
This function configures the pin mux that selects the peripheral function associated with a particular GPIO pin. Only one peripheral function at a time can be associated with a GPIO pin, and each peripheral function should only be associated with a single GPIO pin at a time (despite the fact that many of them can be associated with more than one GPIO pin). To fully configure a pin, a GPIOPinType*() function should also be called.
The available mappings are supplied on a per-device basis in pin_map.h.
References ASSERT, GPIO_O_PCTL, and HWREG.
| void GPIODMATriggerEnable | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Enables a GPIO pin as a trigger to start a DMA transaction.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
This function enables a GPIO pin to be used as a trigger to start a uDMA transaction. Any GPIO pin can be configured to be an external trigger for the uDMA. The GPIO pin still generates interrupts if the interrupt is enabled for the selected pin.
References ASSERT, GPIO_O_DMACTL, and HWREG.
| void GPIODMATriggerDisable | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Disables a GPIO pin as a trigger to start a DMA transaction.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
This function disables a GPIO pin from being used as a trigger to start a uDMA transaction. This function can be used to disable this feature if it was enabled via a call to GPIODMATriggerEnable().
References ASSERT, GPIO_O_DMACTL, and HWREG.
| void GPIOADCTriggerEnable | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Enables a GPIO pin as a trigger to start an ADC capture.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
This function enables a GPIO pin to be used as a trigger to start an ADC sequence. Any GPIO pin can be configured to be an external trigger for an ADC sequence. The GPIO pin still generates interrupts if the interrupt is enabled for the selected pin. To enable the use of a GPIO pin to trigger the ADC module, the ADCSequenceConfigure() function must be called with the ADC_TRIGGER_EXTERNAL parameter.
References ASSERT, GPIO_O_ADCCTL, and HWREG.
| void GPIOADCTriggerDisable | ( | uint32_t | ui32Port, |
| uint8_t | ui8Pins | ||
| ) |
Disable a GPIO pin as a trigger to start an ADC capture.
| ui32Port | is the base address of the GPIO port. |
| ui8Pins | is the bit-packed representation of the pin(s). |
This function disables a GPIO pin to be used as a trigger to start an ADC sequence. This function can be used to disable this feature if it was enabled via a call to GPIOADCTriggerEnable().
References ASSERT, GPIO_O_ADCCTL, and HWREG.