Data Fields
tUSBDHIDMouseDevice Struct Reference

#include <usbdhidmouse.h>

Data Fields

const uint16_t ui16VID
 The vendor ID that this device is to present in the device descriptor. More...
 
const uint16_t ui16PID
 The product ID that this device is to present in the device descriptor. More...
 
const uint16_t ui16MaxPowermA
 The maximum power consumption of the device, expressed in milliamps. More...
 
const uint8_t ui8PwrAttributes
 
const tUSBCallback pfnCallback
 
void * pvCBData
 
const uint8_t *const * ppui8StringDescriptors
 
const uint32_t ui32NumStringDescriptors
 
tHIDMouseInstance sPrivateData
 

Detailed Description

This structure is used by the application to define operating parameters for the HID mouse device.

Field Documentation

§ ui16VID

const uint16_t tUSBDHIDMouseDevice::ui16VID

The vendor ID that this device is to present in the device descriptor.

Referenced by USBDHIDMouseCompositeInit().

§ ui16PID

const uint16_t tUSBDHIDMouseDevice::ui16PID

The product ID that this device is to present in the device descriptor.

Referenced by USBDHIDMouseCompositeInit().

§ ui16MaxPowermA

const uint16_t tUSBDHIDMouseDevice::ui16MaxPowermA

The maximum power consumption of the device, expressed in milliamps.

Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().

§ ui8PwrAttributes

const uint8_t tUSBDHIDMouseDevice::ui8PwrAttributes

Indicates whether the device is self- or bus-powered and whether or not it supports remote wakeup. Valid values are USB_CONF_ATTR_SELF_PWR or USB_CONF_ATTR_BUS_PWR, optionally ORed with USB_CONF_ATTR_RWAKE.

Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().

§ pfnCallback

const tUSBCallback tUSBDHIDMouseDevice::pfnCallback

A pointer to the callback function which is called to notify the application of events relating to the operation of the mouse.

Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().

§ pvCBData

void* tUSBDHIDMouseDevice::pvCBData

A client-supplied pointer which is sent as the first parameter in all calls made to the mouse callback, pfnCallback.

Referenced by USBDHIDMouseSetCBData().

§ ppui8StringDescriptors

const uint8_t* const* tUSBDHIDMouseDevice::ppui8StringDescriptors

A pointer to the string descriptor array for this device. This array must contain the following string descriptor pointers in this order. Language descriptor, Manufacturer name string (language 1), Product name string (language 1), Serial number string (language 1),HID Interface description string (language 1), Configuration description string (language 1).

If supporting more than 1 language, the descriptor block (except for string descriptor 0) must be repeated for each language defined in the language descriptor.

Referenced by USBDHIDMouseCompositeInit(), and USBDHIDMouseInit().

§ ui32NumStringDescriptors

const uint32_t tUSBDHIDMouseDevice::ui32NumStringDescriptors

The number of descriptors provided in the ppStringDescriptors array. This must be (1 + (5 * (num languages))).

§ sPrivateData

tHIDMouseInstance tUSBDHIDMouseDevice::sPrivateData

The private instance data for this device. This memory must remain accessible for as long as the mouse device is in use and must not be modified by any code outside the HID mouse driver.

Referenced by USBDHIDMouseCompositeInit(), USBDHIDMouseInit(), USBDHIDMousePowerStatusSet(), USBDHIDMouseRemoteWakeupRequest(), USBDHIDMouseStateChange(), and USBDHIDMouseTerm().


The documentation for this struct was generated from the following file:
Copyright 2017, Texas Instruments Incorporated